2.1. Release Notes - 08_05_00

2.1.1. Introduction

This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

2.1.2. What’s New

ID Description Module Supported Platforms
PDK-10979 UDMA : Support for scatter-gather list UDMA J721E, J784S4
ETHFW-1912 ENET LLD : support DMA Scatter gather TX functionality ENET J721E
ETHFW-1953 CPSW: lwIP: Checksum offload support ENET J721E
ETHFW-2027 mdio: MDIO CDC errata (i2329) workaround implementation (CPSW) ENET J721E

2.1.3. Upgrade and Compatibility

2.1.3.1. CSL

  • CSL ARM R5 Cache operation APIs now accepts a third argument wait, to specify if the function should wait or not until the operation is completed.

    Old New
    CSL_armR5CacheWb(const void * addr, int32_t size) CSL_armR5CacheWb(const void * addr, int32_t size, bool wait)
    CSL_armR5CacheWbInv(const void * addr, int32_t size) CSL_armR5CacheWbInv(const void * addr, int32_t size, bool wait)
    CSL_armR5CacheInv(const void * addr, int32_t size) CSL_armR5CacheInv(const void * addr, int32_t size, bool wait)
  • Added new API CSL_armR5CacheWait. This can be used to wait for the previous cache wb/wbInv/inv operation to complete.

  • For performance optimizations, following CSL cache line operation functions will not invoke memory barrier instructions. Instead end user is supposed to handle the same after updating all the required cache lines.

    1. CSL_armR5CacheInvalidateDcacheMva
    2. CSL_armR5CacheCleanDcacheMva

2.1.3.2. OSAL

  • taskFxn paramater for TaskP_Create is updated from type ‘void*’ to function pointer of type TaskP_Fxn

    • i.e, TaskP_create expects a function pointer of prototype

      void ( * TaskP_Fxn )( void *arg0, void *arg1 )
      
  • name param in TaskP_Params is updated from type uint8_t * to const char *

  • CycleprofilerP_getTimeStamp does not check for R5F PMU counter overflow and refresh the PMU counter higher bits.

    • In case of FreeRTOS, OS tick timer handles this internally by periodically checking for R5F PMU counter overflow and refresh the higher bits of PMU counter in the event of any overflow.
    • In SafeRTOS and Baremetal, this is not handled by default.
    • A new API, CycleprofilerP_refreshCounter is added to check for R5F PMU counter overflow and refresh the higher bits of PMU counter in the event of any overflow.
    • Baremetal/SafeRTOS applications can periodically invoke the new API CycleprofilerP_refreshCounter to handle R5F PMU counter overflow.

2.1.3.3. VHWA

MSC
  • VHWA_M2M_MSC_MAX_INPUT_BUFF macro is removed and instead a new macro VHWA_M2M_MSC_MAX_IN_CHANNEL is added.

  • Following parameters in Vhwa_M2mMscSl2AllocPrms structure is updated from a single dimensional array of size VHWA_M2M_MSC_MAX_INPUT_BUFF to a multi-dimensional array of size VHWA_M2M_MSC_MAX_INST x VHWA_M2M_MSC_MAX_IN_CHANNEL

    1. maxInWidth
    2. inCcsf
    3. inBuffDepth
    • Applications should update the initialization accordingly.
  • isInterleaveFormat parameter which was earlier present in CSL_MscConfig structure is now moved to Msc_ScConfig in include/msc_cfg.h

    • Applications should update the initialization accordingly.

2.1.3.4. Sciclient / TIFS

  • SYSFW/TIFS have added new PSIL host id verification check. Due to this RM PSIL messages from mcu1_0 should use MSG forwarding instead of sending the message to TIFS directly.
    • mcu1_0 will always be in secure mode when trying to send the message to TIFS directly, to avoid self blocking. And all the BoardCfg RM entries for mcu1_0 are for default non-secure host id. Hence for this case, the new PSIL host id verification will fail.
    • By using MSG forwarding, it retains the host id information of the non-secure/secure mode of mcu1_0. Setting forwarding ensures that the mcu1_0 uses the DM2DMSC secure proxy threads. NOTE: Forwarding always leads to forced polling.
    • For all other default base-port and security messages, mcu1_0 can be in secure mode and send the message to TIFS directly.

2.1.3.5. CSI

  • App can select the source CSIRX instance to re-transmit to a specific CSITX instance using newly added lpbkCsiRxInst parameter in Csitx_InstCfg structure.
  • Added a new parameter enableStrm in Csirx_CreateParams. Previously all supported streams were enabled by default, now this info should be provided by the application.

2.1.3.6. SBL

  • Migrated boot app (a tertiary boot loader) from MCUSW to PDK. This app can be used to boot any HLOS like QNX, Linux, etc. More details on BootApp migration at Boot App

2.1.4. Device Support

  • J721E SR1.1, J721E-HS SR1.1 (BOARD=j721e_evm)

  • Associated TIFS versions:

    TIFS name J721E SR revision
    tifs.bin SR1.0 & SR1.1 GP
    tifs-hs-enc.bin SR1.0 HS
    tifs-sr1.1-hs-enc.bin SR1.1 HS

2.1.5. Validation Information

For details on the validated examples refer to the platform specific test report available here.

2.1.6. Tool Chain Information

Component Version
FreeRTOS Kernel 10.4.3
lwIP stack 2.1.2
lwIP-contrib 2.1.0
TI ARM CLANG 1.3.0.LTS
PRU code generation tools 2.3.3
GCC ARM code generation tools ARCH64 9.2-2019.12
CGT XML Processing Scripts 2.61.00
System Analyzer (UIA Target) 2_30_01_02
Component Version
TI C6x code generation tools 8.3.7
TI C7x code generation tools 3.0.0.STS

2.1.7. Change Request

Refer to monthly roadmap slides for changes in the planned features

2.1.8. Fixed Issues

ID Head Line Module Affected Versions Affected Platforms
PDK-8448 SBL SMP multicore boot test fails with SYSFW rearch SBL 07.01.00 J721E-HS, J7200-HS
PDK-9528 SBL prebuild binary for J721E HS doesn’t work from package SBL 07.03.00 J721E-HS
PDK-11085 SPI instance should be decided by SPI driver and not Board Module OSPI 08.01.00 J721E, J7200
PDK-11240 keywriter: smek gets generated even when argument not specified Security 08.01.00 J721E, J7200
PDK-11237 CSI-Rx UT hangs when run on mcu2_0 CSI2RX 08.02.00 J721E, J721S2
PDK-11762 Remove MCU Only mode demo code from MCUSW Boot App LPM 08.02.00 J721E
PDK-12015 SBL: MCU2_0 or MCU3_0 cannot be booted in LockStep mode SBL 08.02.00 J721E, J7200, J721S2, J784S4
PDK-12065 [CSIRX]: RAW12 packed output format is not working CSI2RX 08.02.00 J721E, J721S2, J784S4
PDK-12080 taskFxn parameter is not pointer to function in TaskP_create OSAL 08.02.00 J721E, J7200, J721S2, J784S4
PDK-12081 UART performance issues in polling mode UART 08.02.00 J721E, J7200, J721S2, J784S4
PDK-12082 [OSAL]: Incorrect type for TaskP_Params.name variable OSAL 08.02.00 J721E, J7200, J721S2, J784S4
PDK-12107 DM: UART Traces are not working with Linux SDK PM 08.02.00 J721E, J7200
PDK-12154 SBL: HS boot flow should unlock ROM firewalls SBL 08.02.00 J721E
PDK-12164 Incorrect DDR End Address with ECC enabled BOARD 08.02.00 J721E, J7200, J721S2, J784S4
PDK-12194 Re-transmission should be enabled by default in CSL MCAN application CSL 08.02.00 J721E, J7200, J721S2, J784S4
PDK-12204 Incorrect parameter check in Dss_m2mDrvDispPipeCfgChk API DSS 08.02.00 J721E
PDK-12210 [CSIRX]: Incorrect powerup sequence CSI2RX 08.04.00 J721E, J721S2, J784S4
PDK-12214 Fix event manager pipe assignment for mutliple pipe scenario DSS 08.04.00 J721E
PDK-12218 [CSL-R5F] Incorrect usage of DMB and DSB for cache operations CSL 08.04.00 J721E, J7200, J721S2, J784S4
PDK-12234 IPC RPMessage_recv() timeout issue IPC 08.04.00 J721E, J7200, J721S2, J784S4
PDK-12239 CSC config get over-written for DSS and DSS_M2M DSS 08.04.00 J721E
PDK-12248 Wrong variable name in makerules_spec documentation COMMON 08.04.00 J721E, J7200, J721S2, J784S4
ETHFW-2029 Enet: SGMII TX/RX not enabled at 100Mbps ENET 08.04.00 J721E, J7200, J784S4

2.1.9. Known Issues

ID Head Line Module Reported in Release Affected Platforms Impact Workaround in this release
PDK-6975 Pulsar (R5F) : High priority interrupt is missed by VIM CSL, OSAL 07.00.00 J721E, J7200 Baremetal implementation is pending Use RTOS instead of baremetal
PDK-9676 UART : Potential interrupt storm UART 07.02.00 J7200, J721E Error interrupt resulting in hang. None
PDK-9696 [SPI] DMA mode does not work for SPI5 McSPI 07.01.00 J721E Cannot use DMA with SPI5 Disable DMA for SPI5 OR use another instance of SPI
PDK-9571 [SPI] Transfer stalls when transfer length is not multiple of FIFO length in DMA mode McSPI 07.02.00 J721E Cannot transfer data if data size is not multiple of FIFO length in DMA mode Use transfer size in multiple of FIFO length
PDK-8300 UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader. UDMA 07.01.00 J721E Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader. Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5.
PDK-6789 MCU/Main NAVSS UDMA memcpy from L2SRAM fails UDMA 07.00.00 J721E Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location Use ring memory from non-L2SRAM location
PDK-5228 Output mismatch when each region requiring 3 TRs VHWA 01.00.00 J721E In multi-region mode with more then 3 TR per region can’t be used In multi-region mode for each region less than 3 TR should be used
PDK-10292 Sciclient Firewall Testapp Fails on HS Device SCICLIENT 07.03.00 J721E-HS None None
PDK-10925 IPC Performance Test hangs after loading the binary IPC 08.01.00 J721E, J7200 The app won’t work for this release None
PDK-11457 MCU Only Mode: IPC attachment with remote cores fail LPM 08.02.00 J721E None None
PDK-11458 MCU Only Mode - Linux boot fails on A72 core LPM 08.02.00 J721E None None
PDK-11854 USART: Spurious DMA Interrupts UART 08.04.00 J721E, J7200, J721S2 None None
PDK-11973 USART: Erroneous clear/trigger of timeout interrupt UART 08.02.00 J721E, J7200, J721S2 None None
PDK-12023 Heap OSAL hangs if previous allocation has buffer overflow OSAL 08.02.00 J721E, J721S2 None None
PDK-12060 Main Domain GPIO does not service interrupts GPIO 08.04.00 J721E, J7200 None None
PDK-12085 [DSS] HPD Pulse event is not handled in the eDP driver DSS 08.02.00 J721E, J721S2, J784S4 None None
PDK-12213 IPC: stack corruption of taskWaiter used in RPMessage_getRemoteEndPt IPC 08.00.00 J721E, J7200, J721S2, J784S4 None Make taskWaiter element as global
PDK-12233 SciServer: Multiple definition of Hwi Data SCICLIENT 08.04.00 J721E, J7200, J721S2, J784S4 None None
PDK-12241 CSIRX: Incorrect DATA Shift value for RAW8 mode CSI2RX 08.04.00 J721E, J721S2, J784S4 None None
PDK-12242 CSIRX: Incorrect Dual Pixel mode for YUV422 CSI2RX 08.04.00 J721E, J721S2, J784S4 None None
PDK-12243 DSS: rxBuffer range check missing in DP_mailbox DSS 08.04.00 J721E, J721S2, J784S4 DP sink module should not send message > 1 KB size None
PDK-12258 MCSPI DMA does not support 48bit address space MCSPI 08.04.00 J721E, J7200, J721S2, J784S4 MCSPI is limited to 32 bit address space None
PDK-12327 FreeRTOS taskLoad is not proper OSAL 08.02.00 J721E, J7200, J721S2, J784S4 Task load calculations could be wrong None
PDK-12358 Non-supported Sciclient APIs are present in header files SCICLIENT 08.04.00 J721E, J7200, J721S2, J784S4 None None
ETHFW-2023 Assertion from EnetMcm_coreAttach API ENET 08.01.00 J721E, J7200, J784S4 Race condition in MCM cmd handling in ETHFW usecases None
ETHFW-2084 Cable connect/disconnect can cause CPSW unrecoverable condition ENET 08.00.00 J721E, J7200, J784S4 Packets will be dropped on the affected MAC port None. Device reboot is required

2.1.10. Limitations

2.1.10.1. PDK

  • PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.
  • TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J721E
  • For Baremetal and SafeRTOS, in case of usage of CycleprofilerP APIs the R5F PMU counter overflow is not handled by default.
    • Applications can periodically use the CycleprofilerP_refreshCounter to check overflow and refresh the higher bits of the PMU counter.

2.1.10.2. ENET

  • Scatter-gather functionality is currently supported only for packet transmission.

2.1.10.3. SafeRTOS

  • None.