40 #ifndef ENET_MOD_PORT_H_ 41 #define ENET_MOD_PORT_H_ 67 typedef struct EnetPort_VlanCfg_s
82 typedef enum EnetPort_EgressPriorityType_e
94 typedef struct EnetPort_TrafficShapingRates_s
106 typedef struct EnetPort_TrafficShapingCfg_s
118 typedef struct EnetPort_PriorityMap_s
128 typedef struct EnetPort_DscpPriorityMap_s
143 typedef struct EnetPort_MaxLen_s
Traffic shaping parameters (committed and excess rates).
Definition: enet_mod_port.h:94
bool dscpIPv4En
Definition: enet_mod_port.h:134
uint64_t excessRateBitsPerSec
Definition: enet_mod_port.h:100
uint32_t portCfi
Definition: enet_mod_port.h:73
VLAN configuration parameters.
Definition: enet_mod_port.h:67
This file contains the basic types using across the Enet driver.
EnetPort_EgressPriorityType
Egress priority type.
Definition: enet_mod_port.h:82
uint32_t mru
Definition: enet_mod_port.h:149
Priority map.
Definition: enet_mod_port.h:118
Definition: enet_mod_port.h:88
uint32_t portPri
Definition: enet_mod_port.h:70
Traffic shaping configuration for all priorities.
Definition: enet_mod_port.h:106
uint32_t portVID
Definition: enet_mod_port.h:76
Definition: enet_mod_port.h:85
#define ENET_PRI_NUM
Packet priority.
Definition: enet_types.h:165
#define ENET_TOS_PRI_NUM
Type of Service (ToS) priority.
Definition: enet_types.h:174
bool dscpIPv6En
Definition: enet_mod_port.h:137
DSCP priority map.
Definition: enet_mod_port.h:128
Maximum packet lengths for TX and RX.
Definition: enet_mod_port.h:143
uint64_t committedRateBitsPerSec
Definition: enet_mod_port.h:97