![Logo](ti_logo.png) |
PDK API Guide for J721E
|
Go to the documentation of this file. 63 #define ENET_CFG_IS_ON(name) ((ENET_CFG_ ## name) == ENET_ON) 66 #define ENET_CFG_IS_OFF(name) ((ENET_CFG_ ## name) == ENET_OFF) 73 #define ENET_CFG_PRINT_BUF_LEN (200U) 76 #define ENET_CFG_HAS_DEFAULT_OSAL (ENET_ON) 79 #define ENET_CFG_HAS_DEFAULT_UTILS (ENET_ON) 82 #define ENET_CFG_SANITY_CHECKS (ENET_ON) 85 #define ENET_CFG_ENETPHY_PHY_MAX (13U) 92 #define ENET_CFG_CPSW_SGMII (ENET_ON) 95 #define ENET_CFG_CPSW_INTERVLAN (ENET_ON) 98 #define ENET_CFG_MDIO_CLAUSE45 (ENET_ON) 101 #define ENET_CFG_CPSW_HOSTPORT_TRAFFIC_SHAPING (ENET_ON) 104 #define ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE (128U) 107 #define ENET_CFG_CPSW_MACPORT_TRAFFIC_SHAPING (ENET_ON) 110 #define ENET_CFG_CPSW_MACPORT_SGMII (ENET_ON) 113 #define ENET_CFG_CPSW_MACPORT_INTERVLAN (ENET_ON) 116 #define ENET_CFG_CPSW_CPTS_STATS (ENET_ON) 119 #define ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE (128U) 122 #if !defined(SOC_AM65XX) 124 #define ENET_CFG_TX_CHANNELS_NUM (8U) 127 #define ENET_CFG_RX_FLOWS_NUM (8U) 130 #define ENET_CFG_RING_MON_NUM (4U) 134 #define ENET_CFG_REMOTE_CLIENT_CORES_MAX (6U) 137 #define ENET_CFG_RM_MAC_ADDR_MAX (10U) 140 #define ENET_CFG_RM_TX_CH_MAX (8U) 143 #define ENET_CFG_RM_RX_CH_MAX (64U) 146 #define ENET_CFG_RM_PRESENT (ENET_ON) 148 #if defined(SOC_AM65XX) 151 #define ENET_CFG_NUM_INSTANCES (7U) 152 #define ENET_CFG_TX_CHANNELS_NUM (4U * ENET_CFG_NUM_INSTANCES) 153 #define ENET_CFG_RX_FLOWS_NUM (8U * ENET_CFG_NUM_INSTANCES) 154 #define ENET_CFG_RING_MON_NUM (8U * ENET_CFG_NUM_INSTANCES) 157 #if defined(SOC_J721E) || defined(SOC_J7200) || defined(SOC_J784S4) 158 #define ENET_CFG_LWIP_IFACE_MAX (2U) 160 #define ENET_CFG_LWIP_IFACE_MAX (1U)