SA2UL Access Outside of SYSFW¶
This guide describes which cryptographic accelerator features are available for access outside of System Firmware and how host software may gain access to the its resources.
Introduction¶
SA2UL is the crypto accelerator subsystem in TIs K3 family of devices. Each SoC has one or more instances of this subsystem. On High Secure (HS) devices, portions of an SA2UL subsystem are dedicated to support authentication and decryption services in System Firmware, while other portions are freely avable for host software to access. System Firmware does not use any SA2UL resources on General Purpose (GP) devices, and on HS devices with multiple SA2UL instances System Firmware does not use the resources on the additional instances. For example:
SoC | Number of SA2UL instances | Device | Used by System Firmware | Host access available |
---|---|---|---|---|
am65x | 1 | AM6_DEV_SA2_UL0 | Yes | Limited |
j721e | 2 | J721E_DEV_MCU_SA2_UL0 | Yes | Limited |
J721E_DEV_SA2_UL0 | No | Yes |
The following section describes the details on availability of the SA2UL resources for host software.
Note
This does not cover the overview of SA2UL or its functional description - please refer to the device TRM for further details.
SA2UL Resource Availability¶
The following table describes the access policies for all SA2UL instances on GP and HS devices
Resource | SA2UL instance | GP Policy | HS Policy |
---|---|---|---|
Control MMR | Primary | Open Access | Read-only access |
Others | Open Access | ||
MMRA | Primary | Open Access | Reserved for System Firmware. System Firmware enables all engines at device boot. Software must confirm engine status from base control MMR. |
Others | Open Access | ||
ECC Aggregator MMR (for SA2UL memories) | Primary | Open Access | Open Access |
Others | |||
TRNG MMR | Primary | Open Access. Engine must be enabled by host software. | Open access. Engine is enabled indefinitely by System Firmware and cannot be modified. |
Others | Open Access. Engine must be enabled by host software. | ||
PKA MMR | Primary | Open Access. Engine must be enabled by host software. | Reserved for System Firmware. Not availablere for host access. |
Others | Open Access. Engine must be enabled by host software. | ||
PSIL Threads | Primary | Full access to all threads 0:M-1 and 0:N-1, where M refers to the total number of ingress threads and N refers to the total egress threads (M * 2 = N). All related engines must beenabled by host software. | System Firmware owns secure threads: ingress thread 0, egress thread 0,1. Open access to ingress thread 1:M-1 and egress threads 2:N-1 only. |
Others | Open Access to all threads. All related engines must be enabled by host software. |
Resource Access¶
Resources listed as open to host software may be accessed through various API available in System Firmware
MMR access
Open MMR regions can be accessed as follows:
- On GP devices, MMRs are open for read/write at device boot
- On HS devices, MMRs are behind unowned firewall regions and configured for
read/write access by all initiators (wildcard access). Permissions can be
updated through TISCI_MSG_SET_FWL_REGION API.
Firewall ownership can be transitioned by TISCI_MSG_CHANGE_FWL_OWNER API in case the host would like to enforce stricter
control access to the module.
- TRNG values may be used for deriving sensitive data (e.g. key generation). Host software may claim firewall ownership and restrict all read/write permissions to just itself in order to prevent eavesdroppers from obtaining the TRNG values. The host can then choose to release the firewall ownership by setting the owner back to none if other hosts require direct access to the module.
Read-only regions are owned by System Firmware and have permissions set up such that all hosts may read the MMR.
PSIL thread access
All PSIL thread pairing and unpairing is performed by the TISCI_MSG_RM_PSIL_PAIR and TISCI_MSG_RM_PSIL_WRITE API.