Board Configuration

Board Configuration in System Firmware

There is board configuration data that serves two roles:

  1. Actual board design choices.
  2. Application defined boot-time configuration. These are detailed below.

Functional goals

Board configuration module enables one time (per boot) configuration of the details of the integration of the SoC onto the board as well as one-time application specific configuration.

Design

Board configuration consists of structured configurations that are placed into regular memory by the host software, made coherent (writeback and fences as required by host architecture) then passed to System Firmware via TISCI_MSG_BOARD_CONFIG. On HS devices, the board config blob is signed and encrypted using customer root public key and customer encryption key for HS-SE devices. For HS-FS and GP devices there are no customer keys, therefore board config must be unsigned and plain text. Please refer to Signing Board Configuration on HS devices on how to sign and encrypt board configuration on HS devices.

It is presumed that this memory is owned by trusted software that will not intentionally corrupt the memory while System Firmware is processing. However, System Firmware will take reasonable precautions for misconfiguration by validating data before it is used.

Warning

It is highly recommended that the TISCI_MSG_BOARD_CONFIG_PM message be sent immediately after TISCI_MSG_BOARD_CONFIG before sending other boardcfg messages to ensure RM and SECURITY have all resources configured as needed.

Power management data used to statically define power management configuration is discussed in detail in Power Management Board Configuration.

Resource management board configuration data is detailed in Resource Management Board Configuration. The RM data defines the following for Hosts:

  • Resource range assignments
  • Order IDs
  • QoS values
  • Priority values
  • Host hierarchy

Security data used to statically define security configuration is discussed in detail in Security Management Board Configuration.

Compile Time Configuration

Define Type Description
BOARDCFG_MAX_MAIN_HOST_COUNT (u16) Maximum number of different processing entities for main, scales all main boardcfg tables. This is the number of simutaneous host id permitted after compacting the holes. Thus, as an example, in soc_doc_am6_public_host_desc_host_list, it is ((u16)18u).
BOARDCFG_MAX_MCU_HOST_COUNT (u16) Maximum number of different processing entities for MCU, scales all MCU boardcfg tables. This is the number of simutaneous host id permitted after compacting the holes. In the example soc_doc_am6_public_host_desc_host_list, it could be up to ((u16)18u) to allow all processing entities to use dedicated resources in MCU.

TISCI API for Board Config

The following are the parameters required in the TI-SCI message to pass board configuration data to System Firmware after System Firmware sends boot notification complete.

Usage

Message Type Normal
Secure Queue Only? Yes

TISCI Message ID

TISCI_MSG_BOARD_CONFIG          (0x000BU)

Message Data Structures

struct tisci_msg_board_config_req

TISCI_MSG_BOARD_CONFIG request to provide the location and size of the boardcfg structure.

Parameter Type Description
hdr struct tisci_header TISCI header
boardcfgp_low u32 Low 32-bits of physical pointer to boardcfg struct.
boardcfgp_high u32 High 32-bits of physical pointer to boardcfg struct.
boardcfg_size u16 Size of configuration data.
boardcfg_devgrp devgrp_t Device group for the base board configuration.

struct tisci_msg_board_config_resp

Empty response for TISCI_MSG_BOARD_CONFIG.

Parameter Type Description
hdr struct tisci_header TISCI header.

Although this message is essentially empty and contains only a header a full data structure is created for consistency in implementation.

Warning

The boardcfg data structures described below must be placed in MCU OCMC SRAM. The address used in the TISCI message will be in MCU OCMC SRAM.

Warning

Please ensure that MSMC is not being accessed when TISCI_MSG_BOARD_CONFIG is sent. System Firmware reconfigures the MSMC firewall on receiving this message. MSMC needs to be inactive for the firewall reconfiguration to succeed.

ABI revision structure

This design requires that both boardcfg_abi_maj and boardcfg_abi_min exactly match what is expected by System Firmware.

Element Type Description
boardcfg_abi_maj u8 Major ABI version (for boardcfg_cfg version, not overall System Firmware version)
boardcfg_abi_min u8 Minor ABI version (for boardcfg_cfg version, not overall System Firmware version)

Configuration substructure enumeration

This is a fixed size c-structure which defines the format of the configuration.

Element Type Description
boardcfg_abi_rev struct boardcfg_abi_rev Board Config ABI version (separate from System Firmware ABI version)
control struct boardcfg_control System Firmware feature control selections
secproxy struct boardcfg_secproxy Secure proxy configuration
msmc struct boardcfg_msmc MSMC configuration
debug_cfg struct boardcfg_dbg_cfg Debug/trace configuration

boardcfg substructure header

This contains a unique magic number for each substructure and the size of the associated superstructure for data validation/API compatibility checks.

Element Type Description
magic u16 unique magic number for data integrity check matching boardcfg substructure header magic numbers
size u16 sizeof(superstructure containing this header) for data integrity check
boardcfg substructure header magic numbers

A unique magic number must be provided for each of the boardcfg structures listed below. The exact value must be used in the magic field of boardcfg substructure header or the boardcfg data will be rejected.

Boardcfg Structure Macro Name Value
boardcfg_control structure BOARDCFG_CONTROL_MAGIC_NUM 0xC1D3U
boardcfg_secproxy structure BOARDCFG_SECPROXY_MAGIC_NUM 0x1207U
Design for boardcfg_msmc BOARDCFG_MSMC_MAGIC_NUM 0xA5C3U
Processor Access List BOARDCFG_PROC_ACL_MAGIC_NUM 0xF1EAU
Host Hierarchy BOARDCFG_HOST_HIERARCHY_MAGIC_NUM 0x8D27U
boardcfg_dbg_cfg BOARDCFG_DBG_CFG_MAGIC_NUM 0x020CU
Extended OTP array configuration BOARDCFG_OTP_CFG_MAGIC_NUM 0x4081U
boardcfg_rm_host_cfg structure BOARDCFG_RM_HOST_CFG_MAGIC_NUM 0x4C41U
boardcfg_rm_resasg structure BOARDCFG_RM_RESASG_MAGIC_NUM 0x7B25U
Derived KEK Management BOARDCFG_DKEK_CFG_MAGIC_NUM 0x5170U

boardcfg_control structure

The boardcfg_control structure is used to enable/disable features in System Firmware based on usecase.

Element Type Description
subhdr struct boardcfg_subhdr Magic and size for integrity check
main_isolation_enable ftbool Enable/disable support for System Firmware main isolation. If disabled, main isolation SCI message will be rejected with NAK.
main_isolation_hostid u16 Host-ID allowed to send SCI-message for main isolation. If mismatch, SCI message will be rejected with NAK.

boardcfg_secproxy structure

Element Type Description
subhdr struct boardcfg_subhdr Magic and size for integrity check
scaling_factor u8 Memory allocation for messages scaling factor. In current design, only value of “1” is supported. For future design, a value of “2” would double all memory allocations and credits, “3” would triple, and so on.
scaling_profile u8 Memory allocation for messages profile number. In current design, only a value of “1” is supported. “0” is always invalid due to fault tolerance.
disable_main_nav_secure_proxy u8 Do not configure main nav secure proxy. This removes all MSMC memory demands from System Firmware but limits MPU channels to one set of secure and one set of insecure. In current design, supports only “0”.

Note

disable_main_nav_secure_proxy paramter is not used in the current System Firmware.

Design for boardcfg_msmc

Cache must be configured by System Firmware in order for MSMC to be used for main secure proxy backing memory and ring memory.

boardcfg_msmc structure

Element Type Description
subhdr struct boardcfg_subhdr Magic and size for integrity check
msmc_cache_size u8 fraction of msmc to be cache in /32 units. Rounds up. Since current msmc support /8 allocation this means that 1/32 rounds up to 1/8.

Design details for System Firmware Debug Console

One value is provided to specific the debug console from the following options specified as bits (so all, some, or none can be enabled)

boardcfg_dbg_dst_ports

Bit Value Definition
TRACE_DST_UART0 0x0001 Traces to UART enabled
TRACE_DST_ITM 0x0004 Traces to ITM (JTAG) enabled
TRACE_DST_MEM 0x0008 Traces to memory buffer enabled

For information on UART instance used for a specific SoC refer to Trace UART Allocation

boardcfg_dbg_src

Bit Value Definition
TRACE_SRC_PM 0x0001 Traces from power management are allowed
TRACE_SRC_RM 0x0002 Traces from resource management are allowed
TRACE_SRC_SEC 0x0004 Traces from security management are allowed
TRACE_SRC_BASE 0x0008 Traces from baseport are allowed
TRACE_SRC_USER 0x0010 Traces from user tasks are allowed
TRACE_SRC_SUPR 0x0020 Traces from supervisor tasks are allowed

boardcfg_dbg_cfg

Field Type Description
subhdr struct boardcfg_subhdr Magic and size for integrity check
trace_dst_enables u16 Each bit from TRACE_DST in struct boardcfg_dbg_dst_ports. Using u16 to allow 2 bits per value for fault tolerance
trace_src_enables u16 Each bit from TRACE_SRC in struct boardcfg_dbg_src. Using u16 to allow 2 bits per value for fault tolerance