VXLIB Function Reference
Mean and Standard Deviation
OpenVX Function Description
Computes the mean pixel value and the standard deviation of the pixels in the input image (which has a dimension width and height).
OpenVX Function Reference Page
https://www.khronos.org/registry/vx/specs/1.1/html/d8/d85/group__group__vision__function__meanstddev.html
VXLIB APIs
VXLIB_meanStdDev_i8u_o32f
: Input image is U8 format and output is float format
Copyright 2022, Texas Instruments Incorporated