VXLIB_src Manifest

2022-13-03

Manifest ID - SRAS00008643

Legend

(explanation of the fields in the Manifest Table below)

Software Name The name of the application or file
Version Version of the application or file
License Type Type of license(s) under which TI will be providing software to the licensee (e.g. BSD-3-Clause, GPL-2.0, TI TSPA License, TI Commercial License). The license could be under Commercial terms or Open Source. See Open Source Reference License Disclaimer in the Disclaimers Section. Whenever possible, TI will use an SPDX Short Identifier for an Open Source License. TI Commercial license terms are not usually included in the manifest and are conveyed through a variety of means such as a clickwrap license upon install, a signed license agreement and so forth.
Location The directory name and path on the media or a specific file where the Software is located. Typically fully qualified path names are not used and instead the relevant top level directory of the application is given. A notation often used in the manifests is [as installed]/directory/*. Note that the asterisk implies that all files under that directory are licensed as the License Type field denotes. Any exceptions to this will generally be denoted as [as installed]/directory/* except as noted below which means as shown in subsequent rows of the manifest.
Delivered As This field will either be “Source”, “Binary” or “Source and Binary” and is the primary form the content of the Software is delivered in. If the Software is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided.
Modified by TI This field will either be “Yes” or “No”. A “Yes” means TI has made changes to the Software. A “No” means TI has not made any changes. Note: This field is not applicable for Software “Obtained from” TI.
Obtained from This field specifies from where or from whom TI obtained the Software. It may be a URL to an Open Source site, a 3rd party licensor, or TI. See Links Disclaimer in the Disclaimers Section.

Disclaimers

Export Control Classification Number (ECCN)

Any use of ECCNs listed in the Manifest is at the user’s risk and without recourse to TI. Your company, as the exporter of record, is responsible for determining the correct classification of any item at the time of export. Any export classification by TI of Software is for TI’s internal use only and shall not be construed as a representation or warranty regarding the proper export classification for such Software or whether an export license or other documentation is required for exporting such Software

Links in the Manifest

Any links appearing on this Manifest (for example in the “Obtained from” field) were verified at the time the Manifest was created. TI makes no guarantee that any listed links will remain active in the future.

Open Source License References

Your company is responsible for confirming the applicable license terms for any open source Software listed in this Manifest that was not “Obtained from” TI. Any open source license specified in this Manifest for Software that was not “Obtained from” TI is for TI’s internal use only and shall not be construed as a representation or warranty regarding the proper open source license terms for such Software.

Export Information

ECCN for Software included in this release:

3D991

VXLIB_src Manifest Table

See the Legend above for a description of these columns.

Software Name Version License Type Delivered As Modified by TI
VXLIB Library 1.1.7 TI Text File License Source and Object N/A Location ~/ti/vxlib/* except for the files listed in (2)
Obtained from TI
VXLIB Library – Khronos 1.1.7 TI Text File License AND Khronos License Source and Object Yes (1) Location See footnote (2)
Obtained from https://www.khronos.org/registry/OpenVX/sample/openvx_sample_1.1.tar.bz2

(1) No file from sample implantation is used as is. Some code snippets for various kernels were copied, primarily as part of the natural c reference library (vxlib_cn.lib).

(2) The following are the individual files that contain some code from the Khronos OpenVX Sample implementation:

ti/vxlib/src/vx/VXLIB_accumulateImage_i8u_io16s/VXLIB_accumulateImage_i8u_io16s_cn.c

ti/vxlib/src/vx/VXLIB_accumulateSquareImage_i8u_io16s/VXLIB_accumulateSquareImage_i8u_io16s_cn.c

ti/vxlib/src/vx/VXLIB_addSquare_i8u_i16s_o16s/VXLIB_addSquare_i8u_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_add_i16s_i16s_o16s/VXLIB_add_i16s_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_add_i8u_i16s_o16s/VXLIB_add_i8u_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_add_i8u_i8u_o16s/VXLIB_add_i8u_i8u_o16s_cn.c

ti/vxlib/src/vx/VXLIB_add_i8u_i8u_o8u/VXLIB_add_i8u_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_IYUVtoRGBX_i8u_o8u/VXLIB_colorConvert_IYUVtoRGBX_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_IYUVtoRGB_i8u_o8u/VXLIB_colorConvert_IYUVtoRGB_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_NVXXtoIYUV_i8u_o8u/VXLIB_colorConvert_NVXXtoIYUV_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_NVXXtoRGBX_i8u_o8u/VXLIB_colorConvert_NVXXtoRGBX_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_NVXXtoRGB_i8u_o8u/VXLIB_colorConvert_NVXXtoRGB_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_NVXXtoYUV4_i8u_o8u/VXLIB_colorConvert_NVXXtoYUV4_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_RGBXtoIYUV_i8u_o8u/VXLIB_colorConvert_RGBXtoIYUV_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_RGBXtoNV12_i8u_o8u/VXLIB_colorConvert_RGBXtoNV12_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_RGBXtoYUV4_i8u_o8u/VXLIB_colorConvert_RGBXtoYUV4_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_RGBtoIYUV_i8u_o8u/VXLIB_colorConvert_RGBtoIYUV_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_RGBtoNV12_i8u_o8u/VXLIB_colorConvert_RGBtoNV12_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_RGBtoYUV4_i8u_o8u/VXLIB_colorConvert_RGBtoYUV4_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_YUVXtoIYUV_i8u_o8u/VXLIB_colorConvert_YUVXtoIYUV_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_YUVXtoNV12_i8u_o8u/VXLIB_colorConvert_YUVXtoNV12_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_YUVXtoRGBX_i8u_o8u/VXLIB_colorConvert_YUVXtoRGBX_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_colorConvert_YUVXtoRGB_i8u_o8u/VXLIB_colorConvert_YUVXtoRGB_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_convertDepth_i16s_o8u/VXLIB_convertDepth_i16s_o8u_cn.c

ti/vxlib/src/vx/VXLIB_convolve_3x3_i8u_c16s_o16s/VXLIB_convolve_3x3_i8u_c16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_convolve_3x3_i8u_c16s_o8u/VXLIB_convolve_3x3_i8u_c16s_o8u_cn.c

ti/vxlib/src/vx/VXLIB_convolve_5x5_i8u_c16s_o16s/VXLIB_convolve_5x5_i8u_c16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_convolve_5x5_i8u_c16s_o8u/VXLIB_convolve_5x5_i8u_c16s_o8u_cn.c

ti/vxlib/src/vx/VXLIB_convolve_7x7_i8u_c16s_o16s/VXLIB_convolve_7x7_i8u_c16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_convolve_7x7_i8u_c16s_o8u/VXLIB_convolve_7x7_i8u_c16s_o8u_cn.c

ti/vxlib/src/vx/VXLIB_convolve_i8u_c16s_o16s/VXLIB_convolve_i8u_c16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_convolve_i8u_c16s_o8u/VXLIB_convolve_i8u_c16s_o8u_cn.c

ti/vxlib/src/vx/VXLIB_equalizeHist_i8u_o8u/VXLIB_equalizeHist_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_fastCornersDetect_i8u/VXLIB_fastCornersDetect_i8u_cn.c

ti/vxlib/src/vx/VXLIB_fastCornersScore_i8u/VXLIB_fastCornersScore_i8u_cn.c

ti/vxlib/src/vx/VXLIB_fastCorners_i8u/VXLIB_fastCorners_i8u_cn.c

ti/vxlib/src/vx/VXLIB_harrisCornersDetect_i32f/VXLIB_harrisCornersDetect_i32f_cn.c

ti/vxlib/src/vx/VXLIB_harrisCornersScore_i16s_i16s_o32f/VXLIB_harrisCornersScore_i16s_i16s_o32f_cn.c

ti/vxlib/src/vx/VXLIB_harrisCornersScore_i32s_i32s_o32f/VXLIB_harrisCornersScore_i32s_i32s_o32f_cn.c

ti/vxlib/src/vx/VXLIB_histogramCdfLut_i32u_o8u/VXLIB_histogramCdfLut_i32u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_histogram_i8u_o32u/VXLIB_histogram_i8u_o32u_cn.c

ti/vxlib/src/vx/VXLIB_magnitude_i16s_i16s_o16s/VXLIB_magnitude_i16s_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_meanStdDev_i8u_o32f/VXLIB_meanStdDev_i8u_o32f_cn.c

ti/vxlib/src/vx/VXLIB_minMaxLoc_i16s/VXLIB_minMaxLoc_i16s_cn.c

ti/vxlib/src/vx/VXLIB_minMaxLoc_i8u/VXLIB_minMaxLoc_i8u_cn.c

ti/vxlib/src/vx/VXLIB_multiply_i16s_i16s_o16s/VXLIB_multiply_i16s_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_multiply_i8u_i16s_o16s/VXLIB_multiply_i8u_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_multiply_i8u_i8u_o16s/VXLIB_multiply_i8u_i8u_o16s_cn.c

ti/vxlib/src/vx/VXLIB_multiply_i8u_i8u_o8u/VXLIB_multiply_i8u_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_phase_i16s_i16s_o8u/VXLIB_phase_i16s_i16s_o8u_cn.c

ti/vxlib/src/vx/VXLIB_subtract_i16s_i16s_o16s/VXLIB_subtract_i16s_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_subtract_i8u_i16s_o16s/VXLIB_subtract_i8u_i16s_o16s_cn.c

ti/vxlib/src/vx/VXLIB_subtract_i8u_i8u_o16s/VXLIB_subtract_i8u_i8u_o16s_cn.c

ti/vxlib/src/vx/VXLIB_subtract_i8u_i8u_o8u/VXLIB_subtract_i8u_i8u_o8u_cn.c

ti/vxlib/src/vx/VXLIB_trackFeaturesLK_i8u/VXLIB_trackFeaturesLK_i8u_cn.c

ti/vxlib/src/vx/VXLIB_trackFeaturesLK_i8u/c66/VXLIB_trackFeaturesLK_i8u.c


Credits

Licenses


VXLIB_src Licenses


TEXAS INSTRUMENTS TEXT FILE LICENSE

Copyright (c) 2021 Texas Instruments Incorporated

All rights reserved not granted herein.
Limited License.

Texas Instruments Incorporated grants a world-wide, royalty-free, non-exclusive license under copyrights and patents it now or hereafter owns or controls to make, have made, use, import, offer to sell and sell ("Utilize") this software subject to the terms herein. With respect to the foregoing patent license, such license is granted solely to the extent that any such patent is necessary to Utilize the software alone. The patent license shall not apply to any combinations which include this software, other than combinations with devices manufactured by or for TI ("TI Devices"). No hardware patent is licensed hereunder.

Redistributions must preserve existing copyright notices and reproduce this license (including the above copyright notice and the disclaimer and (if applicable) source code license limitations below) in the documentation and/or other materials provided with the distribution

Redistribution and use in binary form, without modification, are permitted provided that the following conditions are met:

* No reverse engineering, decompilation, or disassembly of this software is permitted with respect to any software provided in binary form.
* any redistribution and use are licensed by TI for use only with TI Devices.
* Nothing shall obligate TI to provide you with source code for the software licensed and provided to you in object code.

If software source code is provided to you, modification and redistribution of the source code are permitted provided that the following conditions are met:

* any redistribution and use of the source code, including any resulting derivative works, are licensed by TI for use only with TI Devices.
* any redistribution and use of any object code compiled from the source code and any resulting derivative works, are licensed by TI for use only with TI Devices.

Neither the name of Texas Instruments Incorporated nor the names of its suppliers may be used to endorse or promote products derived from this software without specific prior written permission.

DISCLAIMER.

THIS SOFTWARE IS PROVIDED BY TI AND TI"S LICENSORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL TI AND TI"S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.


Khronos License:
----------------

Copyright (c) 2012-2016 The Khronos Group Inc.

Permission is hereby granted, free of charge, to any person obtaining a
copy of this software and/or associated documentation files (the
"Materials"), to deal in the Materials without restriction, including
without limitation the rights to use, copy, modify, merge, publish,
distribute, sublicense, and/or sell copies of the Materials, and to
permit persons to whom the Materials are furnished to do so, subject to
the following conditions:

The above copyright notice and this permission notice shall be included
in all copies or substantial portions of the Materials.

MODIFICATIONS TO THIS FILE MAY MEAN IT NO LONGER ACCURATELY REFLECTS
KHRONOS STANDARDS. THE UNMODIFIED, NORMATIVE VERSIONS OF KHRONOS
SPECIFICATIONS AND HEADER INFORMATION ARE LOCATED AT
https://www.khronos.org/registry/

THE MATERIALS ARE PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT.
IN NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY
CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT,
TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE
MATERIALS OR THE USE OR OTHER DEALINGS IN THE MATERIALS.