5.2. J721E SBL¶
5.2.1. Introduction¶
The Secondary Bootloader (SBL) for J721E initializes the execution environment for multi-core applications and this can be used to demonstrate a real world product experience. This section covers additional details including execution sequence, tools and additional flashing instructions.
The SBL is essentially a baremetal application, and it uses many components from the Processor SDK
- <PDK>/packages/ti/build : For build infrastructure
- <PDK>/packages/ti/csl : For initialization and SoC addresses
- <PDK>/packages/ti/board : For board and usecase specific initialization
- <PDK>/packages/ti/drv/spi : For reading applications from OSPI flash
- <PDK>/packages/ti/drv/udma : For reading data from boot media using DMA
- <PDK>/packages/ti/drv/mmcsd : For reading applications from MMC/SD/eMMC
- <PDK>/packages/ti/fs/fatfs : For reading files from MMC/SD/eMMC
- <PDK>/packages/ti/drv/sciclient : For communicating with DMSC sub-system
- <PDK>/packages/ti/drv/uart : For log messages
- <PDK>/packages/ti/osal : Primitives required by ti/drv components
The SBL is in turn used by the board framework to load and start diagnostics
Bootloader Execution Sequence
- Power On Reset
- ROM Bootloader (RBL)
- Software pre-programmed in Jacinto ROM memory starts executing
- The RBL performs platform configuration and initialization.
- It then checks sysboot pins and chooses booting device
- The RBL then configures PLL and clock settings for R5, and boot media like eMMC, SD/MMC, OSPI, UART, PCIe, Ethernet etc for reliable boot.
- If no valid bootloader found on booting device, the RBL checks for next booting device, based on sysboot pins
- It then gets image size and load address by checking the X.509 certificate that is part of the bootloader image.
- The RBL then verifies, optionally decrypts and loads the binary to internal memory at the load address specified in the X.509 certificate.
- Finally it resets the R5 and passes control to Secondary Bootloader(SBL) running on the R5.
- Secondary bootloader(SBL)
- User level secondary bootloader(SBL) begins execution from internal memory. It enables ATCM, starts PMU timers for profiling, initializes the MCU, and sets up the stack, heap and globals. It then jumps to main().
- Board Initialization is done by calls to Board_init() API.For additional details refer Processor SDK Board Support.
- The RAT is setup. Pin MUX and UART console are setup by calling Board_init() API. The system firmware (SYSFW or TIFS) is then loaded from the boot media into the DMSC subsystem.
- Once the system firmware is up and running, the rest of the initialization can be done.
- This includes optionally using Board_init() to configure PLLs, LPSCs and DDR.
- The SBL then loads the application from the boot media. If the image is signed, the application will be copied into a user specified reserved memory, and the SBL will attempt to verify the image by calling system firmware APIs. On HS devices, the boot proceeds only if image verification passes.
- The SBL parses application image(s) for each of the core(s) from boot media and scatter loads it to memory.
- Once the application is loaded, the SBL communicates with the system firmware to setup the clocks for the core(s) and release it from reset.
- The core then starts executing from application entry point.
NOTE
- RBL requires boot loader (SBL) to be in a special format with the binary image appended to a X.509 certificate. The certificate contains the load address, size and SHA of the bootloader image.
- For a detailed description of ROM bootloader and more information on the image format expected by the RBL refer the initialization chapter in the J721E Technical Reference Manual
- In addition to the bootloader and application, the DMSC firmware binary is also needed for the SoC to complete the system boot flow.
- The first 256 bytes of the ATCM are reserved by SBL for its use. The SBL initializes the ATCM with 0xFF before it uses it.
- If the multicore application image is signed using the TI Dummy Key, instead of a degenerate key (default setting) the same binary can be used on GP and HS devices. For information on the application’s X.509 certificate format, please refer Security X509 Certificate Documentation
- When the R5 is released from reset, it will always fetch and execute the first intruction from address 0x0.
5.2.2. Block Diagram¶
5.2.3. Memory Map¶
5.2.4. Directory structure¶
sbl
│
├── board
│ └── k3
│ └── sbl_main.c <= define main() for SBL, board specific init
│
├── build
│ ├── makefile <= makefile for the SBL component
│ ├── sbl_am65xx.sh <= For legacy, called by Yocto build
│ ├── sbl_boot_test.mk <= Builds SBL single core tests
│ ├── sbl_smp_test.mk <= Builds example app for using SBL lib
│ ├── sbl_mcu0_boot_perf_test.mk <= Builds example app for SBL performance tuning
│ ├── sbl_mcu0_boot_xip_entry.mk <= Builds example trampoline app to demonstrate transitioning to a XIP app from SBL
│ ├── sbl_mcu0_boot_xip_test.mk <= Builds example app to demonstrate XIP execution from XIP capable boot media
│ ├── sbl_img.mk <= builds SBL image that is loaded and executed by ROM code
│ ├── sbl_lib.mk <= Builds sbl library that other apps can link into
│ ├── sbl_multicore_smp.mk <= Builds multi-core image from SBL lib eg. test to demonstrate symmetric multiprocessor boot (SMP)
│ └── sbl_multicore_amp.mk <= Builds multi-core image from single core tests to demonstrate asymmetric multiprocessor boot (AMP)
│
├── example
│ └── k3MulticoreApp
│ ├── binary
│ │ └── [soc]
│ │ ├── sbl_baremetal_*.appimage <= SBL loadable board specific sample apps for testing SBL boot flow on GP devices
│ │ ├── sbl_baremetal_*.appimage.signed <= SBL loadable board specific signed sample apps for testing SBL boot flow on HS devices
│ │ └── sbl_baremetal_*_release.x*.bin <= Binary image that can be eXecuted In Place on XIP capable boot media
| ├── [soc]
│ │ ├── mcuAmplinker.lds <= Linker command file when TI CGT is used for Asym. Multiproc. boot
│ │ ├── mpuAmplinker.lds <= GCC linker command file (for Cortex Axx cores) for Asym. Multiproc. boot
│ │ ├── mcuXiplinker.lds <= Linker command file for XIP trampoline app
│ │ └── xip_entry.lds <= Linker command file for XIP test case
│ ├── mcuBootPerfLinker_j7.lds <= TI CGT Linker command file for SBL performance tuning example (J721E)
│ ├── mcuBootPerfLinker.lds <= TI CGT Linker command file for SBL performance tuning example (AM65xx)
| ├── mcuBootPerfLinker_small.lds <= TI CGT Linker command file for SBL performance tuning example (for boot with MCU domain only)
│ ├── mcu[core#]LockStepLinker.lds <= Linker command file when TI CGT is used for R5 lock-step boot
│ ├── mpuSmplinker.lds <= GCC linker command file (for Cortex Axx cores) for SMP boot
│ ├── xip_entry.asm <= Entry point of XIP trampoline app
│ ├── xip_stub.c <= Simple SBL test app that demonstrates transitioning to a XIP app
│ ├── sbl_amp_multicore.c <= Simple SBL test that displays UART message
│ ├── sbl_amp_multicore_sections.h <= Allows same source to be loaded to different sections for different cores.
│ ├── sbl_mcu_0_boot_perf_benchmark.c <= SBL Test to tune boot performance.
│ ├── sbl_multicore_a53.asm <= Test case entry point for Cortex-Axx cores
│ ├── sbl_multicore_r5.asm <= Test case entry point for Cortex-R5 cores
│ ├── sbl_multicore_r5_sections.inc <= Allows same source to be loaded to different sections for different MCUs.
│ ├── sbl_printf.c <= Lightweight UART printf function for SBL testing
│ ├── sbl_smp_multicore.c <= Simple SBL SMP test that uses SBL lib to reset MPUs
│ └── sbl_smp_r5.asm <= Provides dummy override function for __mpu_init for SMP testcase.
│
├── binary <= ROM bootable SBL images for each board/boot media
│ ├── [board]
│ └── [bootmedia]
│ └── bin
│ └── sbl_[bootmedia]_img_mcu1_0_release.tiimage
│
├── lib <= SBL lib for each boot media/board supported
│ ├── [bootmedia]
│ │ └── [board]
│ │ └── r5f
│ │ └── release
│ │ └── sbl_lib_[bootmedia].aer5f
│ └── cust
│ └── [board]
│ └── r5f
│ └── release
│ └── sbl_lib_cust.aer5f
│
├── soc <= SOC specific SBL code
│ └── k3
│ ├── [soc]
| | └── linker.cmd <= Linker file used for generating ROM loadable SBL image.
│ ├── sbl_err_trap.h <= Error loops for SBL
│ ├── sbl_init.asm <= SBL Entry point
│ ├── sbl_misc.asm <= SBL Assembly utility functions
│ ├── sbl_log.h <= SBL logging framework
│ ├── sbl_sci_client.c <= Calls system firmware on DMSC
│ ├── sbl_sci_client.h
│ ├── sbl_slave_core_boot.c <= Code that contains the sequence to release a core from reset
│ ├── sbl_slave_core_boot.h
│ ├── sbl_soc.c <= Cache Ops, PMU init, image verfication, etc & SoC specific code like RAT Init..
│ ├── sbl_soc_cfg.h <= Abstraction layer for hiding SoC level changes from SBL
│ └── sbl_profile.h <= SBL profiling framework
│
├── src <= Common drivers used across SOCs
│ ├── mmcsd
│ ├── hyperflash
│ ├── ospi
│ ├── qspi
│ ├── uart
│ ├── rprc <= RPRC image parser used by SBL
│ └── spi
│
└── tools
├── btoccs
├── byteswap
├── ccsutil
├── combined_appimage <= Creates a "combined" .appimage file for booting HLOS images (e.g., ATF,U-boot,Linux)
│ ├── bin
│ │ └── [board]
│ │ ├── base-board.dtb <= Default (example) Linux DTB per platform - to be replaced with desired DTB
│ │ └── combined.appimage <= Output "combined" .appimage for HLOS + RTOS images boot (after build)
│ ├── config.mk <= Configuration make include file. Use this to specify images to include in combined.appimage
│ └── makefile <= combined.appimage Makefile
├── flashWriter <= Unused for AM65xx/J721E. AM65xx/J721E uses Uniflash to program flashes.
├── multicoreImageGen <= Stitches multiple RPRC images for different cores into a single image
├── omapl13x_boot_utils <= Unused for AM65xx/J721E
├── omapl13x_sd_card_format <= Unused for AM65xx/J721E
├── out2rprc <= Converts .out into .rprc files, so that SBL can load non-continuous memory sections
├── scripts <= Scripts used by .out generated by CCS projects into SBL loadable images
│ ├── K3ImageGen.bat
│ └── K3ImageGen.sh
└── tiImageGen <= Unused for AM65xx/J721E. Image generation is handled by PDK build framework (<sdk_install_path>/pdk_*/packages/ti/build/)
5.2.5. Image Formats¶
SBL format:
To generate the a bootable image, the SBL build uses the x509CertificateGen script to sign the sbl binary with so that the ROM Boot Loader (RBL) can parse it. The image format expected by the RBL has been described in detail in the Image Format Section of the J721E Technical Reference Manual
Note
For HS devices, the SBL and system firmware have to be signed with the MPK. For an easy out-of-box experience, the Processor SDK for HS devices signs the SBL and system firmware with a TI Dummy Key. Images signed with a TI dummy key will boot on both GP and HS boards from TI. The build system invokes the script <PDK>/packages/ti/build/makerules/x509CertificateGen* which inturn calls OpenSSL to create the X509 certificate.
Note
For compatibility, all signed certificates must include a software revision extension with a minimum value of 1 as ROM will use this to enforce the revision programmed into the device efuses for anti-rollback protection. This default value of 1 is set into the SDK scripts but must be incremented during the lifecycle of the device if or when the efuse value is incremented. See https://software-dl.ti.com/tisci/esd/latest/6_topic_user_guides/otp_revision.html for more details.
Warning
The TI Dummy Key(s) MUST be replaced by customers during production with their own Private Keys. If the TI Dummy Keys are used in a production system, the system will be open to security attacks. The path of the default (dummy) key used by the signing script for HS devices is <PDK>/packages/ti/build/makerules/k3_dev_mpk.pem
Warning
While SBL and system firmware images signed with the TI Dummy Keys will work on both GP and HS devices, the boot time will be significantly impacted on GP devices. Using SBL signed by TI Dummy Keys on GP devices is only recommended during the prototyping phase - when porting code developed on GP to HS devices.
Application image format:
Two utilities - out2rprc and multicoreImageGen are used to convert an application elf image(s) into an image loadable by the SBL. The structure of a multicore application image is provided below:
RPRC File Header Format
| Offset | Binary value |
|---|---|
| 0x00000000 | Magic Word(43525052) |
| 0x00000004 | Entry Point (Location) |
| 0x00000008 | Reserved Addr |
| 0x0000000C | Section Count |
| 0x00000010 | Version |
RPRC Section Header Format
| Offset | Binary value |
|---|---|
| 0x00000000 | Section start Address |
| 0x00000004 | Reserved Addr |
| 0x00000008 | Size |
| 0x0000000C | Reserved CRC |
| 0x00000010 | Reserved |
Multicore boot image format
Meta Header Start
| Offset | Binary value |
|---|---|
| 0x00000000 | Magic String (0x5254534D) |
| 0x00000004 | Number of Files |
| 0x00000008 | Device ID |
| 0x0000000C | Reserved |
Meta Header per Core
| Offset | Binary value |
|---|---|
| 0x00000000 | Core ID |
| 0x00000004 | Image Offset |
Signed application image format:
To convert the multicore application image into a format that can be verified, the build flow uses the x509CertificateGen script to create a x509 certificate for the app image. Images that have a x509 certificate are called signed images. Signed applications images are mandatory for HS devices, but will work also work on GP devices.
Signed images are automatically detected by the SBL and loaded into a scratch memory area specified during SBL build. The scratch memory area used by default is specified in sbl_lib.mk via the flags SBL_SCRATCH_MEM_START and SBL_SCRATCH_MEM_SIZE. The SBL_SCRATCH_MEM* options can also be specified for custom builds to override the defaults.
The SBL scratch memory is unavailable to applications during app load time, as the SBL is still active. Once the SBL transfers control to the application, this memory is available for app use - in other words SBL_SCRATCH_MEM* is available during app runtime.
For information on the application’s X.509 certificate format, please refer Security X509 Certificate Documentation
5.2.6. Building the SBL and its components¶
This section will cover compiling SBL for GP and HS devices. It will also show how to compile a loadable appimage file from an example application, which can be used as a reference to compile your own custom application.
5.2.6.1. Pre-requisites to Building¶
- Set your environment using pdksetupenv.bat or pdksetupenv.sh located in <PDK>/packages directory. Refer to Processor SDK RTOS Building for information on setting up your build environment
NOTE
- SBL needs openssl to build. To check if openssl is present, type the following at the linux or windows prompt.
openssl version
- To build on Linux, you need to have mono installed.
- Refer Build Dependencies for instructions on how to install these tools, if they are not already present on your system.
5.2.6.2. Compiling SBL for GP (General Purpose) Device¶
Compiling the SBL
To build all the SBL components:
cd <PDK>/packages/ti/boot/sbl/build
gmake clean all (for windows)
make clean all (for Linux)
- SBL image files are be located at: <PDK>/packages/ti/boot/sbl/binary/
- SBL examples are located at <PDK>/packages/ti/boot/sbl/examples/k3MulticoreApp/binary
- SBL lib are located at <PDK>/packages/ti/boot/sbl/lib/
Compile time options for the SBL
The SBL supports several compile time options to tweak the SBL to satisfy requirements of ease of use, boot time and size. These can be enabled or disabled by editing sbl/sbl_component.mk
- SBL_LOG_LEVEL : Controls amount of SBL logs (on the MCU UART) and system firmware logs(on WAKEUP UART). Varies from 0(no logs) to 3 (all logs)
- SBL_USE_DMA : Valid values are 0 (use CPU to access boot media) or 1 (use DMA to access boot media).
- SBL_DISPLAY_PROFILE_INFO : At the end of the boot process, displays a log of timestamps at which different SBL profile points are hit. This is useful to see how much time the SBL spends in different functions. SBL_LOG_LEVEL can significantly affect performance numbers.
- SBL_ENABLE_PLL : Dials up all the PLLs calling Board_init(). Makes it easier for applications as they no longer have to initialize the PLLs. However, enabling this significantly increases boot time and power consumption. Requires system firmware to be loaded.
- SBL_ENABLE_CLOCKS : Enables all the module clocks by calling Board_init(). Makes it easier for applications as they no longer have to enable clocks.
- SBL_ENABLE_DDR : Initializes the DDR. At the cost of boot time, this enables applications to run from and use DDR. SBL_ENABLE_CLOCKS and SBL_ENABLE_PLL must also be enabed for this to work. Enabling this option increases the boot time.
- SBL_SKIP_MCU_RESET : Jumps to the MCU0 application entry point without resetting the core. Enables faster boot time. Will not change the MCU’s mode (lock-step/split). Application also inherits the MCU state as the SBL left it in.
- SBL_ENABLE_DEV_GRP_MCU : Will cause the system firmware to only use MCU domain resources during system firmware initialization. This can be done either to support boot when the main power domain is off, or to save boot time.
- SBL_ENABLE_HLOS_BOOT: SBL will take some extra steps to prepare certain peripherals and resources to be handed over for HLOS (e.g., Linux) control from the Cortex-A cores.
- SBL_HLOS_OWNS_FLASH : Ensures the SBL will leave the OSPI flash in single SPI mode, so that the MAIN domain Cortex-A code (e.g., HLOS) can reset the flash and take control of it, if needed.
- SBL_SKIP_PINMUX_ENABLE : SBL will skip any PINMUX init being done in the bootloader and expect that it will be handled by a subsequent application.
- SBL_SKIP_LATE_INIT : SBL will skip calling the SoC Late Init functions, normally contained in SBL_SocLateInit()
- SBL_USE_MCU_DOMAIN_ONLY : SBL will configure & boot MCU domain cores ONLY. Saves boot time when configuring & using MCU domain only (especially when testing MCU-only boot or measuring Early CAN response).
The SBL also supports a “custom” build, in addition to standard out-of-box builds. A custom build is a useful way of testing out the effect of different build options - like when optimizing for boot time, or enabling custom usecases like eXecute In Place (XIP) to reduce memory usage.
For an example of how to use such custom builds, please refer to sbl/sbl_component.mk. It shows how to specify a select list of build options while building SBL images and libs.
HLOS boot
The SBL now also supports booting ARM Trusted Firmware (ATF) along with either U-boot or HLOS images (e.g., Linux + DTB) on the Cortex-A cores of the device, when used together with the “combined_appimage” make facility in the SBL tools dir.
To boot the combined.appimage that is produced, simply build an alternate SBL bootloader target with “_hlos” (GP device) or “_hlos_hs” (HS device) appended to the build target name (only for MMCSD or OSPI boot modes).
SBL Build Target Examples for HLOS Boot:
- GP device : To boot from SD card, use the “sbl_mmcsd_img_hlos” build target. For OSPI boot mode, use “sbl_ospi_img_hlos”.
- HS device : To boot from SD card, use the “sbl_mmcsd_img_hlos_hs” build target. For OSPI boot mode, use “sbl_ospi_img_hlos_hs”.
SBL Startup
The SBL can specify the R5 configuration (lockstep or split) that ROM needs to use when it starts up the SBL. This info is passed to ROM as a field in the X509 certificate. The value in this field can be controlled by editing the build flag R5_STARTUP_MODE in sbl/build/sbl_img.mk
- EFUSE_DEFAULT : SBL will run with the same R5 configuration the boot rom ran in.
- SPLIT_MODE : ROM will switch the R5 to split mode before starting the SBL (default).
Enabling/Disabling JTAG on secure devices
JTAG access is controlled using a field in the X509 certificate.
By default, for an easy out of box experience, the Processor SDK enables debug via JTAG on High Secure devices. Leaving JTAG enabled, while making it easy for software development, creates a major security hole in production devices.
To disable/change the level of JTAG access on HS devices, update the value of the debugType field in the signing scripts build/makerules/x509template.txt (when building from windows) and build/makerules/x509CertificateGen.sh (when building from linux).
Valid values are:
- 0 : Disable all JTAG access (most secure and most restrictive)
- 1 : Use device defaults (most secure and most restrictive)
- 2 : Allow debug of non-secure code, when the CPU is running in secure mode, JTAG connectivity will be lost
- 4 : Allow debug of both secure and non-secure code (least secure and least restrictive). This is the default.
5.2.6.3. Compiling SBL for HS (High Security) Device¶
This section should be skipped if you are using a GP device.
Compile Non-encrypted SBL for HS Device
The steps to build HS SBL and HS Uniflash Programmer are as below:
cd <PDK>/packages/ti/build
make -s sbl_<bootmode>_img_hs BOARD=$BOARD
where boot mode is mmcsd, ospi, hyperflash, uart and $BOARD is j721e_evm or another valid board which can be listed using **make -s help**
This generates HS SBL images under <PDK>/packages/ti/boot/sbl/binary/<$BOARD>_hs folder
NOTE
- Make sure build environment is set up using pdksetupenv if you have not done so when compiling for GP device.
- If the make does not succeed, try setting DISABLE_RECURSE_DEPS=no like so: make -s sbl_<bootmode>_img_hs BOARD=$BOARD DISABLE_RECURSE_DEPS=no.
Building HS Uniflash programmer is similar to SBL. Instead provide the make target as “board_utils_uart_flash_programmer_hs”. This generates HS uniflash programmer image under <PDK>/packages/ti/board/utils/uniflash/target/bin/<$BOARD>_hs folder
Compile Encrypted SBL for HS Device
A few additional steps on top of compiling non-encrypted SBL for HS device is necessary when compiling an encrypted SBL.
- Open the file <PDK>/packages/ti/build/makerules/x509CertificateGen.sh or x509CertificateGen.ps1 if on Windows.
- Edit line 119 of x509CertificateGen to
ENC_BIN=$BIN"-ENC-"$CERT_SIGNinstead ofENC_BIN=$CERT_SIGN"-ENC-"$BIN - Open <PDK>/packages/ti/build/makerules/common.mk
- Edit line 638 of common.mk that starts with $(SBL_CERT_GEN) -b $(SBL_BIN_PATH) ... by adding the flags -e $(PDK_INSTALL_PATH)/ti/build/makerules/k3_dev_mek.txt -y ENCRYPT
- Compile encrypted SBL for HS device using the same command used for non-encrypted SBL for HS device
This generates encrypted HS SBL images under <PDK>/packages/ti/boot/sbl/binary/<$BOARD>_hs folder with the same name as non-encrypted HS SBL image.
5.2.6.4. Compiling appimage that can be loaded by SBL¶
In this section we will demonstrate how you can create a SBL loadable appimage from an existing ELF file.
Memory Map Considerations
Applications that the SBL loads must comply generally with the sbl-memory-usage. In the application’s linker command file, care must be taken to not use the first 0x100 bytes of the MCU R5’s ATCM memory, as well as the SBL reserved memory from 0x41C00100 to 0x41C80000, for J7xx devices (0x41C00100 to 0x41C3E00, for AM65xx). If the applications are signed, no loadable sections must be placed in the SBL scratch memory area. The scratch memory can be used at application runtime for stacks, heaps, etc.
Also, the SCISERVER now needs to be started on MCU1_0, as part of the MCU1_0 application. The board configuration space for SBL to leave behind for the SCISERVER in MCU SRAM should be left as reserved, at least until Sciclient_init() has executed on MCU1_0 - it is from 0x41C80000 to 0x41C82000. Similarly, the common header location from 0x41CFFB00 to 0x41D00000 should also be left untouched until Sciclient_init() has finished execution.
NOTE
- The local address 0x0 of the MPU is not accessible from the MCU, so any MPU linker command file must not specify any loadable sections in that memory region. The SBL will not be able to access that memory to load code or data.
Compile SBL loadable image from ELF executables
Depending on the usecase, an ELF application executable can be converted into an image that can be loaded by SBL in many ways.
- Using CCS: Any project created using the pdkProjectCreate scripts will automatically generate a SBL loadable app, as part of a post-build step.
- Using makefiles: Add the following lines to the component’s .mk file
app_name_SBL_APPIMAGEGEN = yes
export app_name_SBL_APPIMAGEGEN
- Existing ELF executable: By calling the K3ImageGen script.
Linux Syntax: ./K3ImageGen.sh <CoreID> <.out>
Example:
cd <sdk_install_path>/pdk_*/packages/ti/boot/sbl/tools/scripts/
./K3ImageGen.sh 4 sbl_baremetal_boot_test_<board>_mcu1_0TestApp_release.xer5f
Windows Syntax: K3ImageGen.bat "<CoreID> <.out>"
Example:
cd <sdk_install_path>\pdk_*\packages\ti\boot\sbl\tools\scripts\
K3ImageGen.bat "4 sbl_baremetal_boot_test_<board>_mcu1_0TestApp_release.xer5f"
- Multicore Images: Multicore images, as the name suggests, allows the SBL to load applications for multiple cores from a single image. Creating such images involves three steps.
- Generate the ELF application executables for individual cores
- Convert the ELF executables into intermediate .rprc images
- Combine the .rprc images of individual cores to create a single multicore image
To covert any .out into the intermediate .rprc format, execute the following commands
For Linux:
mono <PDK>/packages/ti/boot/sbl/tools/out2rprc/bin/out2rprc.exe input.out output.rprc
For Windows:
<PDK>\packages\ti\boot\sbl\tools\out2rprc\bin\out2rprc.exe input.out output.rprc
To stitch multiple .rprc images into a multicore image, execute the following command
For Linux:
<PDK>/packages/ti/boot/sbl/tools/multicoreImageGen/bin/MulticoreImageGen LE 55 output.appimage <core_id_1> core_1.rprc <core_id_2> core_2.rprc
For Windows:
<PDK>/packages/ti/boot/sbl/tools/multicoreImageGen/bin/MulticoreImageGen.exe LE 55 output.appimage <core_id_1> core_1.rprc <core_id_2> core_2.rprc
NOTE
- The linux host environment needs to have mono installed.
- The values used for the Core ID and Device ID can be found in sbl/soc/k3/ sbl_slave_core_boot.h
- To simply load an ELF without executing it, use CoreID value ONLY_LOAD_ID
- If an image for MCU_1 core is provided, the SBL will attempt to switch to split mode.
- If only an image for MCU_0 is provided, the SBL will not change the mode of the MCU subsystem.
- To enable SMP on the MPU, ie, to get multiple MPUs execute from a single binary
from the same address, use one of the following core_ids
- MPU1_SMP_ID: The same app binary runs on both cores in MPU cluster 1
- MPU2_SMP_ID: The same app binary runs on both cores in MPU cluster 2
- MPU_SMP_ID: The same app binary runs all the MPUs
Boot a HLOS+RTOS appimage using the combined_appimage tooling
Creating a combined.appimage file including all images necessary to boot U-boot or HLOS on the SoC’s Cortex-A cores, as well as booting RTOS images on the other remote cores can be done with the following 4 steps:
- Modify the sbl/tools/combined_appimage/config.mk file HLOS_BIN_PATH var to point to the desired HLOS images to be booted
- Modify the HLOS_BOOT var in the same file to select “development” option (boots to SPL/U-boot) or “optimized” option (boots ATF/OPTEE/Linux)
- Modify the RTOS_BIN_PATH var there to point to your RTOS binaries and then list the cores & binaries to be loaded in the vars: IMG1, IMG2, ...
- Make the combined.appimage output app using the following make command:
make BOARD=<board> GCC_LINUX_ARM_PATH=<path>
Example:
cd <sdk_install_path>/pdk_*/packages/ti/boot/sbl/tools/combined_appimage
make BOARD=<board> GCC_LINUX_ARM_PATH=<sdk_install_path>/gcc-arm-9.2-2019.12-x86_64-aarch64-none-elf
cd bin/<board>
ls *.appimage
Converting ELF executables to executable binary images
Sometimes, for extremely constrained and specialized usecases like ultra-low-latency boot or DDR-less systems, an ELF application executable can be converted into a binary image that can executed directly from the boot media, without loading into internal memory.
As internal memory is always accessible, this mode of execution allows some otherwise mandatory steps steps like DDR initlization or clock initialization to be done later or skipped altogether.
Working with such highly contrained systems require some special steps..
- Make sure that the boot media supports eXecuting In Place (XIP).
- Use the custom SBL build to select the build options to build a SBL that meets the usecase requirements.
- In the linker command file for the application, make sure that all the data sections, stacks, heaps and globals are in internal read/write memory
- In the linker command file for the application, make sure that there are no holes in the loadable sections. Such non-contiguous sections can drastically blow up the binary image size, when compared to the ELF executable size.
- To generate an executable binary image from the applications ELF file, add the following lines to the component’s .mk file
app_name_SBL_APP_BINIMAGEGEN = yes
export app_name_SBL_APP_BINIMAGEGEN
Compile encrypted SBL loadable image for HS device from ELF executables
An edit to our appimage generation script is necessary to generate encrypted appimage:
- Open <PDK>/packages/ti/boot/sbl/tools/scripts/K3ImageGen.sh for Linux or K3ImageGen.bat for Windows
- Edit line 88 that starts with “$PDK_INSTALL_PATH/ti/build/makerules/x509... by adding the flags: -e $PDK_INSTALL_PATH/ti/build/makerules/k3_dev_mek.txt -y ENCRYPT
Now the K3ImageGen script generates encrypted appimage instead of non-encrypted appimage. It can still be used like so:
cd <sdk_install_path>/pdk_*/packages/ti/boot/sbl/tools/scripts
./K3ImageGen.sh 4 <path_to_ELF_file>/sbl_baremetal_boot_test_<board>_mcu1_0TestApp_release.xer5f
The generated appimage should be in <PDK>/packages/ti/boot/sbl/examples/k3MulticoreApp/binary/<board>/ directory which also has some ELF files that you can use to test the script.
5.2.7. Testing the SBL¶
SBL provides test applications to demonstrate booting the A53/A72 and R5 cores in both symmetric/lock step & asymmetric/split-mode and other features. The multicore sample application prints a message on the UART for each core. The functionality the different tests exercises are listed below.
- sbl_*_boot_test_*_all_coresTestApp_release: A single multicore boot test case that boots each core in the SoC with a separate app. Also tests DDR loading
- sbl_*_boot_test_*_xxxx_xTestApp_release.appimage: A simple testcase for booting core xxxx_x (eg. MCU1_0, MPU2_0 etc.)
- sbl_*_smp_test_*_all_coresTestApp_release.appimage: A single SMP boot test case that boots MCUs in lock step. The MCU app then uses the SBL lib to boot all the MPUs in SMP mode, ie, all the MPUs execute a single binary from the same address.
- sbl_baremetal_boot_perf_*_mcu1_0TestApp_release.appimage: A single MCU1_0 test case that can be used to measure the effect of enabling/disabling the perf. tuning knobs in the SBL for OSPI boot. The size of the test case can be easily modified by changing the values of .space directives in sbl/example/k3MulticoreApp/ sbl_boot_perf_r5.asm to profile for different app image sizes.
- sbl_baremetal_boot_xip_test_*_mcu1_0TestApp_release.xer5f.bin: A testcase demonstrating booting an XIP application from OSPI flash. Please refer to sbl/build/ sbl_mcu0_boot_xip_test.mk and the related linker command file, under sbl/example/k3MulticoreApp/j721e/mcuXiplinker.lds, to see how to convert an existing application into an XIP application. The sbl_*_xip_entry_*.appimage works in tandem with sbl_*xip_test_*.xer5f.bin to transition the system from non-xip to xip boot, as the ROM, by default, does not support XIP from boot media. After programming the sbl and syfw, to program both sbl_*_xip_entry_*.appimage and sbl_*xip_test_*.xer5f.bin into OSPI flash, use the following uniflash commands
For Windows:
.\dslite.bat --mode processors -c COM9 -f <PDK>\packages\ti\boot\sbl\example\k3MulticoreApp\binary\<soc>\sbl_baremetal_boot_xip_entry_<board>_mcu1_0TestApp_release.appimage -d 3 -o 100000
.\dslite.bat --mode processors -c COM9 -f <PDK>\packages\ti\boot\sbl\example\k3MulticoreApp\binary\<soc>\sbl_baremetal_boot_xip_test_<board>_mcu1_0TestApp_release.xer5f.bin -d 3 -o 1C0000
For Linux:
sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f <PDK>/packages/ti/boot/sbl/example/k3MulticoreApp/binary/<soc>/sbl_baremetal_boot_xip_entry_<board>_mcu1_0TestApp_release.appimage -d 3 -o 100000
sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f <PDK>/packages/ti/boot/sbl/example/k3MulticoreApp/binary/<soc>/sbl_baremetal_boot_xip_test_<board>_mcu1_0TestApp_release.xer5f.bin -d 3 -o 1C0000
An example test log for sbl_*_boot_test_*_all_coresTestApp_release is
SBL Revision: xx.xx.xx.xx (MMM DD YYYY - HH:MM:SS)
TIFS(or SYSFW) ver xx.x.x-v20xx.xx (xxx xxx)
MPU1_0 running
MPU1_1 running
MPU2_0 running
MPU2_1 running
MCU1_1 running
MCU1_0 running
MCU1_0 reports: All tests have passed
An example log for sbl_*_smp_test_*_all_coresTestApp_release.appimage is
SBL Revision: xx.xx.xx.xx (MMM DD YYYY - HH:MM:SS)
TIFS(or SYSFW) ver xx.x.x-v20xx.xx (xxx xxx)
MPU SMP boot test
Cores 0 & 1 will boot from 0x801007a0
Cores 6 & 7 will boot in lockstep from 0x70050000
Resetting all ARM cores now...
No of Cortex-A core(s) running: 1
No of Cortex-A core(s) running: 2
No of Cortex-R core(s) running: 3
All tests have passed
An example log for sbl_baremetal_boot_perf_*_mcu1_0TestApp_release.appimage, when the best boot time is reached is
Time elapsed since start of SBL: 36665us
fxn:boot_perf_test_main cycles: 14666041
Attempting board config ...BOARD_INIT_PLL ...passed
BOARD_INIT_MODULE_CLOCK...passed
BOARD_INIT_DDR...passed
Analyzing run results ....
Boot time is now optimized....
All tests have passed
Profiling info ....
MCU @ 400000000Hz.
cycles per usec = 400
fxn: main line: 75 cycle: xxx timestamp: 432us
.
.
.
fxn: SBL_SlaveCoreBoot line: 231 cycle: xxx timestamp: 36149us
The test log for sbl_*_xip_test_*.xer5f.bin is
MCU1_0 running
5.2.8. Boot Modes¶
The SBL supports MMCSD, OSPI, and UART Boot modes. The different boot modes supported for Jacinto is tabulated below.
| MMCSD | OSPI | UART | PCIe | ETH | HYPERFLASH | |
| J721E EVM | YES | YES | YES | NO | NO | NO |
5.2.8.1. Booting Via SD Card¶
- Preparing the SD card.
- Booting the testcase from SD card.
Preparing the SD card
- To boot the target the SD card should be bootable. Follow the steps to Creating bootable SD card in Linux.
- To update the SBL with a newer version, copy the sbl image (sbl_mmcsd_img_mcu1_0_release.tiimage) to the SD card. Rename it to tiboot3.bin
- Copy the generated application image(*.appimage or *.appimage.signed) to the SD card. Rename it to app
- Update the TIFS with a newer version, copy the TIFS system firmware image binary (or, for HS device, use the encrypted TIFS system firmware binary, “tifs-hs-enc.bin”) found in <PDK>/packages/ti/drv/sciclient/soc/V1 to the SD card as tifs.bin.
Booting the testcase from SD card
- Insert SD card into the SD card slot of the board.
- Refer to the Boot Modes section in the J721E EVM Hardware Users Guide to setup the EVM to boot from MMCSD.
- Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
- Power cycle the board to boot the application from the SD card.
- The test logs will be displayed on the MCU UART
5.2.8.2. Booting Via OSPI flash¶
- Programming the OSPI flash
- Flash addresses for Images
- Booting the testcase from OSPI flash
Flash addresses for Images
- tiboot3.bin (SBL) is flashed to address 0x0
- <system_firmware_name>.bin (TIFS or SYSFW) is flashed to address 0x80000
- <app_name>.appimage (APP) is flashed to address 0x100000
- Optional: <xip_app>.bin (XIP.bin) is flashed to 0x1C0000
- OSPI PHY tuning data binary must also be flashed to the start of the last flash sector (e.g., usually a 512kB or 256kB size sector)
Note: The file <system_firmware_name>.bin will be tifs.bin for a J7xx device (for HS device, use the encrypted firmware binary, tifs-hs-enc.bin).
Booting the testcase from OSPI flash
- Refer to the Boot Modes section in the J721E EVM Hardware Users Guide to setup the EVM to boot from OSPI.
- Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
- Power cycle the board to boot the application from the OSPI flash.
- The test logs will be displayed on the MCU UART
5.2.8.3. Booting via UART¶
- Refer to the Boot Modes section in the J721E EVM Hardware Users Guide to setup the EVM to boot from UART.
- Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
- Power cycle the board, the console should show a sequence of CCC being printed
- Choose the X-Modem interface and send the SBL that was built for UART. After the transfer is completed, repeat the same steps for the system firmware and the application. You will see notifications to perform these actions.
Note: The system firmware binary will be tifs.bin for a J7xx device (for HS device, use the encrypted firmware binary, tifs-hs-enc.bin).
Warning
If the system firmware binary is not present in the boot media, the boot will fail without displaying any logs on the MCU UART. SBL enables UART logging only after successfully starting the system firmware image. If the system firmware load fails, the RBL will eventually reset the system.
5.2.9. EVM Setup for testing SBL¶
For information on board specific requirements like power supply, UART console port connections refer the Hardware User guide of the respective boards.
The configurations needed to setup UART console through a serial terminal application on host PC are listed in the next section.
UART Console Setup
PDK SBL prints messages on the UART Serial Console running on the host. Hence, a serial terminal application (like Tera Term/HyperTerminal/minicom) should be running on the host.
- The host serial port must be configured at 115200 baud, no parity, 1 stop bit and no flow control.
- Please ensure that the local echo setting for the terminal is turned off.
- All SBL prints are routed to the MCU UART
- To verify setup is correct, setup the EVM to boot from UART as the Primary Boot Device (refer to J721E EVM Hardware Users Guide ) Power cycle the EVM, and look for the string CCCCCCC on the UART.