Introduction
This application demonstrates the use of VISS node and TI's 2A (AE & AWB) algorithm. It captures RAW images from the image sensor, processes it in VPAC and displays using Display Sub-System. It also processes H3A data for AE and AWB algorithms.
Supported plaforms
Platform | Linux x86_64 | Linux+RTOS mode | QNX+RTOS mode | SoC |
Support | YES | YES | YES | J721e |
Supported image sensors
Sensor | Data Format | Resolution | Frame Rate(s) |
IMX390 | Bayer RAW12 HDR | 1936x1096 | 30, 60 |
AR0233 | Bayer RAW12 HDR | 1920x1280 | 30 |
AR0820 | RCCB RAW12 HDR | 3840x2160 | 27 |
UB9xx Test Pattern | Bayer RAW12 | 3840x2160 | 39 |
UB9xx Test Pattern | YUV422 (UYVY) | 640x480 | 29 |
GW5_AR0233 | YUV422 (UYVY) | 1920x1080 | 30 |
Data flow (RAW12 input)
Steps to run the application on J721e EVM (Linux + RTOS mode)
- Build the application and related libraries as mentioned in Build Instructions for Linux+RTOS mode.
- Connect camera board on any port of Fusion1 board. Application will prompt the user for port selection.
- Use the is_interactive flag to run the demo in an interactive mode which allows the user to select sensor, processing options and print performance characteristics on the UART console.
- Run the app as shown below
cd /opt/vision_apps
source ./vision_apps_init.sh
./vx_app_single_cam.out
- The output is displayed through DSS on HDMI or eDP display - Display interface selection through compile time srtting in the file platform//rtos/common/app_cfg_mcu2_0.h.
Steps to run the application on J721e EVM (QNX + RTOS mode)
- Build the application and related libraries as mentioned in Build Instructions for QNX+RTOS mode.
- Connect camera board on any port of Fusion1 board. Application will prompt the user for port selection.
- Use the is_interactive flag to run the demo in an interactive mode which allows the user to select sensor, processing options and print performance characteristics on the UART console.
- Run the app as shown below
cd /ti_fs/vision_apps
. ./vision_apps_init.sh
./vx_app_single_cam.out
- The output is displayed through DSS on HDMI or eDP display - Display interface selection through compile time setting in the file platform//rtos/common/app_cfg_mcu2_0.h.
Steps to run the application on Linux PC (PC Emulation mode)
- Build the application and related libraries as mentioned in Build Instructions for PC emulation mode.
- Create a test root folder on the PC with the following subdirectories.
- Copy all the raw images to input folder.
- Copy dcc binaries (if any) to dcc_bins folder.
- Create a cfg file specifying raw properties and usecase preferences. One example is included in PSDK at
<psdk_root>/vision_apps/apps/basic_demos/app_single_cam/x86_test_data/001/
- Execute single camera PC app with cfg file as the argument. For e.g.
cd <psdk_root>/vision_apps/
./out/PC/x86_64/LINUX/release/vx_app_single_cam --cfg ./out/PC/x86_64/LINUX/release/vx_app_single_cam apps/basic_demos/app_single_cam/x86_test_data/001/x86_app.cfg
- The output folders will be created and output images will be saved in the corresponding folders.
- Known Issue : LDC node does not support DCC in PC Emulation mode. ldc_enable must be set to 0 in cfg file.