Introduction
This application demonstrates the functionality of a mosaic image generation using OpenGL. It takes in an input image and generates a 2x2 mosaic of that image.
Supported plaforms
Platform | Linux x86_64 | Linux+RTOS mode | QNX+RTOS mode | SoC |
Support | NO | YES | YES | J721e |
Steps to run the application
- Build the application and related libraries as mentioned in Build Instructions
- The input file comes from "${VX_TEST_DATA_PATH}/test_data/psdkra/app_opengl_mosaic/input1_file.bin"
- In Linux+RTOS or QNX+RTOS mode
- VX_TEST_DATA_PATH environment variable is set as part of vision_apps_init.sh
- Run the app as shown below on the J721e EVM target
cd /opt/vision_apps
source ./vision_apps_init.sh
./vx_app_arm_opengl_mosaic.out
- The output mosaic image will be output to a file called "mosaic_output_file.bin" at the location "/opt/vision_apps/test_data/output/".
- The output image is in RGB format with dimensions 1920x1080. It can be viewed with an image viewer that supports this file format, such as 7YUV.