Introduction
TIDL-RT supports various base feature extractors / back-bone networks like Resnets, MobileNets, EfficientNets, ShuffleNets, VGG, DenseNet etc. Apart from these back-bone networks TIDL-RT also supports following post processing meta architectures from Object Detection:
- Single Shot Detection (SSD)
- You Only Look Once (YOLO) V3 and V5 Architecture
- RetinaNet Architecture
- pointPillars Architecture for 3D object detection from lidar data
A Single Shot Detection (SSD)
A.1 Caffe
TIDL-RT supports SSD networks and post processing layers as defined in Caffe-SSD implementation by original SSD authors. User should follow the following steps to provide this information to TIDL-RT via import configuration file:
- Set the metaArchType = 0 (TIDL_metaArchCaffeJacinto)
- Set inputNetFile and inputParamsFile to point to Caffe Prototxt and Caffemodel file with post processing information
User can refer following models and configuration as reference:
- JdetNet512x512:
- Model Link
- Import config file : ti_dl/test/testvecs/config/import/public/caffe/tidl_import_jdetNet.txt
- Pelee Pascal VOC 304x304:
- Model Link
- Import config file : ti_dl/test/testvecs/config/import/public/caffe/tidl_import_peeleNet.txt
A.2 TensorFlow/TFLite
TIDL-RT supports SSD - post processing as defined in TensorFlow Object detection API. User should follow the following steps to provide this information to TIDL-RT via import configuration file:
- Set the metaArchType = 1 (TIDL_metaArchTFSSD)
- List of all the Box and Class prediction heads as part of outDataNamesList
- Set metaLayersNamesList to point to the corresponding pipeline config file
User can refer following model and configuration as reference:
A.3 ONNX
TIDL-RT supports SSD - post processing in ONNX model format. In order to enable this, TIDL-RT defines a protocol buffer format which enables providing the SSD post processing information as defined by original SSD author to TIDL. Protocol buffer definition is available in the following file:
├── ti_dl # Base Directory
│ ├── utils
| | |── tidlMetaArch/tidl_meta_arch.proto
User should follow the following steps to provide this information to TIDL-RT via import configuration file:
- Set the metaArchType = 3 (TIDL_metaArchTIDLSSD)
- List the the tensor names of the Box and Class prediction heads as in original model in the prototxt file. An example for the same is given here
- Set metaLayersNamesList to point to the prototxt file
TIDL-RT model import tool would make the complete network with Flatten, Concatenate and ODPost processing layer. This mechanism is validated with models trained in Pytorch and exported to ONNX. The Object detection demo in SDK uses this flow. User can refer following model and configuration as reference:
- MLPerf ssd-resnet34:
- Model link
- Import Config file: ti_dl/test/testvecs/config/import/public/onnx/tidl_import_mlperf_resnet34_ssd.txt"
B. YOLO Architecture
TIDL-RT supports Yolo architecture (V3 and V5) for object detection post processing. This architecture also takes post processing inform as defined in ONNX-SSD section. User can refer following model and configuration as reference:
- Set the metaArchType = 4 (TIDL_metaArchTIDLYolo) for V3 architecture and metaArchType = 6 (TIDL_metaArchTIDLYoloV5) for V5 architecture
- List the the tensor names of the Box and Class prediction heads as in original model in the prototxt file.
- Set metaLayersNamesList to point to the prototxt file
User can refer following import configuration file as reference :
- YoloV3 model:
- Model link
- Import Config file: ti_dl/test/testvecs/config/import/public/onnx/tidl_import_yolo3.txt
- Protocol Buffer file: ti_dl/test/testvecs/config/import/public/onnx/tidl_import_yolo3_metaarch.prototxt
C. RetinaNet Architecture
TIDL-RT supports RetinaNet architecture for object detection post processing.This architecture also takes post processing inform as defined in ONNX-SSD section. User should follow the following steps to provide this information to TIDL-RT via import configuration file:
- Set the metaArchType = 5 (TIDL_metaArchTIDLRetinaNet)
- List the the tensor names of the Box and Class prediction heads as in original model in the prototxt file.
- Set metaLayersNamesList to point to the prototxt file
D. 3D Object Detection
TIDL-RT supports pointPillars architecture for 3d object detection post processing.This architecture also takes post processing information as defined in ONNX-SSD section. User should follow the following steps to provide this information to TIDL-RT via import configuration file:
- Set the metaArchType = 7 (TIDL_metaArchTIDL3DOD)
- List the the tensor names of the Box , Class and Direction prediction heads as in original model in the prototxt file. An example for the same is given here
- Set metaLayersNamesList to point to the prototxt file
Example TIDL Proto File for Custom SSD network
In the below example box_input: "376", 376 is the output tensor name of convolutions layer with box/loc prediction. in_width and in_height are base image resolution. This shall match with width and height parameters as set in the import config file. All the other parameters are as defined by Original Caffe-SSD implementation.
name: "TIAD SSD ARCH"
caffe_ssd {
name: "ssd_post_proc"
box_input: "376"
box_input: "380"
box_input: "384"
box_input: "388"
box_input: "392"
box_input: "396"
class_input: "378"
class_input: "382"
class_input: "386"
class_input: "390"
class_input: "394"
class_input: "398"
output: "psd_bboxes"
in_width: 768
in_height: 384
prior_box_param {
min_size: 46.1
max_size: 113.7
aspect_ratio: 3.0
flip: true
clip: false
variance: 0.1
variance: 0.1
variance: 0.2
variance: 0.2
offset: 0.5
step: 16
}
prior_box_param {
min_size: 113.7
max_size: 181.2
aspect_ratio: 3.0
aspect_ratio: 5.0
flip: true
clip: false
variance: 0.1
variance: 0.1
variance: 0.2
variance: 0.2
offset: 0.5
step: 32
}
prior_box_param {
min_size: 181.2
max_size: 248.8
aspect_ratio: 3.0
aspect_ratio: 5.0
flip: true
clip: false
variance: 0.1
variance: 0.1
variance: 0.2
variance: 0.2
offset: 0.5
step: 64
}
prior_box_param {
min_size: 248.8
max_size: 316.4
aspect_ratio: 3.0
aspect_ratio: 5.0
flip: true
clip: false
variance: 0.1
variance: 0.1
variance: 0.2
variance: 0.2
offset: 0.5
step: 128
}
prior_box_param {
min_size: 316.4
max_size: 384.0
aspect_ratio: 3.0
aspect_ratio: 5.0
flip: true
clip: false
variance: 0.1
variance: 0.1
variance: 0.2
variance: 0.2
offset: 0.5
step_w: 256
step_h: 192
}
prior_box_param {
min_size: 384.0
max_size: 768.0
aspect_ratio: 3.0
aspect_ratio: 5.0
flip: true
clip: false
variance: 0.1
variance: 0.1
variance: 0.2
variance: 0.2
offset: 0.5
step: 384
}
detection_output_param {
num_classes: 4
share_location: true
background_label_id: 0
nms_param {
nms_threshold: 0.60
top_k: 100
}
code_type: CENTER_SIZE
keep_top_k: 100
confidence_threshold: 0.5
}
}
Example TIDL Proto File for Custom 3D-OD network based on pointPillars
A sample prototext file pointPillars network is provided below. In the below example 208, 206, 207 are the box,class, location head convolution output for pointPillars network. voxel_size_x and voxel_size_y are voxel sizes in meters. Valid area range is provided through min_x/y/z and max_x/y/z, and those values are in meters. Valid area is divided in multiple voxels each of size voxel_size_x/voxel_size_y as described in pointPillars original paper. max_points_per_voxel is the maximum number of points allowed inside in each voxel. If any voxel has 3d points more than max_points_per_voxel, then extra 3D points are discarded.
name: "3dod_ssd"
tidl_3dod {
name: "point_pillars"
min_x: 0.0
max_x: 69.120
min_y: -39.680
max_y: 39.680
min_z: -1.78
max_z: -1.78
voxel_size_x : 0.16
voxel_size_y : 0.16
max_points_per_voxel : 32
box_input: "208"
class_input: "206"
dir_input: "207"
prior_box_3dod_param {
anchor_width: 1.6
anchor_length: 3.9
anchor_height: 1.56
rotation: 0.0
rotation: 90.0
}
detection_output_param {
num_classes: 1
share_location: true
background_label_id: -1
nms_param {
nms_threshold: 0.01
top_k: 100
}
code_type: CODE_TYPE_3DOD
keep_top_k: 100
confidence_threshold: 0.1
}
}