51 #include <src/ip/sdlr_vtm.h> 52 #include <src/ip/sdl_ip_vtm.h> uint8_t SDL_VTM_configVdCtrl
Definition: sdl_ip_vtm.h:88
VTM Voltage Domain configuration.
Definition: sdl_vtm.h:80
int32_t SDL_VTM_intrCntrl(SDL_VTM_InstVd instance, SDL_VTM_intrCtrl intrCtrl)
Set maximum Threshold values of VTM Temperature sensor.
SDL_VTM_InstVd
Definition: sdl_soc_vtm.h:109
uint32_t vtm_ts_th
Definition: sdl_vtm.h:142
SDL_VTM_tsThrVal thr_val
Definition: sdl_vtm.h:108
SDL_VTM_tsGlobal_cfg tsGlobal_cfg
Definition: sdl_vtm.h:90
int32_t SDL_VTM_verifyConfigVd(SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig)
VTM Voltage Domain configures verification.
VTM Static Registers for Temperature sensor.
Definition: sdl_vtm.h:136
VTM temperature sensor configuration.
Definition: sdl_vtm.h:98
uint32_t vtm_ts_ctrl2
Definition: sdl_vtm.h:138
SDL_VTM_configVdCtrl configVdCtrl
Definition: sdl_vtm.h:82
uint32_t vtm_vd_evt_sel_ctrl
Definition: sdl_vtm.h:121
SDL_VTM_vid_opp vid_opp
Definition: sdl_vtm.h:84
int32_t low_temp_in_milli_degree_celsius
Definition: sdl_vtm.h:106
int32_t SDL_VTM_getStaticRegistersTs(SDL_VTM_InstTs instance, SDL_VTM_staticRegsTs *pStaticRegs)
VTM Temperature sensor readback Static configuration registers.
VTM temperature sensor Stat values.
Definition: sdl_ip_vtm.h:623
uint8_t SDL_VTM_Stat_read_ctrl
Definition: sdl_ip_vtm.h:478
int32_t SDL_VTM_verifyConfigTs(SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig)
VTM Temperature sensor configures verification.
uint32_t vtm_ts_th2
Definition: sdl_vtm.h:144
uint8_t vid_opp_val
Definition: sdl_vtm.h:86
VTM Static Registers for Voltage Domain.
Definition: sdl_vtm.h:119
int32_t SDL_VTM_getStaticRegistersVd(SDL_VTM_InstVd instance, SDL_VTM_staticRegsVd *pStaticRegs)
VTM Voltage Domain readback Static configuration registers.
VTM temperature sensor band gap control.
Definition: sdl_ip_vtm.h:573
VTM temperature sensor threshold values.
Definition: sdl_ip_vtm.h:600
uint32_t vtm_ts_ctrl
Definition: sdl_vtm.h:140
uint16_t SDL_VTM_intrCtrl
Definition: sdl_ip_vtm.h:172
int32_t SDL_VTM_initTs(SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig)
VTM Temperature sensor initialization.
SDL_VTM_configTsCtrl configTsCtrl
Definition: sdl_vtm.h:100
int32_t SDL_VTM_initVd(SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig)
VTM Voltage Domain initialization.
uint16_t SDL_VTM_vdEvtSel_set
Definition: sdl_ip_vtm.h:199
int32_t SDL_VTM_getTemp(SDL_VTM_InstTs instance, uint32_t *pTempVal)
Read VTM Temperature sensor values in degree celcius.
SDL_VTM_tsGlobal_cfg vtm_global_cfg
Definition: sdl_vtm.h:125
int32_t SDL_VTM_getSensorStatus(SDL_VTM_InstTs instance, const SDL_VTM_Stat_read_ctrl *pCtrl, SDL_VTM_Stat_val *pStat_val)
Read VTM Temperature sensor status.
SDL_VTM_Ctrlcfg tsCtrl_cfg
Definition: sdl_vtm.h:102
SDL_VTM_InstTs
Definition: sdl_soc_vtm.h:77
uint8_t SDL_VTM_vid_opp
Definition: sdl_ip_vtm.h:124
VTM Global Configuration Registers.
Definition: sdl_ip_vtm.h:535
uint32_t vtm_vd_opp_vid
Definition: sdl_vtm.h:123
int32_t high_temp_in_milli_degree_celsius
Definition: sdl_vtm.h:104
SDL_VTM_vdEvtSel_set vd_temp_evts
Definition: sdl_vtm.h:88
uint8_t SDL_VTM_configTsCtrl
Definition: sdl_ip_vtm.h:106