53 #if defined (SOC_J721E) SDL_PBIST_testType
PBIST self test type.
Definition: sdl_pbist.h:83
This file contains the top level SDL-FL API's for PBIST.
This file contains the SoC-specific SDL PBIST API's and definitions.
This structure contains the different configuration used for PBIST.
Definition: pbist/V0/sdl_ip_pbist.h:88
int32_t SDL_PBIST_selfTest(SDL_PBIST_inst instance, SDL_PBIST_testType testType, const SDL_PBIST_config *pConfig, bool *pResult)
PBIST self test.
Definition: sdl_pbist.h:97
Definition: pbist/soc/j721e/sdl_pbist.h:191
int32_t SDL_PBIST_getPOSTStatus(SDL_PBIST_postResult *pResult)
PBIST POST result status.
SDL_PBIST_inst
PBIST instance.
Definition: pbist/soc/j721e/sdl_pbist.h:78
Definition: sdl_pbist.h:91
int32_t SDL_OSAL_getClecOutputEvent(uint32_t *clecOutputEvt)
Application-provided API to give the PBIST module a clec output event to use upon request for a PBIST...
int32_t SDL_OSAL_releaseClecOutputEvent(uint32_t clecOutputEvt)
Application-provided API to allow PBIST module to release a clec event.