SDL API Guide for J721E
|
===========================================================================
The SDL ESM module provides API to configure ESM events
The Error Signaling Module (ESM) aggregates safety-related events and/or errors from throughout the device into one location. It can signal both low and high priority interrupts to a processor to deal with a safety event and/or manipulate an I/O error pin to signal an external hardware that an error has occurred. Therefore an external controller is able to reset the device or keep the system in a safe, known state.
The SDL APIs provide APIs to do the following functionalities.
Sub Modules | |
ESM Data Structures | |
ESM Enumerated Data Types | |
ESM Functions | |
ESM Macro defines | |