J7200 Processor Descriptions

Introduction

This chapter provides information of Processor and Host IDs that are permitted in the J7200 SoC. These Processor IDs represent an actual physical processor on the SoC.

NOTE: This should not be confused with HOST_ID.

Enumeration of Processor IDs

Processor ID Processor Name Location in SoC
0x20 A72SS0_CORE0_0 COMPUTE_CLUSTER_J7VCL_TB_VDC_MAIN_0_MSMC_EN: (Cluster 0 Processor 0)
0x21 A72SS0_CORE0_1 COMPUTE_CLUSTER_J7VCL_TB_VDC_MAIN_0_MSMC_EN: (Cluster 0 Processor 1)
0x01 MCU_R5FSS0_CORE0 J7VCL_MCU_SEC_MMR_MCU_0: (Cluster 0 Processor 0)
0x02 MCU_R5FSS0_CORE1 J7VCL_MCU_SEC_MMR_MCU_0: (Cluster 0 Processor 1)
0x06 R5FSS0_CORE0 J7VCL_MAIN_SEC_MMR_MAIN_0: (Cluster 0 Processor 0)
0x07 R5FSS0_CORE1 J7VCL_MAIN_SEC_MMR_MAIN_0: (Cluster 0 Processor 1)