54 #ifndef RM_TISCI_CORE_H 55 #define RM_TISCI_CORE_H uint16_t range_start_sec
Definition: tisci_rm_core.h:128
This file contains:
Definition: tisci_rm_core.h:90
struct tisci_header hdr
Definition: tisci_rm_core.h:125
uint8_t secondary_host
Definition: tisci_rm_core.h:94
Get resource range response message.
Definition: tisci_rm_core.h:124
uint8_t subtype
Definition: tisci_rm_core.h:93
struct tisci_header hdr
Definition: tisci_rm_core.h:91
uint16_t range_num_sec
Definition: tisci_rm_core.h:129
uint16_t range_start
Definition: tisci_rm_core.h:126
struct tisci_msg_rm_get_resource_range_req __attribute__((__packed__))
uint16_t range_num
Definition: tisci_rm_core.h:127
uint16_t type
Definition: tisci_rm_core.h:92