The list of kernels supported in hwa module.
Each kernel listed here can be used with the vxGetKernelByName
call. When programming the parameters, use
VX_INPUT
for [in]
VX_OUTPUT
for [out]
VX_BIDIRECTIONAL
for [in,out]
When programming the parameters, use
VX_TYPE_IMAGE
for a vx_image
in the size field of vxGetParameterByIndex
or vxSetParameterByIndex
VX_TYPE_ARRAY
for a vx_array
in the size field of vxGetParameterByIndex
or vxSetParameterByIndex
- or other appropriate types in vx_type_e.
◆ TIVX_MODULE_NAME_IMAGING
#define TIVX_MODULE_NAME_IMAGING "imaging" |
Name for OpenVX Extension kernel module: imaging.
◆ H3A_MAX_WINH
◆ tivxRegisterImagingTargetAewbKernels()
void tivxRegisterImagingTargetAewbKernels |
( |
void |
| ) |
|
Function to register IMAGING Kernels on the aewb Target.
◆ tivxUnRegisterImagingTargetAewbKernels()
void tivxUnRegisterImagingTargetAewbKernels |
( |
void |
| ) |
|
Function to un-register IMAGING Kernels on the aewb Target.
◆ tivxAewbNode()
VX_API_ENTRY vx_node VX_API_CALL tivxAewbNode |
( |
vx_graph |
graph, |
|
|
vx_user_data_object |
configuration, |
|
|
vx_distribution |
histogram, |
|
|
vx_user_data_object |
h3a_aew_af, |
|
|
vx_user_data_object |
ae_awb_result_prev, |
|
|
vx_user_data_object |
ae_awb_result, |
|
|
vx_user_data_object |
dcc_param |
|
) |
| |
[Graph] Creates a AEWB Node.
- Parameters
-
[in] | graph | The reference to the graph. |
[in] | configuration | Configuration of type tivx_aewb_config_t needed by AEWB to parse DCC and H3A stats |
[in] | histogram | (optional) Histogram Optional input for AE. Not supported currently |
[in] | h3a_aew_af | Structure of type tivx_h3a_data_t specifying H3A properties and pointer to the statistics output from VISS |
[in] | ae_awb_result_prev | AE and AWB results from previous iteration. Type tivx_ae_awb_params_t. Optional. Not used currently |
[out] | ae_awb_result | AE and AWB results from previous iteration. Type tivx_ae_awb_params_t |
[in] | dcc_param | Buffer containing DCC Tuning Parameters for 2A node |
- See also
TIVX_KERNEL_AEWB_NAME
- Returns
vx_node
.
- Return values
-
vx_node | A node reference. Any possible errors preventing a successful creation should be checked using vxGetStatus |
◆ tivx_aewb_hist_t