4.10. Release notes - 06_00_01¶
4.10.1. What’s New¶
Note
Only regression testing is performed based on the changes. Full testing will be done in 6.01.00 release
This is a patch release on top of the 6.00.00 release to address below key features and bugs. Refer respective component release notes for details on the changes.
J721E Beta board support with Leo PMIC processor board
Support for TI MM RTOS decoder package consisting H.264 decoder (library and source package)
4 channel 3D Surround view demo using VISS, GPU, FPDLink 2MP Cameras, HDMI Display
AR233 sensor support
DSS BT601 discrete sync support in DSS RTOS driver
Improved stability and performance for Auto Valet Parking Demos
Critical bugs fixes related to stability seen in Ethernet and Imaging demos
EDP display interoperability issue and hot-plug-detect (HPD) support
This release in tested on the below HW platforms,
J721E SoC and J721E EVM
eDP output from J721E EVM
MMC/SD, eMMC, OSPI, UART, Ethernet from J721E EVM
Infotainment daughter card, required for HDMI display demos
Fusion1 with UB960 FPD link daughter card with 4x UB953-IMX390 FPD Link sensors, required for CSI2RX capture demos
GESI daughter card, required for some 8 port ethernet switch demos
Some of the key software features are listed below (already supported in earlier releases),
Linux on A72 and SysBIOS on R5F, C6x, C7x CPUs with IPC (inter-processor communication) working across all CPUs
RTOS based bootloader via SBL in PDK and Linux based bootloader via uboot in PSDK Linux Auto
PDK with CSI2, DSS, VPAC, DMPAC, UDMA, MMC/SD, UART, IPC, Ethernet, OSPI drivers
TIDL and MMALIB for CNN acceleration using C7x/MMA
TI OpenVX software stack running across A72, R5F, C6x, C7x CPUs in RTOS only mode as well as Linux+RTOS mode
TI OpenVX nodes for VPAC, DMPAC, CSI2 capture, display, TIDL, OpenGL and OpenVX v1.1 defined nodes
Imaging library for auto-exposure, auto-whitebalance algorithms, image sensor framework
8 port ethernet switch firmware
ADSA/Vision demos for CNN applications like object classification, parking spot detect, semantic segmentation, auto valet parking
ADSA/Vision demos for Camera applications like 1CH/4CH IMX390 CSI2 Capture + VISS + display
Gateway demos for CAN to ethernet routing
Display sharing and cluster demo applications
MCU SW for MCU island integration demos
MCAL AutoSAR drivers (part of MCU SW package)
VXLIB - OpenVX v1.1 low level kernel for C66x integrated with TIOVX
Perception toolkit (PTK) for Lidar,Radar,Camera fusion (PC based only)
TI Code generation tools for R5F, C6x, C7x
ARM GCC Code generation tools for A72 (needs to be downloaded separately)
4.10.2. Device Support and Validation Information¶
SoC |
Build Host (OS) |
Run Target (OS) |
Test Plaform |
---|---|---|---|
J721e |
x86_64 (Linux Ubuntu 18.04) |
R5F, C6x, C7x running TI-RTOS A72 running Linux |
J721e EVM with daughter cards |
PC emulation mode |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
x86_64 (Linux Ubuntu 18.04) |
4.10.3. Known Issues¶
Refer to component release notes for known issues in each component