50 #ifndef ICSSG_TIMESYNC_H_ 51 #define ICSSG_TIMESYNC_H_ 77 typedef enum IcssgTimeSync_ClkType_e
92 typedef struct IcssgTimeSync_Cfg_s
uint32_t syncOut_pwidth_WC
Definition: icssg_timesync.h:111
TimeSync configuration parameters.
Definition: icssg_timesync.h:92
uint32_t syncOut_start_WC
Definition: icssg_timesync.h:108
IcssgTimeSync_ClkType
ICSSG TimeSync clock types.
Definition: icssg_timesync.h:77
Definition: icssg_timesync.h:86
IcssgTimeSync_ClkType clkType
Definition: icssg_timesync.h:105
Definition: icssg_timesync.h:80
Definition: icssg_timesync.h:83
This file contains the type definitions and helper macros for the Enet Time Synchronization module in...
bool enable
Definition: icssg_timesync.h:102