65 #define ENET_CFG_TRACE_LEVEL_NONE (0U) 68 #define ENET_CFG_TRACE_LEVEL_ERROR (1U) 71 #define ENET_CFG_TRACE_LEVEL_WARN (2U) 74 #define ENET_CFG_TRACE_LEVEL_INFO (3U) 77 #define ENET_CFG_TRACE_LEVEL_DEBUG (4U) 80 #define ENET_CFG_TRACE_LEVEL_VERBOSE (5U) 83 #ifndef ENET_CFG_TRACE_TRACE_LEVEL 84 #define ENET_CFG_TRACE_TRACE_LEVEL (ENET_CFG_TRACE_LEVEL_INFO) 88 #define ENET_CFG_TRACE_FORMAT_FUNC (0U) 91 #define ENET_CFG_TRACE_FORMAT_FILE (1U) 94 #define ENET_CFG_TRACE_FORMAT_FULL (2U) 97 #ifndef ENET_CFG_TRACE_TRACE_FORMAT 98 #define ENET_CFG_TRACE_TRACE_FORMAT (ENET_CFG_TRACE_FORMAT_FUNC) Definition: enet_trace.h:117
Definition: enet_trace.h:135
Definition: enet_trace.h:124
EnetTrace_TraceLevel
Enumerates the types of trace level.
Definition: enet_trace.h:108
Definition: enet_trace.h:146
Definition: enet_trace.h:111
Definition: enet_trace.h:114