47 #ifndef ENET_MOD_STATS_H_ 48 #define ENET_MOD_STATS_H_ 66 #define ENET_STATS_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \ 67 ENET_IOCTL_STATS_BASE | \ 77 typedef enum EnetStats_Ioctl_e
EnetStats_Ioctl
Statistics IOCTL commands.
Definition: enet_mod_stats.h:77
#define ENET_STATS_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for STATS module.
Definition: enet_mod_stats.h:66
Print Stats registers.
Definition: enet_mod_stats.h:95
Get the hardware version of the Stats module.
Definition: enet_mod_stats.h:86
Get host port statistics.
Definition: enet_mod_stats.h:111
Get MAC port statistics.
Definition: enet_mod_stats.h:124
Reset host port statistics.
Definition: enet_mod_stats.h:138
Reset MAC port statistics.
Definition: enet_mod_stats.h:149
This file contains the type definitions and helper macros for the Enet Module interface.