47 #ifndef ENET_MOD_HOSTPORT_H_ 48 #define ENET_MOD_HOSTPORT_H_ 67 #define ENET_HOSTPORT_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \ 68 ENET_IOCTL_HOSTPORT_BASE | \ 78 typedef enum EnetHostPort_Ioctl_e
219 typedef enum EnetHostPort_IngressPriorityType_e
Get VLAN priority regeneration map.
Definition: enet_mod_hostport.h:150
Get MRU and MTU.
Definition: enet_mod_hostport.h:204
Disable ingress traffic shaping configuration.
Definition: enet_mod_hostport.h:186
Definition: enet_mod_hostport.h:222
Get ingress DSCP priority (TOS) map.
Definition: enet_mod_hostport.h:132
Print host port registers.
Definition: enet_mod_hostport.h:96
This file contains the type definitions and helper macros that are common for host and MAC ports.
Enable host port.
Definition: enet_mod_hostport.h:105
Check if checksum offload is enabled.
Definition: enet_mod_hostport.h:213
Get QoS egress priority map.
Definition: enet_mod_hostport.h:168
EnetHostPort_IngressPriorityType
Port priority type.
Definition: enet_mod_hostport.h:219
EnetHostPort_Ioctl
Host port IOCTL commands.
Definition: enet_mod_hostport.h:78
Definition: enet_mod_hostport.h:225
Get ingress traffic shaping configuration.
Definition: enet_mod_hostport.h:195
Enable ingress traffic shaping configuration.
Definition: enet_mod_hostport.h:177
Get the hardware version of the host port module.
Definition: enet_mod_hostport.h:87
Set VLAN priority regeneration map.
Definition: enet_mod_hostport.h:141
Set ingress DSCP priority (TOS) map.
Definition: enet_mod_hostport.h:123
This file contains the type definitions and helper macros for the Enet Module interface.
#define ENET_HOSTPORT_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for host port module.
Definition: enet_mod_hostport.h:67
Set QoS egress priority map.
Definition: enet_mod_hostport.h:159
Disable host port.
Definition: enet_mod_hostport.h:114