![Logo](ti_logo.png) |
PDK API Guide for J721E
|
Go to the documentation of this file. 63 #define ENET_CFG_IS_ON(name) ((ENET_CFG_ ## name) == ENET_ON) 66 #define ENET_CFG_IS_OFF(name) ((ENET_CFG_ ## name) == ENET_OFF) 73 #define ENET_CFG_PRINT_BUF_LEN (200U) 76 #define ENET_CFG_HAS_DEFAULT_OSAL (ENET_ON) 79 #define ENET_CFG_HAS_DEFAULT_UTILS (ENET_ON) 82 #define ENET_CFG_SANITY_CHECKS (ENET_ON) 85 #define ENET_CFG_ENETPHY_PHY_MAX (13U) 92 #if defined(SOC_TPR12) || defined(SOC_AWR294X) 93 #define ENET_CFG_CPSW_SGMII (ENET_OFF) 95 #define ENET_CFG_CPSW_SGMII (ENET_ON) 99 #define ENET_CFG_CPSW_INTERVLAN (ENET_ON) 102 #define ENET_CFG_MDIO_CLAUSE45 (ENET_ON) 105 #define ENET_CFG_CPSW_HOSTPORT_TRAFFIC_SHAPING (ENET_ON) 108 #define ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE (128U) 111 #define ENET_CFG_CPSW_MACPORT_TRAFFIC_SHAPING (ENET_ON) 114 #if defined(SOC_TPR12) || defined(SOC_AWR294X) 115 #define ENET_CFG_CPSW_MACPORT_SGMII (ENET_OFF) 117 #define ENET_CFG_CPSW_MACPORT_SGMII (ENET_ON) 121 #define ENET_CFG_CPSW_MACPORT_INTERVLAN (ENET_ON) 124 #define ENET_CFG_CPSW_CPTS_STATS (ENET_ON) 127 #define ENET_CFG_CPSW_CPTS_EVENTS_POOL_SIZE (128U) 130 #if !defined(SOC_AM65XX) 132 #define ENET_CFG_TX_CHANNELS_NUM (8U) 135 #define ENET_CFG_RX_FLOWS_NUM (8U) 138 #define ENET_CFG_RING_MON_NUM (4U) 142 #define ENET_CFG_REMOTE_CLIENT_CORES_MAX (6U) 145 #define ENET_CFG_RM_MAC_ADDR_MAX (10U) 148 #define ENET_CFG_RM_TX_CH_MAX (8U) 151 #define ENET_CFG_RM_RX_CH_MAX (64U) 154 #if defined(SOC_TPR12) || defined(SOC_AWR294X) 155 #define ENET_CFG_RM_PRESENT (ENET_OFF) 156 #elif defined(SOC_J721E) || defined(SOC_J7200) || defined(SOC_AM65XX) 157 #define ENET_CFG_RM_PRESENT (ENET_ON) 159 #error "SOC not supported" 162 #if defined(SOC_AM65XX) 165 #define ENET_CFG_NUM_INSTANCES (7U) 166 #define ENET_CFG_TX_CHANNELS_NUM (4U * ENET_CFG_NUM_INSTANCES) 167 #define ENET_CFG_RX_FLOWS_NUM (8U * ENET_CFG_NUM_INSTANCES) 168 #define ENET_CFG_RING_MON_NUM (8U * ENET_CFG_NUM_INSTANCES) 171 #if defined(SOC_J721E) || defined(SOC_J7200) 172 #define ENET_CFG_LWIP_IFACE_MAX (2U) 174 #define ENET_CFG_LWIP_IFACE_MAX (1U)