43 #include <ti/csl/tistdtypes.h> 54 #define TRUE ((Bool) 1) 55 #define FALSE ((Bool) 0) 94 #define CSL_PASS ( (int32_t) (0)) 95 #define CSL_EFAIL (-(int32_t) (1)) 96 #define CSL_EBADARGS (-(int32_t) (2)) 97 #define CSL_EINVALID_PARAMS (-(int32_t) (3)) 98 #define CSL_ETIMEOUT (-(int32_t) (4)) 99 #define CSL_EOUT_OF_RANGE (-(int32_t) (5)) 100 #define CSL_EUNSUPPORTED_CMD (-(int32_t) (6)) 101 #define CSL_EUNSUPPORTED_OPS (-(int32_t) (7)) 102 #define CSL_EALLOC (-(int32_t) (8)) 107 #define NULL ((void*)0) 111 #if defined (HOST_EMULATION) 117 #define NULL_PTR (NULL) 119 #define NULL_PTR ((void *)0) 132 #define STW_SOK (CSL_PASS) 133 #define STW_EFAIL (CSL_EFAIL) 134 #define STW_EBADARGS (CSL_EBADARGS) 135 #define STW_EINVALID_PARAMS (CSL_EINVALID_PARAMS) 136 #define STW_ETIMEOUT (CSL_ETIMEOUT) 137 #define STW_EOUT_OF_RANGE (CSL_EOUT_OF_RANGE) 138 #define STW_EUNSUPPORTED_CMD (CSL_EUNSUPPORTED_CMD) 139 #define STW_EUNSUPPORTED_OPS (CSL_EUNSUPPORTED_OPS) Uint16 CSL_BitMask16
Definition: csl_types.h:63
unsigned long long int CSL_Uint64
Definition: csl_types.h:74
int32_t CSL_ErrType_t
CSL error type.
Definition: csl_types.h:84
volatile Uint16 CSL_Reg16
Definition: csl_types.h:67
Int16 CSL_ModuleId
Definition: csl_types.h:59
Uint32 CSL_Xio
Definition: csl_types.h:60
volatile Uint8 CSL_Reg8
Definition: csl_types.h:66
Int16 CSL_Uid
Definition: csl_types.h:58
Definition: csl_types.h:79
volatile Uint32 CSL_Reg32
Definition: csl_types.h:68
Definition: csl_types.h:80
Uint32 CSL_BitMask32
Definition: csl_types.h:64
Int16 CSL_InstNum
Definition: csl_types.h:71
Uint8 CSL_BitMask8
Definition: csl_types.h:62
Int16 CSL_ChaNum
Definition: csl_types.h:72
Int16 CSL_Status
Definition: csl_types.h:70
CSL_OpenMode
CSL open mode.
Definition: csl_types.h:78