2.1. Release Notes - 08_00_00¶
2.1.1. Introduction¶
This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
2.1.2. What’s New¶
ID | Description | Module | Supported Platforms |
---|---|---|---|
PDK-9782 | PDK OSAL: Support for SW Timer, Mailbox, Mutex, Heap and Load modules | OSAL | J721E, J7200, AM65xx |
PDK-9369 | PDK OSAL Support for FreeRTOS on R5F | OSAL | J721E, J7200, AM65xx |
JACINTOREQ-1429 | PDK R5F Drivers Migration to support FreeRTOS | ALL | J721E, J7200, AM65xx |
PDK-9679 PDK-9678 | Uniflash Update for XIP Flow and XIP Flashing Flow update | COMMON | J721E, J7200, AM65xx |
JACINTOREQ-1212 | Enet LLD: Integrate open source LWIP TCP/IP stack | Enet | J721E, J7200, AM65xx |
ID | Description | Module | Supported Platforms |
---|---|---|---|
PDK-9541 | DDR Boot Time Optimizations | BOARD | J721E, J7200 |
PDK-6879 | WA for DDR: VRCG high current mode must be used during LPDDR4 CBT | BOARD | J721E, J7200 |
ID | Description | Module | Supported Platforms |
---|---|---|---|
PDK-9355 | FreeRTOS Support on C6x for CPU | OSAL,COMMON | J721E |
PDK-9323 | DSS M2M: Scaling | DSS | J721E |
PDK-9322 | DSS M2M: Multi-Channel Support | DSS | J721E |
PDK-5200 | FlexConnect: Memory -> VISS -> MSC -> Memory (YUV420) | VHWA | J721E |
PDK-8778 | Keywriter - PDK SBL example application | SBL, SECURITY | J721E |
2.1.3. Upgrade and Compatibility¶
2.1.3.1. FreeRTOS¶
See FreeRTOS Chapter for more details.
2.1.3.2. lwIP¶
This release introduces lwIP TCP/IP stack support for J721E on R5F cores. lwIP is supported and validated with FreeRTOS, it’s not supported on TI-RTOS (SysBIOS).
Enet LLD implements the lwIP driver interface which enables lwIP stack to run transparently on top of the Ethernet peripherals supported by Enet driver. Enet LLD provides a lwIP example application which showcases lwIP integration on peripherals supported by Enet driver, where user can run tests such as ping, UDP/TCP echo and iperf. This example supports DHCP and static IP. For more information, see Enet LLD examples section.
lwIP stack is enabled for CPSW_2G and CPSW_9G.
This is the last release with TI NDK TCP/IP stack support. Enet LLD NIMU example has been validated as well on supported cores in this release. TI NDK stack support will be scoped out starting from next release.
2.1.3.3. OSAL¶
As part of FreeRTOS Migration, following new OSAL modules are added
- ClockP <= SW Timer
- MailboxP <= Software Mailbox
- MutexP <= Mutex
- HeapP <= For creating arbitrary heaps
- LoadP <= Task / CPU Load measurement [FreeRTOS Only]
Also following are the updates for existing OSAL modules.
- EventP
- New API EventP_wait()
- EventP_pend() supports only SysBIOS. This will be obsolete in next release. Migrate to new similar API EventP_wait()
- QueueP
- Header file is renamed to QueueP.h from Queue.h
- Following OSAL Queue APIs supports only SysBIOS and will be obsolete in next release. Migrate to new QueueP APIs
Old API New API Osal_Queue_Handle QueueP_Handle Osal_Queue_Elem QueueP_Elem -NA- QueueP_Params -NA- QueueP_Params_init Osal_Queue_construct + Osal_Queue_handle QueueP_create -NA- QueueP_delete Osal_Queue_put QueueP_put Osal_Queue_get QueueP_get Osal_Queue_empty QueueP_isEmpty
2.1.3.4. DDR¶
DDR Boot time(initialization + training) is optimized in this release and is now in the range of ~35 ms.
This includes:-
- DDR Register Settings updates and
- Disabled DDR Register write verification, given there is DDR inline ECC. (Support for register Verification post init/training will be provided in future release.)
Priming of DDR for ECC is now optimized by usage of UDMA.
Following in PDK_INSTALL_DIR/packages/ti/board/src/j721e_evm/include/board_cfg.h can be modified as per the user requirement.
/* Note with ECC enabled, all memory is not usable: 1/8 memory used for inline ECC */ #define BOARD_DDR_ECC_END_ADDR (0xF1FFFFFFU) /* Enable/Disable DDR Memory Prime for ECC. Define the following macro to enable. */ #undef BOARD_DDR_ENABLE_DDR_MEM_PRIME
2.1.3.5. XIP¶
A new twin appimage bootflow has been introduced. There is one appimage for RAM sections and one appimage for xip sections.
- For each CPU, the compiler+linker toolchain is used to create the application .out “ELF” file which can be loaded and run via CCS
- The below “post build” steps are then used to convert the application .out into a “flash” friendly format - For each CPU, out2rpc is used to convert the ELF .out to a binary file containing only the loadable sections. This is called a RPRC file. - For each CPU, xipGen is used to split this RPRC file into two RPRC files. - One RPRC, containing the section that during boot need to be loaded to RAM - Second RPRC, containing the section that during boot are not loaded to RAM but are instead “eXecuted In Place”, i.e XIP - multiCoreGen is then used to combine all the non-XIP RPRC files per CPU into a single .appimage file which is a concatenation of the individual CPU specific RPRC files. - multiCoreGen is used again to combine all the XIP RPRC files per CPU into a single .appimage_xip file which is a concatenation of the individual CPU specific RPRC XIP files.
- This .appimage and .appimage_xip is then flashed to the EVM using Uniflash
- Upon booting, the SBL interpets the .appimage and loads the RAM sections into respective memory.
- The .appimage_xip contains the sections that are executed in place.
See XIP Programming Guide for more details.
2.1.3.6. SMP mode¶
- SMP Support is de-scoped and PDK Examples will not support execution in SMP mode
2.1.3.7. Board Diagnostics¶
- Board diagnostics stress test is not supported
2.1.3.8. PCIe, USB¶
- PCIE and USB Support is removed for J721E.
2.1.4. Device Support¶
J721E EVM SR1.0 and SR1.1, J721E-HS EVM (BOARD=j721e_evm)
Associated TIFS versions:
TIFS name J721E SR revision tifs.bin SR1.0 & SR1.1 GP tifs-hs-enc.bin SR1.0 HS tifs-sr1.1-hs-enc.bin SR1.1 HS
2.1.5. Validation Information¶
For details on the validated examples refer to the platform specific test report available here.
2.1.6. Tool Chain Information¶
Component | Version |
---|---|
FreeRTOS Kernel | 10.4.3 |
Sys Bios | 6_83_02_07 |
XDC Tools | 3_61_04_40_core |
lwIP stack | 2.1.2 |
lwIP-contrib | 2.1.0 |
Network Development Kit (NDK) | 3_80_00_19 |
Network Services for NDK (NS) | 2_80_00_17 |
TI ARM R5F code generation tools | 20.2.0.LTS |
PRU code generation tools | 2.3.3 |
GCC ARM code generation tools | ARCH64 9.2-2019.12 |
CGT XML Processing Scripts | 2.61.00 |
System Analyzer (UIA Target) | 2_41_00_01 |
Component | Version |
---|---|
TI C6x code generation tools | 8.3.7 |
TI C7x code generation tools | 1.4.2.LTS |
2.1.7. Change Request¶
ID | Head Line | Original Fix Version | New Fix Version |
---|---|---|---|
JACINTOREQ-1518 | PDK: R5 SafeRTOS CPU support descope | 08.00.00 | 08.01.00 |
JACINTOREQ-1441 | PDK: C7x FreeRTOS CPU support descope | 08.00.00 | 08.01.00 |
JACINTOREQ-1504 | PDK: PCIE and USB Descope for J721E | 08.00.00 | None |
2.1.8. Fixed Issues¶
ID | Head Line | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
PDK-10131 | [McSPI] Incorrect input clock in example | McSPI | 07.03.00 | J721E, J7200 |
PDK-9437 | Increase in Boot time when DDR ECC is enabled | Board | 07.02.00 | J721E, J7200 |
PDK-9426 | ECAP CSL Capture Event Counter Reset Function Fails | CSL | 07.03.00 | J721E, J7200 |
PDK-6793 | osal - semaphore should not be used for mutex | OSAL | 06.02.00 | J721E, J7200 |
PDK-9594 | UDMA: Event Disable and Enable Failure for shared events | UDMA | 07.03.00 | J721E, J7200, AM65xx |
PDK-10315 | [SBL]: SBL does not set NB priorities for the HS device | SBL | 07.03.00 | J721E-HS, J7200-HS |
ID | Head Line | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
PDK-10304 | Using RPMessage_recvNb() causes Mutex Overflow | IPC | 07.01.00 | J721E |
PDK-9873 | [CSIRX]: Incorrect condition check when starting the stream | CSIRX | 07.03.00 | J721E |
PDK-9759 | [Board]: SciClient_init from Board_init should not application SciClient_init configuration | Board | 07.03.00 | J721E |
PDK-9756 | [CSITX]: Incorrect DPHY instance used in the driver | CSITX | 07.03.00 | J721E |
PDK-9694 | [CSITX]: CSITX supports only 4 lane speeds | CSITX | 07.03.00 | J721E |
PDK-9681 | [DSS CSL-FL]DSS displays corrupted data OR w/o colors on the screen | DSS | 07.03.00 | J721E |
PDK-9677 | Interrupt mode in sciclient is not working on HS Device | SciClient | 07.01.00 | J721E |
PDK-9673 | csl: serdes: invertTXPolarity not set by CSL_serdesLaneEnable() | CSL | 07.01.00 | J721E |
PDK-9456 | I2C Driver does not return error when camera/client is not available on the I2C bus | I2C | 07.02.00 | J721E |
PDK-9433 | MASTER _BYPASS bit in PHY_MASTER_CONTROL should be controlled based on the clock | OSPI | 07.02.00 | J721E |
PDK-9376 | [SciClient]Clock Source Macros are missing for odd numbered GP Timers | SciClient | 07.01.00 | J721E |
PDK-8848 | pixel clock for HDMI is fixed/hardcoded | DSS | 07.01.00 | J721E |
PDK-8653 | CSI2-RX: Stream FIFO Overflow observed for 4 channel input with FrameSync | CSIRX | 06.02.00 | J721E |
PDK-8600 | SBL optimizations for OSPI boot mode | SBL | 07.00.00 | J721E |
PDK-6992 | [DSS]: Support for BT 601 requires additional patch | DSS | 07.00.00 | J721E |
PDK-5224 | Active DP -> HDMI adapter doesn’t work | DSS | 00.03.00 | J721E |
2.1.9. Known Issues¶
ID | Head Line | Module | Reported in Release | Affected Platforms | Impact | Workaround in this release |
---|---|---|---|---|---|---|
PDK-6975 | Pulsar (R5F) : High priority interrupt is missed by VIM | CSL, OSAL | 07.00.00 | J721E, J7200, AM65xx | Baremetal implementation is pending | Use SYSBIOS instead of baremetal |
PDK-8320 | ICSS V1 CSL not up to date with ICSSG | CSL | 07.00.00 | J721E, AM65xx | None | Patch available. Will be included in next release |
PDK-9676 | UART : Potential interrupt storm | UART | 07.02.00 | J7200, J721E | Error interrupt resulting in hang. | None |
PDK-8601 | CSL ECC test application fails on J721E and J7200 | CSL | 07.01.00 | J721E, J7200 | None | None |
PDK-9696 | [SPI] DMA mode does not work for SPI5 | McSPI | 07.01.00 | J721E | Cannot use DMA with SPI5 | Disable DMA for SPI5 OR use another instance of SPI |
PDK-9571 | [SPI] Transfer stalls when transfer length is not multiple of FIFO length in DMA mode | McSPI | 07.02.00 | J721E | Cannot transfer data if data size is not multiple of FIFO length in DMA mode | Use transfer size in multiple of FIFO length |
PDK-9947 | [CSIRX]: hangs is observed when re-running example with different number of channels | CSIRX | 07.03.00 | J721E | Unable to re-run application with different number of cameras | Power-cycle the board before reloading the application next time |
PDK-8407 | J721E: MCU Timer 0 is not usable from application (sysbios) with SBL | OSAL, SBL | 07.01.00 | J721E | None | Use any other timer |
PDK-8300 | UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader. | UDMA | 07.01.00 | J721E | Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader. | Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5. |
PDK-6789 | MCU/Main NAVSS UDMA memcpy from L2SRAM fails | UDMA | 07.00.00 | J721E | Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location | Use ring memory from non-L2SRAM location |
PDK-6549 | MCU2 core diagnostic tests not running through sbl | BOARD | 07.00.00 | J721E | None | Use CCS/JTAG to run the tests |
PDK-6548 | Display port (eDP) diagnostic test failure | BOARD | 07.00.00 | J721E | None | Use display sample application |
PDK-5228 | Output mismatch when each region requiring 3 TRs | VHWA | 01.00.00 | J721E | In multi-region mode with more then 3 TR per region can’t be used | In multi-region mode for each region less than 3 TR should be used |
ETHFW-1843 | mcu1_0: Exception in NIMU example in SD card boot | ENET | 08.00.00 | J721E | Affects SD card boot of mcu1_0 TI-RTOS image | Another timer instance can be used |
ETHFW-1845 | examples: MAC loopback app test causes abort in debug mode during restart | ENET | 08.00.00 | J721E | Impacts only ‘debug’ example app | None |
PDK-9528 | SBL prebuild binary for J721E HS doesn’t work from package | SBL | 07.03.00 | J721E-HS | None | Cleanup the SBL library and re-build the SBL image for HS. Commands: - Clean sbl_lib_uart (make sbl_lib_uart_clean) - Build for HS (make -sj sbl_uart_img_hs) |
PDK-10292 | Sciclient Firewall Testapp Fails on HS Device | SCICLIENT | 07.03.00 | J721E-HS | None | None |
2.1.10. Limitations¶
2.1.10.1. PDK¶
- PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.
2.1.10.2. ENET¶
- lwIP stack integration doesn’t support checksum hardware-offload feature.
- ICSSG integration with lwIP and NDK is done only for ICSSG Dual-MAC. Driver level support is available for Dual-MAC and Switch.
- TimeSync PTP integration is done only for ICSSG-Dual MAC.
- TimeSync is possible only in one MAC port at a time.
- Different VLAN modes are not supported in Dual-MAC mode (within given ICSSG MAC ports). Both MACs should either be in VLAN aware or VLAN unaware mode.
- Independent VLAN learning is not supported in Dual-MAC mode.