| Makefile flag | Valid values (default value in bold) | Description |
|---|---|---|
| PROFILE | debug or release or all | "debug" for debug only build, "release" for release only build, "all" for both debug and release builds |
| BUILD_TARGET_MODE | yes or no | "yes" to build for SoC platform. In case you are building only for PC keep this to "no" |
| BUILD_QNX_A72 | yes or no | "yes" if you want to build for QNX on A72. In case you are building for RTOS only mode or Linux + RTOS mode, keep this to "no" |
| BUILD_LINUX_A72 | yes or no | "yes" if you want to build for ARM Linux on A72. In case you are building for RTOS only mode or QNX + RTOS mode, keep this to "no" |
| BUILD_EMULATION_MODE | yes or no | "yes" to build for PC emulation mode. In case you are building only for SoC keep this to "no" |
| BUILD_CT_* | yes or no | "yes" to enable OpenVX conformance tests for specific group of tests (CT). Typically during development one would keep all to "no" and only enable the required tests in respective CT "test_main.h" |
| Makefile flag | Valid values (default value in bold) | Description |
|---|---|---|
| BUILD_CPU_<cpu name> | yes or no | "yes" if you want that CPU in your build, else keep it to "no". Note, BUILD_CPU_MPU1, BUILD_CPU_MCU2_0 MUST be kept as "yes" Note, If building for MCU1_0, please refer to the developer note here. Note, if switching between building with BUILD_CPU_MCU1_0 turned on and off, you will need to re-install the bootfs and targetfs to the SD card as described here Step 1: Prepare SD card for boot (one time only). |
| BUILD_APP_TIRTOS_LINUX | yes or no | "yes" to build Linux+RTOS mode binaries for selected CPUs. Keep to "no" if you are not interested in Linux+RTOS binaries. By default this is set to BUILD_LINUX_A72 |
| BUILD_APP_TIRTOS_QNX | yes or no | "yes" to build QNX+RTOS mode binaries for selected CPUs. Keep to "no" if you are not interested in QNX+RTOS binaries. By default this is set to BUILD_QNX_A72 |
| File | #define | Description |
|---|---|---|
| app_cfg.h | ENABLE_IPC_<cpu name> | #undef these to disable a CPU from the system, #define to enable in the system Note, this must match the BUILD_CPU_<cpu name> vision_apps/vision_apps_build_flags.mak |
| app_cfg_mcu2_0.h | ENABLE_DSS_HDMI | #define this to enable HDMI display via Infotainment daughter card, make sure to #undef ENABLE_DSS_EDP and ENABLE_DSS_DSI as well; ethernet firmware must also be disabled by following these instructions How to disable ETHFW |
| app_cfg_mcu2_0.h | ENABLE_DSS_EDP | #define this to enable eDP display via base EVM, make sure to #undef ENABLE_DSS_HDMI and ENABLE_DSS_DSI as well. Issues have been reported when ethernet firmware is enabled and using certain eDP displays or using an eDP to HDMI adaptor. If issues are observed with an eDP display, try disabling ethernet firmware. Instructions can be found here How to disable ETHFW |
| app_cfg_mcu2_0.h | ENABLE_DSS_DSI | #define this to enable DSI display, make sure to #undef ENABLE_DSS_EDP and ENABLE_DSS_HDMI as well |
| app_cfg_mcu2_0.h | ENABLE_DSS | #undef this to disable display (both HDMI and eDP), if you don't have display panel or daughter card for display |