C6000 C/C++ Code Generation Tools v8.3.7 Release Notes
Table of Contents
- 1 Support Information
- 2 C++ 2014 support
- 3 Printf Support for Vector Data Types
- 4 Use of Vector Data Types no longer requires optimizer
- 5 Compiler Option –legacy
- 6 New Linker Feature: Using memory for multiple purposes
- 7 New Linker Option –ecc
- 8 New Function Inlining Control Pragmas
- 9 Bug related to restrict pointers fixed
1 Support Information
1.1 List of Resolved and Known Defects
Resolved defects
| ID | Summary |
|---|---|
| CODEGEN-7227 | Compiler incorrectly optimizes unsigned loop counter which wraps around |
| CODEGEN-7146 | Compiler loses conversion to size_t in length argument to memcpy |
| CODEGEN-7011 | Compiler intermittently fails with INTERNAL ERROR: optimizer experienced a segmentation fault |
| CODEGEN-6914 | Enum type with no enumerators fails to emit DW_AT_byte_size, crashes CCS |
| CODEGEN-6866 | Compiler computes wrong offset for structure member, causing CCS to display it incorrectly |
| CODEGEN-6810 | Parser failure with nested lambdas |
| CODEGEN-6783 | Ensure C std headers do not issue MISRA warnings |
| CODEGEN-6757 | Use of C++ lambda causes Dwarf debug information to be incorrect, and prevents debugging the code |
| CODEGEN-6581 | Optimizer fails with segmentation fault |
| CODEGEN-6476 | switch statement where controlling expression is C++ scoped enum with underlying type smaller than int crashes compiler unless optimization is used |
| CODEGEN-6452 | Initializing function objects causes compilation to take much longer |
| CODEGEN-6419 | Compiler may crash if two thread-local accesses in one function are separated by a function call |
| CODEGEN-6289 | Pointer to VLA 2D array computation in IF condition is double-adjusted and garbled |
| CODEGEN-6132 | pdd tool fails when program includes unused file |
| CODEGEN-6130 | deque push_back of structure larger than 64-bytes tries to write to invalid memory location |
| CODEGEN-6004 | OFD erroneously prints 0x<decimal> where hex was intended |
| CODEGEN-5986 | Compiler may crash when auto as return type of uninstantiated member function in template class resolves to template parameter |
| CODEGEN-5943 | Compiler may lose volatile qualifier in A->B->C when B and C are both volatile |
| CODEGEN-5905 | Linker command file option –define with pathname with many directory components leads to error: “source line too long” |
| CODEGEN-5903 | Using –openmp:device and an improperly-declared target variable causes C6000 compiler to fail with INTERNAL ERROR: acpia6x experienced a segmentation fault |
| CODEGEN-5843 | Use of –check_misra=14.10 causes non-MISRA related warning to be emitted |
| CODEGEN-5791 | C++ enum class with explicit type has some problems |
| CODEGEN-5778 | Duplicate definitions of ldexp and ldexpl |
| CODEGEN-5777 | Compiler schedules an M-unit instruction too soon after MPYSP2DP or MPYSPDP |
| CODEGEN-5623 | Makefile dependence generation (–preproc_dependency) should quote spaces in filenames |
| CODEGEN-5574 | Loop controlled by unsigned char counter iterates more than 255 times |
| CODEGEN-5569 | C++ constructor which uses volatile causes compiler to crash |
| CODEGEN-5563 | Checking for MISRA rule 20.1 causes macro redefinition to be ignored |
| CODEGEN-5533 | Loop with Cortex-R, -mf3, and DWARF debug leads to assembler error “defined differently in each pass” |
| CODEGEN-5527 | Local structure initialization is incorrectly optimized away |
| CODEGEN-5486 | Global constexpr class errors out when assigning to member data |
| CODEGEN-5450 | Compiler mistakenly parallelizes MPYSPDP with single-cycle write of its SP input |
| CODEGEN-5236 | Register allocation failure |
| CODEGEN-5164 | Under –speculate_loads=auto, linker creates zero-filled fill sections instead of reducing the size of the corresponding memory range |
| CODEGEN-5119 | Using #pragma RETAIN does not keep a static file level variable |
| CODEGEN-5040 | –c64p_dma_l1d_workaround is missing from 8.x compilers |
| CODEGEN-5033 | Functions in <string> incorrectly return NULL |
| CODEGEN-4931 | Applying attribute((used)) to static variable does not work |
| CODEGEN-4885 | See MISRA diagnostics when compiling stdio.h |
| CODEGEN-4700 | Incorrect diagnostic when using macro that comes from macro library |
| CODEGEN-4668 | Macro with temp label causes assembler to crash |
| CODEGEN-4634 | Use of stdarg.h va_start macro causes a write to the wrong local variable |
| CODEGEN-4621 | Remove COFF global linker symbols from documentation for ELF-only targets |
| CODEGEN-4600 | Warning when using pragma RETAIN with attribute((noinit)) |
| CODEGEN-4548 | Compiler manual incorrectly spells option –disable_software_pipelining. It is spelled –disable_software_pipeline. |
| CODEGEN-4525 | Unreachable code in linear assembly may lead to crash |
| CODEGEN-4113 | Assembler computes wrong result for expression 0x232800 % 0x10000 |
| CODEGEN-4078 | Linker takes over 5 minutes to finish |
| CODEGEN-3931 | Compiler crashes while handling 0 length array in zero sized struct |
| CODEGEN-3918 | Writing multiple input sections in one line unexpectedly changes how input sections are combined into output sections |
| CODEGEN-3797 | Documentation should state that users must use far keyword when declaring C/C++ data symbols defined by the linker |
| CODEGEN-3613 | Some vector types computations are not carried out |
| CODEGEN-2346 | Compiler produces incorrect code at -o2 optimization |
| CODEGEN-2286 | palign(8) of .init_array messes up __TI_INITARRAY_Limit address |
| CODEGEN-2113 | Hex utility mishandles space in directory name of output file |
| CODEGEN-1979 | Statements before declarations with no white space (aggravated by macros) may cause incorrect parser error |
| CODEGEN-1154 | ltoa definition conflicts with quasi-standard ltoa |
| CODEGEN-848 | Local struct with non-constant initializer treated as static scope variable |
| CODEGEN-260 | XML output needs encoding specification |
Open defects
| ID | Summary |
|---|---|
| CODEGEN-7337 | Compiler incorrectly issues remark: value copied to temporary, reference to temporary used |
| CODEGEN-6929 | Compiler generates many more single cycle NOP instructions |
| CODEGEN-6662 | C6000: callstack replicates caller function indefinitely when Step Into/Over |
| CODEGEN-6509 | Compiler error: no instance of function template matches the argument list |
| CODEGEN-6296 | Unexpectedly large loop-carried dependence bound in loop that touches struct containing array |
| CODEGEN-4942 | Conditional clause function call with GCC statement argument causes compiler crash |
| CODEGEN-1489 | lnk6x emits warnings about .tdata and .tbss when .TI.tls specification is present in a linker command file |
| CODEGEN-1013 | Array with many dimensions hangs parser |
| CODEGEN-793 | Ill advised enum scalar usage gets MISRA diagnostic, but similar usage of enum array does not |
| CODEGEN-792 | Array that is correctly initialized erroneously gets a MISRA diagnostic about size not being specified |
| CODEGEN-766 | Use of short form of options in C_OPTION may cause spurious warning |
| CODEGEN-750 | %#x should not prefix 0x to a zero value |
| CODEGEN-747 | Should reject certain unitless instructions in parallel with certain other instructions |
| CODEGEN-696 | Disassembler fails to disassemble DPINT DPTRUNC DPSP |
| CODEGEN-676 | C99 math.h macros not supported |
| CODEGEN-675 | C99 header file fenv.h not supported |
| CODEGEN-674 | isunordered not supported |
| CODEGEN-651 | Hex converter map file does not list all sections for RAM model program with initialized sections with .cinit records |
| CODEGEN-650 | Hex converter fails to process RAM model .cinit records for initialized sections |
| CODEGEN-633 | Floating point addition rounding error |
| CODEGEN-631 | pow(min, max) and pow(max, max) incorrect |
| CODEGEN-630 | global labels defined in .cproc region are discarded |
| CODEGEN-606 | When failing to place a section, include size of trampolines in error message |
| CODEGEN-581 | RTS float arithmetic functions rounding error |
| CODEGEN-367 | modf(-Inf, 1.0) with -mv6740 enters infinite loop |
| CODEGEN-322 | Structure is not initialized correctly when using -o2 or -o3 optimization |
| CODEGEN-292 | When building with -o2, compiler sometimes fails to complete compilation |
| CODEGEN-115 | compiler is scheduling use of A8 too early causing an incorrect branch |
| CODEGEN-104 | Linker gives misleading warning when dot expressions used in SECTION directive for .stack section |
| CODEGEN-63 | DWARF does not correctly represent variables stored in register pairs |
| CODEGEN-56 | Forward reference in .space generates an internal error |
| CODEGEN-30 | Compilers on PC will not work without TMP set |
1.2 Compiler Wiki
A Wiki has been established to assist developers in using TI Embedded Processor Software and Tools. Developers are encouraged to read and contribute to the articles. Registered users can update missing or incorrect information. There is a large section of compiler-related material. Please visit:
https://processors.wiki.ti.com/index.php?title=Category:Compiler
1.3 Compiler Documentation
The “TMS320C6000 Optimizing Compiler User’s Guide” can be downloaded from:
https://www.ti.com/tools-software/compilers/download.html
Navigate to the C6000 Code Generation Tools section to view the user guide in HTML or PDF format.
1.4 TI E2E Community
Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The Code Composer Studio support forum can be found at:
http://e2e.ti.com/support/tools/ccs/f/81
1.5 Defect Tracking Database
Issues filed against the TI compilers can be searched in the Code Generation Tools Defect Database.
2 C++ 2014 support
As of v8.3, the compiler supports the C++14 version of the C++ standard. C++03 is no longer supported. See the C++14 Standard ISO/IEC 14882:2014. For a description of unsupported C++ features, see Section 7.2 of the “TMS320C6000 Optimizing Compiler User’s Guide”.
The move to C++14 will break ABI compatibility with previous C++ RTS releases. Attempting to link old C++ object code with the new RTS will result in a link-time error. Suppressing this error will likely result in undefined symbols or undefined behavior during execution.
C ABI compatibility will not be affected by this change.
In most cases, recompiling old source code with the new RTS should be safe. However, due to the changes made in the language, some constructs will result in syntax errors. Some common issues include:
- Macro expansion immediately adjacent to string literals may fail due to the inclusion of new string literals and literal suffixes. Ex: u8“def” will fail to compile if ‘u8’ is a macro “def”_x will fail to compile if ’_x’ is a macro
- New keywords: alignas, alignof, char16_t, char32_t, constexpr, decltype, noexcept, nullptr, static_assert, and thread_local
- The auto keyword has been repurposed and is no longer a valid storage class specifier. Similarly, the register keyword has been deprecated and will be removed in the future.
A full list can be found in Appendix C, section 2 of the C++14 standard.
3 Printf Support for Vector Data Types
As of v8.3, the printf() function included it the RTS supports vector data types. The convention set by OpenCL 1.2 as documented in Section 6.12.13 of the OpenCL 1.2 standard is followed with one exception. This exception is to do with use of ll instead of l in the format string for longlong vector conversions.
Example:
float4 f = (float4)(1.0f, 2.0f, 3.0f, 4.0f); uchar4 uc = (uchar4)(0xFA, 0xFB, 0xFC, 0xFD);
printf(“f4 = %2.2v4hlf\n”, f); printf(“uc = %#v4hhx\n”, uc);
/* Output: */ f4 = 1.00,2.00,3.00,4.00 uc = 0xfa,0xfb,0xfc,0xfd
4 Use of Vector Data Types no longer requires optimizer
Usage of vector data types previously required the optimizer. As of v8.3, use of the optimizer is no longer required i.e. the –vectypes option can be used without specifying a -o[0-3] option.
5 Compiler Option –legacy
As of the 8.2.2 release, a compiler option, –legacy, has been added. When legacy code bases tuned for C6000 CGT v7.4.x or older exhibit performance degradations (cycles or code size) with later compiler versions, this option may help. Do not use this option in new applications. Any new features added to newer tool chains will not be available when the –legacy option is used.
6 New Linker Feature: Using memory for multiple purposes
As of v8.3, this feature enables overlaying an initialized section with the same load and run address with other sections that have separate load and run addresses.
One way to reduce memory required is to use the same range of memory for multiple purposes. It is possible to use a range of memory at first for system initialization and startup. Once that phase is complete, the same memory can then be repurposed as a collection of uninitialized data variables, or a heap. To implement this scheme, use the variation of UNION which allows one section to be initialized, and the remaining sections to be uninitialized.
Generally, an initialized section (one with raw data, such as .text) in a union must have its load allocation separately specified. However, one and only one initialized section in a union can be allocated at the union’s run address. By listing it in the union with no load allocation at all, it will use the union’s run address as its own load address.
For example:
UNION run = FAST_MEM
{ .cinit .bss }
.cinit is an initialized section. It will be loaded into FAST_MEM at the run address of the union. .bss is an uninitialized section. Its run address will also be that of the union.
7 New Linker Option –ecc
In previous versions, linker generated ECC has been enabled via an ECC specifier on memory ranges in the linker command file. This makes it difficult for TI to provide linker command files with ECC specified because users need the ability to enable/disable the support.
Starting with v8.3, users can enable/disable ecc support via the –ecc=[on|off] linker option. Existing users of ECC will need to specify –ecc=on
8 New Function Inlining Control Pragmas
Three new pragmas to control function inlining were added in this version:
a) The FORCEINLINE pragma will force functions to be inlined in the annotated statement i.e., it has no effect on those functions in general, only on function calls in a single statement.
b) The FORCEINLINE_RECURSIVE pragma will force inlining not only of calls visible in the statement, but also in the inlined bodies of calls from that statement.
c) The NOINLINE pragma prevents calls within a single statement from being inlined. (NOINLINE is the inverse of the FORCEINLINE pragma.)
9 Bug related to restrict pointers fixed
A bug that could propagate a restrict pointer into a disjoint scope (e.g., an inlined function) and make a wrong decision about memory disambiguation was fixed.
The fix may cause performance degradations when a restrict pointer is passed into an inlined function.
Based on the definition of ‘restrict’, ‘restrict’ means within the scope of the declaration of a pointer P. Only P or expressions based on P will be used to access the object or sub-object pointed to by P. A pointer copy of another restrict pointer can inherit the restrictness only when they are in the same scope or nested scopes.
For example:
int x[100]; void test() { int restrict p1; int restrict p2;
p1 = x; p2 = x+1;
foo(p1); bar(p2); }
void foo(int* r1) { *(r1+1) = 0; return; }
void bar(int* r2) { *r2 = 1; return; }
After inlining foo() and bar(), we have:
void test() { int restrict p1; int restrict p2;
p1 = x; p2 = x+1;
{// inlined function f00() int r1 = p1; (r1+1) = 0; }
{// inlined function bar() int r2=p2; r2 = 1; } }
Previous versions of the compiler might propagate p1 and p2 for r1 and r2, and incorrectly determine that (r1+1) and r2 do not alias.
This fix may cause performance degradations when pointers in disjoint scopes actually do not access the same memory locations, because the compiler has to assume that alias exists.