Jacinto 7 TIDL Release Notes
Version: 01.03.00
Contents
- Introduction
- Licensing
- What's New
- Documentation
- Upgrade and Compatibility Information
- Device Support
- Validation Information
- Fixed Issues
- Known Issues
- Technical Support
- Package Versioning
Introduction
The package consists of the Texas Instruments J7 TIDL Software
Licensing
The licensing information of this library, as well as any third-party components included which are made available under a number of other open-source licenses are enumerated as part of the manifest. Note : Below Links would work only after installing the package
Documentation
1 | User's Guide | [HTML] |
3 | Software Manifest | [HTML] |
What's New
Here are a few of the new features supported in this release:
- Added NEO-AI-DLR support
- TVM model compliation for heterogeneous execution (ARM+C7x-MMA)
- Standalone test application is moved to Linux. CCS based testing is deprecated
- Added support for below layers
- Sigmoid layer
- Standalone Pad layer
- Color conversion (YUV420SP to RGB) Layer
- Depth to Space (Pixel Shuffle) Layer
- Optimized Object detection Post Processing Layer
- Improved Post Training Quantization
- Channel wise quantization support for Depth wise convolution layers
Upgrade and Compatibility Information
NA
Device Support
Target SoC | Target Plaform | Build environment (OS) | Target environment (OS) |
J721E EVM | x86_64 Linux PC | x86_64 (Linux) | NA |
J721E EVM | x86_64 Windows PC | x86_64 Windows | NA |
Validation Information
This release was built and validated using the following tools:
Dependencies (included in Processor SDK RTOS Automotive):
- ivision - 01_00
- MMALIB - 01_03_00_06
- PDK - CORE SDK 7.1
- C7x CGT - ti-cgt-c7000_1.4.0.LTS
Dependencies (NOT included in Processor SDK RTOS Automotive):
- Microsoft Visual Studio Verison 14.2
- GCC version 5.4.0 (In Ubuntu 18.04)
- OpenCV: 3.1.0 (for Test bench Only)
- Protobuf: 3.5.1 (for Import tool only)
- flatbuffers : 1.11.0(for Import tool only)
Fixed Issues
ID | Description | Module | Affected Versions | Affected Platforms |
---|---|---|---|---|
TIDL-887 | NC: Returning Error code 10 with given network | TOOL | 01.01.00 | J721E |
TIDL-912 | 16-bits Conv layer 3x3 stride 2 fails in customer network, issue shows up in natc | COMPUTE | 01.02.00 | J721E |
TIDL-964 | strideOffset not being set correctly in case of zero padding for a layer | TOOL | 01.02.00 | J721E |
TIDL-1053 | Small weight range results into accuracy drop | TOOL | 01.02.00 | J721E |
TIDL-1143 | Softmax layer : CI and Reference output's are not matching | COMPUTE | 01.02.00 | J721E |
TIDL-1152 | Pooling : Reference output is not matching NATC output | COMPUTE | 01.02.00 | J721E |
TIDL-1153 | Concat Layer is writing more than required when output goes to DDR | COMPUTE | 01.02.00 | J721E |
TIDL-1172 | Inner Product layer stuck on Target | COMPUTE | 01.02.00 | J721E |
TIDL-1174 | Mismatch in Concat Layer for Large feature map case | COMPUTE | 01.02.00 | J721E |
TIDL-1180 | Max Pooling layer result is wrong | COMPUTE | 01.02.00 | J721E |
Known Issues
ID | Description | Module | Reported in Release | Affected Platforms | Occurrence | Workaround in this release |
---|---|---|---|---|---|---|
TIDL-864 | Concat trace dump mismatch between REF & CN/CI | COMPUTE | 01.02.00 | J721E | Rare | NA |
TIDL-1188 | Strong accuracy degradation on 16-bit compared to 8-bit with model containing LeakyReLU | COMPUTE | 01.02.00 | J721E | Rare | Disable Bias in convolution layer |
TIDL-1197 | Model execution order for a branch is not optimal | COMPUTE | 01.02.00 | J721E | Rare | No fucntional issue, Only Performance drop would be obsrved |
Technical Support
For technical support, please post your questions on TI E2E Forum for Automotive ADAS SoCs.
For additional assistance, contact local TI Field Application Engineer
Package Versioning
Each package version is composed of 4 period-delimited numbers - represented here by the letters M, m, p and b [M.m.p.b]
. The table below provides a descriptive reference regarding package version numbering.
Digit | Meaning | Description |
---|---|---|
1 (M=Major) | Major revision | Incremented when the new version is substantially different from the previous For example, a new module added or an existing module's algorithm significantly altered. |
2 (m=minor) | Minor revision | Incremented when the new version has changed but not in a major way. For example, some minor changes in the API or feature set. |
3 (p=patch) | Patch number | Incremented for all other source code changes. This include any packaging support code. |
4 (b=build) | Build number | Incremented for each release delivery to CM. Reset for any change to M, m or p |
Copyright 2018, Texas Instruments Incorporated