2. Getting Started¶
2.1. Build from Source¶
Important
To run many of the demos in this SDK, the companion HLOS package also needs to be download separatly; either Processor SDK Linux or Processor SDK QNX.
Refer below table to get started with topic of your interest.
Topic |
Documentation Links |
ADAS, Vision, DL |
See vision apps [LINK] |
Gateway |
See ethernet firmware [LINK] See gateway demos [LINK] |
Integrated MCU |
See MCUSW [LINK] |
RTOS Device Drivers |
See PDK [LINK] |
2.2. Running Out of the Box Demos¶
Out of the Box Demos refers to prebuilt linux filesystem and boot partition with demo binaries and firmware preintegrated. It is downloadable as a tar ball from the SDK release page and can be extracted to an SD card and loaded on the board via a simple script without the need to download the source package or build anything.