4.14. UDMA¶
4.14.1. Introduction¶
The DMA architecture specifies the data structures used by standard communications modules to facilitate direct memory access (DMA) and to provide a consistent application programming interface (API) to the host software in multi-core devices. The data structures and the API used to manipulate them will be jointly referred to as NAVSS. For more information on NAVSS DMA architecture, refer to the device Technical Reference Manual
The UDMA driver provides API to program the DMA portion of the NAVSS subsystem to setup and initiate transfers. Below are the high level features supported by the driver
- Both Main and MCU NAVSS instances
- Supports all DMA operations from both instances from all the cores in the SOC
- UDMAP block copy using native NAVSS channels
- DRU block copy using direct TR submission to DRU register
- DRU block copy using indirect (PSIL) TR submission to UDMA external channels
- PDMA module to initiate transfers to/from PDMA peripherals like UART, McASP, McSPI, ADC, MCAN
- DMA transfer to/from from native PSIL peripherals like EMAC, CPSW, SA2UL
- Event and interrupt management like DMA completion, channel chaining, interrupt sharing using IA
- Resources management across instances and cores for UDMAP DMA channels,RX flow, External UTC channel (DRU), interrupt aggregators (IA), interrupt routers (IR),global events, ring accelerators (RA)
- Interaction with DMSC RM module via SCICLIENT for all non-RealTime (NRT) configuration
- Supports both TI-RTOS and baremetal
Notes
- UDMA driver doesn’t manage/allocate the descriptor and RA memory.The caller need to allocate and provide the required memory.
- UDMA driver doesn’t use any global variables. All the required object memory like channel, driver instance, event etc should be allocated by the caller
This document has detailed API description that user can use to make use of the UDMA driver.
4.14.2. User Interface¶
For details about individual fields of this library structure, see the PDK doxygen documentation
4.14.2.1. APIs¶
The UDMA driver API can be broadly divided into the following categories
- UDMAP native channel API
- DRU (External UTC) channel API
- PDMA channel operations
- Event and interrupt API
- Ring API
In addition to above drivers the UDMA package also includes many sample examples which show how to use the drivers in different ways. Many of these sample examples use a common set of APIs which a user may find useful to refer to for use in their final application.
API reference for application:
#include <ti/drv/udma/udma.h>
4.14.3. Application¶
4.14.3.1. Examples¶
| Name | Description
|
Expected Results
|
|---|---|---|
| UDMA ADC RX application | This performs PDMA
RX data capture
from ADC. ADC is
configured in
single shot mode
and captures
APP_ADC_NUM_CH
channel of ADC
data. The FIFO is
configured to
generate a DMA
trigger after
all channel data
is captured
|
The application
checks the ADC
channel ID and
prints pass on
successful
completion
|
| UDMA Chaining application | UDMA chaining
sample application
performing a chain
of block copy using
channel global
trigger: CH0 -> CH1
-> ... -> CHx.
The first channel
doesn’t user a
global trigger and
each channel
triggers the next
channel’s global
trigger through
the channel’s TR
event register.
A channel’s source
buffer is previous
channel destination
buffer. This
ensures that
chaining trigger
worked in a
synchronized manner
when the memory
compare matches
|
The application
checks the
destination buffer
with source buffer
and prints pass on
successful
completion
|
| UDMA CRC application | This performs
UDMA CRC operation
|
The application
checks the
calculated CRC
value with
pre-calculated CRC
value and prints
pass on successful
completion
|
| UDMA Direct TR DRU application | UDMA DRU memcpy
sample application
performing block
copy using direct
TR submission via
DRU registers
|
The application
checks the
destination buffer
with source buffer
and prints pass on
successful
completion
|
| UDMA In-Direct TR DRU application | UDMA DRU memory
copy sample
application
performing block
copy using Type 15
Transfer Record
(TR15) using
Transfer Record
Packet Descriptor
(TRPD)
for developers.
|
The application
checks the
destination buffer
with source buffer
and prints pass on
successful
completion
|
| UDMA Blockcopy application | UDMA memory copy
sample
application
performing block
copy using Type 15
Transfer Record
(TR15) using
Transfer Record
Packet Descriptor
(TRPD)
|
The application
checks the
destination buffer
with source buffer
and prints pass on
successful
completion
|