TI Autonomous Driving Algorithms (TIADALG) Library API Guide
File List
Here is a list of all files with brief descriptions:
 cache.h
 ti_file_io.h
 ti_file_io_msg.h
 tiadalg_alg_int_interface.hThis file defines internal common data structures for all the modules
 tiadalg_common_data_struct.hThis file defines common data structures for all the modules
 tiadalg_common_utils.h
 tiadalg_configparser.h
 tiadalg_dof_plane_seperation.hThis file defines the interface for creating three plane output from packed output from DOF h/w
 tiadalg_fisheye_transformation.hThis file defines the interface for fish eye transformation of list of key points
 tiadalg_image_color_blending.hThis file defines the interface for image color blending to highlight pixel level detection derived by other algorithm such as semantic segmentation
 tiadalg_image_preprocessing.h
 tiadalg_img_proc.h
 tiadalg_interface.h
 tiadalg_mem_manager.h
 tiadalg_select_top_feature.hThis file defines the interface for multiple element descriptor matching
 tiadalg_solve_pnp.hThis file defines the interface for pose estimation using pnp technique
 tiadalg_sparse_upsampling.hThis file defines the interface for sparse up-sampling and convolution operation
 tiadalg_test_interface.h
 tiadalg_visual_localization.hThis file defines the interface for TI AD Ego localization algorithm

© Copyright 2018 Texas Instruments Incorporated. All rights reserved.
Document generated by doxygen 1.8.6