50 #ifndef ti_osal_Queue__include 51 #define ti_osal_Queue__include 66 struct Osal_QueueElem *
next;
69 struct Osal_QueueElem *
prev;
void * Osal_Queue_get(Osal_Queue_Handle queueHandle)
Function to return the element at the front of the queue.
void Osal_Queue_construct(void *structPtr, const void *queueParams)
Function to construct the queue.
struct Osal_QueueElem * prev
Definition: Queue.h:69
bool Osal_Queue_empty(Osal_Queue_Handle queueHandle)
Function to perform queue empty chcek.
Queue element.
Definition: Queue.h:64
void * Osal_Queue_Handle
Definition: Queue.h:76
Osal_Queue_Handle Osal_Queue_handle(void *structPtr)
Function to return the queue handle from the structure.
void Osal_Queue_put(Osal_Queue_Handle queueHandle, Osal_Queue_Elem *ptr)
Function to put the element to the queue.
struct Osal_QueueElem * next
Definition: Queue.h:66