![]() |
TI Deep Learning Library User Guide
|
This page lists layers/operators supported in current TIDL version. By default, TIDL releases include import tool supporting Caffe, Tensorflow, ONNX, tflite. Import tool will translate/import the training result file(prototxt+caffemodel, pb, onnx) to TIDL format.
Note
In the current release, Only models/networks listed in the Sample Pre-trained CNN Models for TIDL are supported . Any Network which is not included in this list will NOT be supported
More networks (Including custom networks) will be supported in the future releases.
| No | TIDL Layer Type | Caffe Layer Type | Tensorflow Ops | ONNX Ops | tflite Ops | Notes |
|---|---|---|---|---|---|---|
| 1 | TIDL_ConvolutionLayer | Convolution ConvolutionDepthwise | Conv2D DepthwiseConv2dNative | Conv | CONV_2D DEPTHWISE_CONV_2D | Regular & depth-wise conv will be imported as conv. For TF and tflite DepthwiseConv2dNative, depth_multiplier shall be 1 in Number of input channels > 1. ReLU & BN & Pooling will be merged into conv to get better performance. 1x1 conv will be converted to innerproduct. Validated kernel size: 1x1, 3x3, 5x5, 7x7. if stride == 4, only support kernel == 11x11. if stride == 2, kernel should less than 7. if kernelH*kernelW*input channel/groupNum+enableBias % 64 != 0, performance is not optimal. |
| 2 | TIDL_BatchNormLayer | BatchNorm | FusedBatchNorm | BatchNormalization | ReLU & Scale & Bias & PReLU will be merged & imported as BN. 16bit is not optimal for current version. All the channel-wise Broad cast operations are mapped to BN now. | |
| 3 | TIDL_PoolingLayer | Pooling | MaxPooling AvgPooling Mean | MaxPool AveragePool GlobalAveragePool | MAX_POOL_2D AVERAGE_POOL_2D MEAN | Validated pooling size: 1x1(MAX, stride 1x1/2x2), 2x2, 3x3. 4x4 pooling is not optimal. |
| 4 | TIDL_EltWiseLayer | EltWise | Add Mul | Add Mul | ADD MUL | Only support SUM/MAX/PRODUCT. Only support 2 inputs. |
| 5 | TIDL_InnerProductLayer | InnerProduct | MatMul | Gemm | FULLY_CONNECTED | Input shape must be 1x1x1xN. Please use global pooling/flatten before innerproduct. Feature size larger than 2048*2048 is not optimal. |
| 6 | TIDL_SoftMaxLayer | SoftMax | Softmax | Softmax | SOFTMAX | Input shape must be 1x1x1xN. Please use global pooling/flatten before softmax. |
| 7 | TIDL_Deconv2DLayer | Deconvolution | Conv2DTranspose | ConvTranspose | TRANSPOSE_CONV | Recommend to use Resize/Upsample to get better performance. Only 4x4 kernel with 2x2 stride is supported |
| 8 | TIDL_ConcatLayer | Concat | ConcatV2 | Concat | CONCATENATION | Concat will do channel-wise combination by default. Concat will be width-wise if coming after a flatten layer. used in the context of SSD |
| 9 | TIDL_SliceLayer | Slice | Slice | Split | NA | Only support channel-wise slice. |
| 10 | TIDL_CropLayer | Crop | NA | NA | NA | |
| 11 | TIDL_FlattenLayer | Flatten | NA | Flatten | NA | 16bit is not optimal in current version. |
| 12 | TIDL_ArgMaxLayer | ArgMax | Argmax | ArgMax | ARG_MAX | Only support axis == 1, mainly for the last layer of sematic segmentation. |
| 13 | TIDL_DetectionOutputLayer | DetectionOutput | tensorflow Object Detection API | NA | NA | Please refer to comment 1. |
| 14 | TIDL_ShuffleChannelLayer | ShuffleChannel | NA | Reshape + Transpose + Reshape | NA | |
| 15 | TIDL_ResizeLayer | NA | ResizeNearestNeighbor ResizeBilinear | UpSample | RESIZE_NEAREST_NEIGHBOR RESIZE_BILINEAR | Only support 2x2, 4x4. |
| No | Caffe Layer Type | Tensorflow Ops | ONNX Ops | tflite Ops | Notes |
|---|---|---|---|---|---|
| 1 | Bias | BiasAdd | Bias will be imported as BN. | ||
| 2 | Scale | Scale will be imported as BN. | |||
| 3 | ReLU | Relu Relu6 | Relu | RELU RELU6 | ReLU will be imported as BN. |
| 4 | PReLU | Prelu | PReLU will be imported as BN. | ||
| 5 | Split | Split | Split layer will be removed after import. | ||
| 6 | Reshape | Reshape | Reshape | RESHAPE | Please refer to comment 1. |
| 7 | Permute | Please refer to comment 1. | |||
| 8 | Priorbox | Please refer to comment 1. | |||
| 9 | Pad | Pad | PAD | Padding will be taken care of during import process, and this layer will be automatically removed by import tool. | |
| 10 | MINIMUM | For relu6 / relu8 | |||
| 11 | DropOut | This layer is only used in training, and this layer will be automatically removed during import process. | |||
| 12 | Squeeze | Flatten | |||
| 13 | Shape | Resize | |||
| 14 | Transpose | For ShuffleChannelLayer | |||
| 15 | Clip | Parametric activation threshold PACT |
Any unrecognized layers/operators will be converted to TIDL_UnsupportedLayer as a place-holder. The shape & parameters might not be correct. You may get the TIDL import result, but the result contains a unsupported layer, which will not work on target/PC. |