![]() |
TI Deep Learning Library User Guide
|
TIDL Support Below Post Processing types in Stand alone Test application to Sanity test the model deployments. For all the post processing inFileFormat shall be 2. All the these post processing in test application are only for demo purpose not production quality.
This post processing implements top-1 and top-5 accuracy computation for classification networks. The input list file shall contain the list of file with expected class index. Refer the imageNet_sample_val.txt file in the testvecs folder for reference
This post processing Draws the detected box on the original input image. Unique color for each class. The input file shall contain the list of input images to be processed. Maximum 21 classes are supported. There is no limit on number of detected objects
This post processing colors each pixel in the input image with unique color for each class index or depth estimation.