4.2. Release notes - 06_01_01¶
4.2.1. Features¶
Note
New features vs previous release are marked in bold
4.2.1.1. Hardware support¶
- J721E Alpha and Beta EVM support with Leo PMIC processor board
- Fusion1 RevC daughter card with UB960 FPDLink deserializer
- IMX390 2MP CSI2 image sensor + UB953 FPDLink serializer
- AR0233 2.5MP CSI2 image sensor + UB953 FPDLink serializer
- AR0820 8MP CSI2 image sensor + UB953 FPDLink serializer
- GESI(Gateway/Ethernet Switch/Industrial) daughter card (for additional ethernet and CAN ports)
- Infotainment daughter card (for HDMI output)
4.2.1.2. Software features¶
Important
Below is a summary of key features. Refer individual SDK Components release notes for more details
4.2.1.2.1. Vision Apps (ADAS, Vision, DL demos)¶
- OpenVX based demos for ADAS, Vision, deep learning applications
- TI-RTOS on C7x, C6x, R5F and Linux on A72
- Integrates all major PSDKRA and PSDKLA SW components like TIDL, MMALIB, PDK, OpenVX, OpenGL, video codec, C6x algorithms, imaging/sensors, IPC, Linux, TI-RTOS, SPL/uboot.
- Integrates all major HW components like CSI2 camera, eDP/HDMI display, UART, I2C, ethernet, SD card
- Deep learning demos
- Image Classification demo
- Auto valet parking (AVP) demo
- semantic segmentation, Parking spot detect and Vehicle detect algorithms
- 1 channel, 3 algo @ 56 fps mode
- 3 channel, 3 algo @ 28 fps mode (combined network for parking spot and vehicle detect)
- Surround view demos
- 3D surround view using GPU on 4x 2MP 30fps live camera input
- 3D surround view calibration application
- ADAS/Vision demos
- Dense optical flow (DOF) demo
- Stereo disparity engine demo
- Single and multi camera CSI2RX + VISS + LDC + MSC + Display demo
- C7x algorithm offload demo
- Perception Toolkit (PTK) Demos
- Camera based SFM and occupancy grid mapping using Dense optical flow HW engine
- Radar and lidar occupancy grid mapping
- Camera SFM, radar, lidar fusion for occupancy grid mapping
- OpenVX target nodes
- image pre-processing (YUV 2 RGB) nodes for DL demos
- image post-processing and visualization nodes for deep learning, DOF, Stereo demos
- lidar, radar, camera SFM nodes for PTK demos
- OpenGL nodes for surround view
- Profiling, logging and other utility APIs
4.2.1.2.2. Gateway Demos¶
- CAN-Ethernet gateway demo to showcase P2P (Protocol to Protocol) translation
- Full duplex routing between: CAN-to-Ethernet, Ethernet-to-CAN and CAN-to-CAN.
4.2.1.2.3. Platform Development Kit (PDK)¶
- RTOS device drivers running on R5F, C6x, C7x, A72
- Supported drivers and modules
- Board diagnostic library
- CPSW (2G and 9G)
- CSI2 camera
- CSL-FL (Chip support library)
- DSS display (eDP and HDMI, BT601 discrete sync mode)
- GPIO
- I2C
- IPC (inter processor communication)
- McASP
- MMCSD with FATFS (A72 with RTOS)
- OSAL
- SBL secondary bootloader
- SCI Client (DMSC interface)
- SPI driver (SPI, QSPI, OSPI, Hyperflash)
- UART
- UDMA and DRU
- VPAC and DMAC (VHWA)
4.2.1.2.4. MCU Software (MCU SW)¶
- AutoSAR MCAL driver and demo applications running on R5F
- AutoSAR MCAL driver for Adc, Can, CDD IPC,Dio, Eth, Gpt, Pwm, Spi & Wdg
- MCU Demo Applications
- CAN Profiling Application
- CDD IPC Profiling Application
- SPI IPC Profiling Application
4.2.1.2.5. TI Deep learning Library (TIDL) and MMALIB¶
- TIDL deep learning inference engine library running on C7x/MMA
- MMALIB for accelerating convolution, deconvolution layers on MMA (used by TIDL internally)
- TIDL network import tool and performance analyzer tool
- Supports Caffe, ONXX, TFlite network import formats
- Supported layers: Convolution, deconvolution, pooling, ReLU, Elt-wise, Inner product, Soft-max, and many more, refer TIDL user guide (LINK)
- Custom / User defined layer Call-back to plugin user specific layers
4.2.1.2.6. TI OpenVX (TIOVX)¶
- OpenVX v1.1 compliant implementation with graph pipelining and user data object extension support
- OpenVX API on A72 running Linux
- OpenVX target kernels on C7x, C6x, R5F, A72
- OpenVX v1.1 C6x kernels
- OpenVX nodes for
- TIDL (C7x)
- VISS (R5F)
- LDC (R5F)
- MSC (multi-scalar) (R5F)
- Pyramid (using MSC) (R5F)
- BLNF (bilateral noise filter) (R5F)
- CSI2 camera (R5F)
- Display (eDP and HDMI) (R5F)
- Video decode (R5F)
- OpenVX tutorials for getting started
- PyTIOVX tools for target kernel code generation
4.2.1.2.7. Imaging¶
- IMX390 2MP sensor driver (30/60fps) with IQ tuning
- AR0233 2.5MP sensor driver with IQ tuning
- AR0820 8MP sensor driver with IQ tuning
- TI Auto-exposure and auto white-balance algorithms
4.2.1.2.8. Ethernet Switch Firmware (ETHFW)¶
- Ethernet switch firmware running on R5F for CPSW9G
- Layer 2 switching
- NDK integration
- Remote switch configuration server
- GUI switch configuration tool
- Inter VLAN routing
- IP next header filtering
- Rate limiting
4.2.1.2.9. TI Autonomous Driving Algorithms (TIADALG)¶
- Image pre-processing APIs for color plane conversion and separation YUV to RGB for DL applications (C6x optimized)
- Camera Pose estimation API using solve pnp technique (C6x optimized)
- Visual localization algorithm (C6x optimized)
4.2.1.2.10. Video Codecs¶
- Single and multi channel H264 decoder on RTOS R5F
- Upto 1080p 30fps resolution, I and I+P frame
- NV12 and 8b output
4.2.1.2.11. TI-RTOS¶
- SysBIOS for R5F, C6x, C7x, A72
- Network developer kit (NDK) on R5F
4.2.1.2.12. Code Gen Tools (CGT)¶
- TI Compiler, assembler, linker for R5F, C6x, C7x
- GCC compiler for A72 (needs to be downloaded separately)
4.2.2. Device Support and Validation Information¶
SoC | Build Host (OS) | Run Target (OS) | Test Plaform |
---|---|---|---|
J721e | x86_64 (Linux Ubuntu 18.04) | R5F, C6x, C7x running TI-RTOS A72 running Linux |
J721e EVM with daughter cards |
PC emulation mode | x86_64 (Linux Ubuntu 18.04) | x86_64 (Linux Ubuntu 18.04) | x86_64 (Linux Ubuntu 18.04) |
4.2.3. Known Issues¶
Refer to individual SDK Components release notes for known issues in each component