Reshape to full dimensions given.
Definition: c/Image.h:75
Do not resize, may overflow (not recommended)
Definition: c/Image.h:79
struct Renderer Renderer
Definition: c/Renderer.h:81
void Image_show(Image *obj)
Keep aspect ratio, match largest dimension (no overflows)
Definition: c/Image.h:78
void Image_delete(Image *obj)
struct Image Image
Definition: c/Image.h:84
PTK_FitType
Definition: c/Image.h:73
void Image_hide(Image *obj)
Keep aspect ratio, match x (may overflow y)
Definition: c/Image.h:76
Image * Image_create(Renderer *r, uint32_t texture, uint32_t invert, PTK_FitType fit)
Keep aspect ratio, match y (may overflow x)
Definition: c/Image.h:77
void Image_setTexture(Image *obj, uint32_t tex)