![]() |
TI Deep Learning Library User Guide
|
The compiler is released with TI Deep learning library package. Mainly it contains
This above mentioned executable of this compiler is called internally while importing the network model. It is recommended not to use this compiler directly and let it be used by import tool. Executables of import tool are available as part of TI Deep Learning Library package at below path
Below command can be used to invole the network compiler on a pre imported model,
A successful execution of utility will create a directory mentioned in the configuration file as OUTPUT_DIR and the directory will have multiple *.csv file for each unique configuration. The name format of generated CSV file is as below networkName_Analysis_DSP**NUMCORES**_FRQ**FREQ**_DATA**datatype**_MSMCS**MSMCSIZE_KB**DDRE**DDR_EFFICIENCY**_EMIFP**NUMEMIF_PORTS**_DDRMTS**DDRFREQ_MHZ**__**INWIDTH**x**INHEGIHT** Example: jacintoNet11v2_Analysis_DSP1_FRQ1000_DATA0_MSMCS8192_DDRE0.60_EMIFP1_DDRMTS4266_1024x512 An example result file as shown as below
The file contains the layer wise processing time along with the network parameters of the layer. At the end it provides a summary of total execution time, DDR bandwidth and MSMC SRAM (onchip memory) bandwidth.