Remote Device User Guide
|
"Remote Device" is the device virtualisation and sharing component within Processor SDK RTOS Automotive (PSDKRA) that can be used to share a physical device across multiple cores and OS The architecture and data / control flow for remote device framework is shown in below figure
The main modules in remote device are listed below
Remote device Modules | Description |
---|---|
Protocol | Server - client communication protocols |
Server framework | Core remote device functionality |
Display Server | Display virtualisation service |
Display Examples | Example application to demonstrate remote device capabilities |
concerto | Makefile build infrastructure |
docs | User documentation |