![]() |
MMALIB User Guide
|
This module consists of kernels to implement the core computations occurring in the context of convolutional neural networks.
Sub Modules | |
| MMALIB_CNN_convolve_col_smallNo_ixX_ixX_oxX | |
| Kernel for computing CNN-style 2D convolution using column major data ordering on the input and output feature maps. This approach computes more quickly if filter grouping is chosen such that Ni=No=1, or if filter grouping is chosen such that NiFrFc < MMA_SIZE, otherwise use regular convolution method MMALIB_CNN_convolve_row_ixX_ixX_oxX. This kernel is also referred to as depth-wise convolution. | |
| MMALIB_CNN_convolve_row_ixX_ixX_oxX | |
| Kernel for computing dense CNN convolution with row based processing and matrix multiplication. | |
| MMALIB_CNN_deconvolve_row_ixX_ixX_oxX | |
| Kernel for computing dense CNN deconvolution with row-based processing and matrix-matrix multiplication. | |
| MMALIB_CNN_fullyConnected_ixX_ixX_oxX | |
| Kernel provides compute functionality of Fully Connected Layer. | |