2.13. OSAL¶
2.13.1. Introduction¶
The SDL requires the application to provide an OSAL implementation for various functionalities in order to keep SDL as OS-agnostic. Primarily, the SDL requires OSAL implementations for interrupt registration and enable/disable, and also for a delay mechanism needed for POK programming.
The following APIs shall be provided by the application by calling SDL_OSAL_init:
SDL_OSAL_init()
SDL_OSAL_enableInterrupt()
SDL_OSAL_disableInterrupt()
SDL_OSAL_registerInterrupt()
SDL_OSAL_deregisterInterrupt()
SDL_OSAL_globalDisableInterrupts()
SDL_OSAL_globalRestoreInterrupts()
SDL_OSAL_printf()
SDL_OSAL_delay()
Additionally, the following optional APIs may be provided
SDL_OSAL_printf();
2.13.2. Example Usage¶
The SDL provides a sample implementation of these APIs as part of the SDL test suite. The sample implementation re-uses PDK OSAL APIs from the SDK in order to provide the services. This is verified with the following Operating Systems:
Non-OS (Baremetal)
The existing baremetal sample OSAL interface can be used, or the application may implement it’s own. To use the existing sample interface:
Add the source file osal_interface.c (located in test/osal/src/) to the application’s build
Include the header osal_interface.h (located in test/osal/) to the application’s source file
Call the example’s OSAL initializtion function SDL_TEST_osalInit() to initialize the OSAL. Do this before calling any SDL APIs.
Alternatively, the application may implement it’s own OSAL. An example of how to do this is shown below
Define the OSAL APIs
pSDL_OSAL_hwipHandle SDL_TEST_registerInterrupt(SDL_OSAL_hwipParams *pParams) { HwiP_Params hwipParams; HwiP_Params_init(&hwipParams); hwipParams.arg = pParams->callbackArg; return HwiP_create(pParams->intNum, pParams->callback, &hwipParams); } int32_t SDL_TEST_enableInterrupt(uint32_t intNum) { HwiP_enableInterrupt(intNum); return SDL_PASS; } int32_t SDL_TEST_disableInterrupt(uint32_t intNum) { HwiP_disableInterrupt(intNum); return SDL_PASS; } int32_t SDL_TEST_globalDisableInterrupts(uintptr_t *key) { *key = HwiP_disable(); return SDL_PASS; } int32_t SDL_TEST_globalRestoreInterrupts(uintptr_t key) { HwiP_restore(key); return SDL_PASS; }
Initalize the OSAL Interface
SDL_OSAL_Interface osal_interface = { .enableInterrupt = (pSDL_OSAL_interruptFunction) SDL_TEST_enableInterrupt, .disableInterrupt = (pSDL_OSAL_interruptFunction) SDL_TEST_disableInterrupt, .registerInterrupt = (pSDL_OSAL_registerFunction) SDL_TEST_registerInterrupt, .deregisterInterrupt = (pSDL_OSAL_deregisterFunction) HwiP_delete, .globalDisableInterrupts = (pSDL_OSAL_globalDisableInterruptsFunction) SDL_TEST_globalDisableInterrupts, .globalRestoreInterrupts = (pSDL_OSAL_globalRestoreInterruptsFunction) SDL_TEST_globalRestoreInterrupts, .printFxn = (pSDL_OSAL_printFunction) UART_printf, .delay = (pSDL_OSAL_delayFunction) Osal_delay, }; int32_t main(void) { SDL_ErrType_t ret = SDL_PASS; ret = SDL_OSAL_init(&osal_interface); return ret; }
2.13.3. Examples¶
Test apps that are meant for verifying the functionality of the module are also provided.
Test App Name |
Description |
Location |
Build Command |
|---|---|---|---|
osal_app |
|
[sdl_install_dir]/test/osal |
make osal_test_app PROFILE=release |