3.1. ESM Safety Example¶
3.1.1. Introduction¶
This example demonstrates High and Low priority events received from the WKUP_ESM, MCU_ESM, and ESM (Main domain ESM) through the application-registered callback. It also shows routing and clearing of events to the MCU_SAFETY_ERRORn pin.
This example displays setting up ESM to
Enable/Disable input events to the ESM module for each ESM instance
Registration of application callback for ESM error events for each ESM instance
Designating input events as high priority or low priority for each ESM instance
Designating direct pin routing to MCU_SAFETY_ERRORn pin for external monitor communication
The following modules are used as triggers to monitor and handle ESM events:
Voltage and Thermal Manager (VTM)
Timer
ECC
3.1.2. Use Cases¶
Use Case
Description
ESM
Input Event
Input Trigger
Priority
Action
UC-1
Configuration of Low Priority ESM event with no error pin trigger using WKUP_ESM0. Error event is triggered and app is notified of event
WKUP_ESM0
WKUP_VTM0_THERM_LVL_GT_TH1_INTR_0 Temp greature than early warning threshold
Change threshold in VTM to trigger early warning, then return thresholds back to normal to simulate “cooling down”.
Low
Error event is logged by application. Print event to UART. Error event is cleared
UC-2
Configuration of High Priority ESM event with error pin trigger using WKUP_ESM0. Application handles the error event in software and clears the error pin.
WKUP_ESM0
WKUP_VTM0_THERM_LVL_GT_TH2_INTR_0
Change threshold in VTM to trigger early warning, then alter thresholds again to pass temperature critical threshold. Lastly, return thresholds back to normal to simulate “cooling down”.
High
Error event is logged by application. Print event to UART. Application clears error pin to simulate resolution of event by software.
UC-3
Configuration of High Priority ESM event with error pin trigger. Applicatino is unable to handle the error event in software and does not clear the error pin.
WKUP_ESM0
WKUP_VTM0_THERM_LVL_GT_TH2_INTR_0
Change threshold i nVTM to trigger early warning, then alter thresholds again to pass temperature critical threshold. Lastly, return thresholds back to normal to simulate “cooling down”.
High
Error event is logged by application. Print event to UART. Application does not clear the error pin in order to simulate no internal resolution by software. Simulates notification to external monitor.
UC-4
Configuration of Low Priority ESM event with no error pin trigger using MCU_ESM0. Error is triggered and application is notified of the event.
MCU_ESM0
MCU_TIMER3_INTR_PEND_0
Timer expiration
Low
Error event is logged by application. Print event to UART. Error event is cleared and execution continues.
UC-5
Configuration of High Priority ESM event with error pin trigger using MCU_ESM0. Application handles the error event in software and clears the error pin.
MCU_ESM0
MCU_TIMER2_INTR_PEND_0
Timer expiration
High
Error event is logged by application. Print event to UART. Application clears error pin to simulate resolution of event by software.
UC-6
Configuration of Low Priority ESM event with no error pin trigger using ESM0. Error event is triggered and app is notified of event.
ESM0
ECC error injection
Low
Error event is logged by application. Print event to UART. Error event is cleared and execution continues.
UC-7
Configuration of Hishg Priority ESM event with error pin trigger using ESM0. Application handles the error event in software and clears the error pin.
ESM0
ECC error injection
High
Error event is logged by application. Print event to UART. Application clears error pin to simulate resolution of event by software.
3.1.3. Example Details¶
The example should be loaded to the hardware using the Secondary Boot Loader (SBL) from the SDK.
Example Name |
Location |
Build Command |
|---|---|---|
esm_wkup_mcu_app |
[sdl_install_dir]/examples/esm/wkup_mcu_esm0/ |
make esm_wkup_mcu_app PROFILE=release |
esm_main_app |
[sdl_install_dir]/examples/esm/main_esm0/ |
make esm_main_app PROFILE=release |
3.1.4. Expected Output¶
esm_wkup_mcu_app:
ESM Example Application
VTM_ESM_init: Init WKUP ESM complete
TIMER_ESM_init: Init MCU ESM complete
ESM example init complete
Any clear of MCU_SAFETY_ERRORn pin will first wait 10 usecs
Minimum Time Interval is 99 usecs
ESM timer initialization complete
Starting Test Case 0
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Got ltThr0 interrupt through ESM module
System at a temperature below the threshold of lt_thr0
System running at a safe temperature
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
Take action
ESM instance #1, ESM interrupt type = High Priority ESM event
case 0 sucess
Use Case 0 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
Starting Test Case 1
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
Take action
ESM instance #1, ESM interrupt type = High Priority ESM event
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Got ltThr0 interrupt through ESM module
System at a temperature below the threshold of lt_thr0
System running at a safe temperature
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
timerExpPinDisable: before clear, ESM instance 1 view of MCU_SAFETY_ERRORn pin is 0
case 1 sucess
Use Case 1 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
Starting Test Case 2
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
ESM Call back function called : instType 0x1, intType 0x1, grpChannel 0x0, index 0xa, intSrc 0xa
Take action
ESM instance #1, ESM interrupt type = High Priority ESM event
timerExpPinDisable: before clear, ESM instance 1 view of MCU_SAFETY_ERRORn pin is 0
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x8, intSrc 0x8
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Got ltThr0 interrupt through ESM module
System at a temperature below the threshold of lt_thr0
System running at a safe temperature
ESM Call back function called : instType 0x1, intType 0x2, grpChannel 0x0, index 0x9, intSrc 0x9
Take action
ESM instance #1, ESM interrupt type = Low Priority ESM event
Use Case 2 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
Starting Test Case 3
ERR: Unexpected ESM Instance 2 and ESM Interrupt Type 2
ESM Call back function called : instType 0x2, intType 0x2, grpChannel 0x1, index 0x19, intSrc 0x39
Take action
ESM instance #2, ESM interrupt type = Low Priority ESM event
Use Case 3 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
Starting Test Case 4
ERR: Unexpected ESM Instance 2 and ESM Interrupt Type 1
ESM Call back function called : instType 0x2, intType 0x1, grpChannel 0x1, index 0x18, intSrc 0x38
Take action
ESM instance #2, ESM interrupt type = High Priority ESM event
timerExpPinDisable: before clear, ESM instance 2 view of MCU_SAFETY_ERRORn pin is 0
Use Case 4 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
ESM Example Application summary
-------------------------------
Completed 5 Test Cases
Received 4 High Priority Interrupts
Received 9 Low Priority Interrupts
Test Case Event Log
------------------
Test Case 0: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 0: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 0: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
ESM instance #1, ESM interrupt type = High Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
ESM instance #1, ESM interrupt type = High Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 2: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 2: ESM Call back function called : grpChannel 0x0, index 0xa, intSrc 0xa
ESM instance #1, ESM interrupt type = High Priority ESM event
Test Case 2: ESM Call back function called : grpChannel 0x0, index 0x8, intSrc 0x8
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 2: ESM Call back function called : grpChannel 0x0, index 0x9, intSrc 0x9
ESM instance #1, ESM interrupt type = Low Priority ESM event
Test Case 3: ESM Call back function called : grpChannel 0x1, index 0x19, intSrc 0x39
ESM instance #2, ESM interrupt type = Low Priority ESM event
Test Case 4: ESM Call back function called : grpChannel 0x1, index 0x18, intSrc 0x38
ESM instance #2, ESM interrupt type = High Priority ESM event
ESM Example Application: Complete
All Use cases have passed.
esm_input_trig.c:638:esm_app:PASS
-----------------------
1 Tests 0 Failures 0 Ignored
esm_main_app:
ESM Example Application
ESM_ECC_Example_init: Init MAIN ESM complete
SDTF_init: MCU MSMC ECC Init complete
ESM_ECC_Example_init: ECC Callback Init complete for Main ESM
ESM Safety Example tests: starting
MSMC Double bit error inject Example test UC-6: starting
ESM Call back function called : instType 0x3, intType 0x2, grpChannel 0x1, index 0x10, intSrc 0x30
Take action
Low Priority Interrupt Executed
ECC Error Call back function called : eccMemType 16, errorSrc 0x2, ramId 107, bitErrorOffset 0x00000000, bitErrorGroup 0
MSMC Double bit error inject test: Subtype 0x6b test complete
UC-6: Got Low priority ESM Interrupt
MSMC Double bit error inject Example test UC-7: starting
ESM Call back function called : instType 0x3, intType 0x1, grpChannel 0x1, index 0x11, intSrc 0x31
Take action
High Priority Interrupt Executed
ECC Error Call back function called : eccMemType 16, errorSrc 0x1, ramId 20, bitErrorOffset 0x00000000, bitErrorGroup 0
MSMC Double bit error inject test: Subtype 0x14 test complete
UC-7: Got High priority ESM Interrupt
ESM Safety Example tests: success
ESM UC-6 and UC-7 Test Passed.
All Use_Cases have passed.
main.c:292:esm_app:PASS
-----------------------
1 Tests 0 Failures 0 Ignored