TIOVX User Guide
TIOVX Supported Kernels

Legend

Meaning of terms in the following tables,

  • DMA: Kernel implemented and memory access done using DMA (NOTE: Not enabled in this release)
  • Cache: Kernel implemented and memory access done using CPU Cache
  • [empty]: Kernel is not supported on target

OpenVX Standard Kernels

This table lists the mapping of standard OpenVX kernels to compute targets on the Jacinto7 platform. When mapped to C7X DSP, it indicates if it is implemented using BAM DMA acceleration, or cache only.

All of the below kernels default to running on the standalone C7X DSP. If a different target is needed, it can be selected from the available targets indicated below by using the vxSetNodeTarget() API.

Note: all of the standard kernels were initially developed on J721E running on the C66x DSP. When porting to the C7x, the VXLIB kernels and TIOVX kernel wrappers were recompiled for the C7x. If custom kernels need to be recompiled from C66x to C7x, these kernels in VXLIB and associated kernel wrappers in TIOVX can be referenced for information on how to recompile these kernels.

Kernel C7X HWA PC Emulation Support
Absolute Difference Cache Yes
Accumulate Cache Yes
Accumulate Squared Cache Yes
Accumulate Weighted Cache Yes
Arithmetic Addition Cache Yes
Arithmetic Subtraction Cache Yes
Bitwise AND Cache Yes
Bitwise EXCLUSIVE OR Cache Yes
Bitwise INCLUSIVE OR Cache Yes
Bitwise NOT Cache Yes
Box Filter Cache Yes
Canny Edge Detector Cache Yes
Channel Combine Cache Yes
Channel Extract Cache Yes
Color Convert Cache Yes
Convert Bit depth Cache Yes
Custom Convolution Cache Yes
Dilate Image Cache Yes
Equalize Histogram Cache Yes
Erode Image Cache Yes
Fast Corners Cache Yes
Gaussian Filter Cache Yes
Non Linear Filter Cache Yes
Harris Corners Cache Yes
Histogram Cache Yes
Gaussian Image Pyramid Cache VPAC_MSC* Yes
Laplacian Image Pyramid Cache Yes
Reconstruction from a Laplacian Image Pyramid Cache Yes
Integral Image Cache Yes
Magnitude Cache Yes
Mean and Standard Deviation Cache Yes
Median Filter Cache Yes
Min, Max Location Cache Yes
Optical Flow Pyramid (LK) Cache Yes
Phase Cache Yes
Pixel-wise Multiplication Cache Yes
Remap Cache Yes
Scale Image Cache VPAC_MSC* Yes
Sobel 3x3 Cache Yes
TableLookup Cache Yes
Thresholding Cache Yes
Warp Affine Cache Yes
Warp Perspective Cache Yes
  • Subset of configuration options and or accuracy tradeoff to speed is to be considered for this HWA implementation.

TI Extension Kernels

Note: the below node implementation locations have changed from the 8.6 to 9.0 releases. The new locations can be referenced in Directory Structure document.

Kernel Target Remote Core(s) PC Emulation Support
tivxCaptureNode CSIRX MCU2_0 No
tivxDisplayNode DSS MCU2_0 No
tivxTIDLNode C7x + MMA C7X_1 / C7X_2 / C7X_3 / C7X_4 Yes
tivxVpacVissNode VPAC1_VISS / VPAC2_VISS MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxVpacLdcNode VPAC1_LDC / VPAC2_LDC MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxVpacNfGenericNode VPAC1_NF / VPAC2_NF MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxVpacNfBilateralNode VPAC1_NF / VPAC2_NF MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxVpacMscScaleNode VPAC1_MSC / VPAC2_MSC MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxVpacMscPyramidNode VPAC1_MSC / VPAC2_MSC MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxVpacFcVissMscNode VPAC_FC / VPAC2_FC MCU2_0 (VPAC1) / MCU4_0 (VPAC2) Yes
tivxDmpacSdeNode DMPAC_SDE MCU2_1 Yes
tivxDmpacDofNode DMPAC_DOF MCU2_1 Yes
tivxCsitxNode CSITX MCU2_0 Yes
tivxDisplayM2MNode DSS MCU2_0 Yes
tivxObjArraySplitNode MPU / MCU2_0 A72 / MCU2_0 Yes