2.5. VTM : Voltage and Thermal Management¶
2.5.1. Introduction¶
The Voltage and Thermal Management (VTM) controls the temperature monitors in the die. The VTM provides interrupt and event generation for overtemperature through the Error Signaling Module (ESM). It supports 3 different alerts:
an early alert so that firmware/software can start doing high-temperature thermal management,
a follow-up interrupt for reporting to firmware/software that the temperature has dropped to a safe level,
and a late interrupt whose high level can be used to trigger a hardware-voltage domain reset
SDL supports configuration of the VTM voltage domain and temperature warning. The 3 different alerts are also supported via the SDL ESM Handler, like all other ESM events. The SDL API can also be used to configure the VTM Maximum temperature threshold.
The VTM module provides the following functionality for the application
Ability to initialize VTM
Ability to check the status of the temperature sensor based on alert temperature
Ability to clear and contorl the VTM event inerrupts
2.5.2. Example Usage¶
The following shows an example of SDL VTM API usage by the application to set up the VTM for monitoring for events. Events can be monitored by enabling the events in the associated ESM instance.
Configure the VTM Thresholds and enable events
SDL_VTM_configTs cfgTs; SDL_VTM_intrCtrl ctrl; SDL_VTM_configVd cfgVd; /* Initialize the config structure */ memset(&cfgTs, 0x0, sizeof(SDL_VTM_configTs)); /* Set the control bit for the Temperature sensor config to "SET_THR", indicating we want to set the thresholds */ cfgTs.configTsCtrl = SDL_VTM_VD_CONFIG_CTRL_SET_THR; /* Set the Temperature sensor config */ cfgTs.thr_val.thrValidMap = SDL_VTM_GT_TH1_VALID | \ SDL_VTM_GT_TH2_VALID | \ SDL_VTM_LT_TH0_VALID; cfgTs.thr_val.gtTh2En = TRUE; cfgTs.thr_val.gtTh2 = gt_thr2_adc_code; cfgTs.thr_val.gtTh1En = TRUE; cfgTs.thr_val.gtTh1 = gt_thr1_adc_code; cfgTs.thr_val.ltTh0En = TRUE; cfgTs.thr_val.ltTh0 = lt_thr0_adc_code; SDL_VTM_initTs(SDL_VTM_INSTANCE_TS_0 , &cfgTs); /* Select all 3 interrupts to enable using "INTR_EN_SET" control bits */ ctrl = SDL_VTM_VD_GT_THR2_INTR_EN_SET | \ SDL_VTM_VD_GT_THR1_INTR_EN_SET | \ SDL_VTM_VD_LT_THR0_INTR_EN_CLR; /* enable the threshold interrupts */ SDL_VTM_intrCntrl(SDL_VTM_INSTANCE_VD_DOMAIN_1, ctrl); /* Initialize the config structure */ memset(&cfgVd, 0x0, sizeof(SDL_VTM_configVd)); cfgVd.configVdCtrl = SDL_VTM_VD_CONFIG_CTRL_EVT_SEL; cfgVd.vd_temp_evts = SDL_VTM_VD_EVT_SELECT_TEMP_SENSOR_0; /* enable the tracking of temperature events on this VD */ SDL_VTM_initVd(SDL_VTM_INSTANCE_VD_DOMAIN_1, &cfgVd);
Convert from Temperature to ADC Code
int32_t temp_val = 64000; // temperature in milli degrees Celsius SDL_VTM_adc_code adc_code; SDL_VTM_tsConvTempToAdc(temp_val, SDL_VTM_INSTANCE_TS_0, &adc_code);
Convert from ADC Code to Temperature
SDL_VTM_adc_code adc_code = 404; int32_t temp_val; // temperature in milli degrees Celsius SDL_VTM_tsConvAdcToTemp(adc_code, SDL_VTM_INSTANCE_TS_0, &temp_val);
Get Current Temperature Value
SDL_VTM_iStat_read_ctrl readCtrl; SDL_VTM_adc_code adc_code; /* Get current temperature value */ readCtrl = SDL_VTM_TS_READ_DATA_OUT_VAL; SDL_VTM_getSensorStatus(iSDL_VTM_INSTANCE_TS_0, &readCtrl, &statusVal); adc_code = statusVal.data_out; // data_out has the current temperature
Acknowledge and Disable an interrupt
SDL_VTM_intrCtrl ctrl; /* Ack and disable the interrupt, by clearing the pending and enable bits */ ctrl = (SDL_VTM_VD_GT_THR2_INTR_EN_CLR | \ SDL_VTM_VD_GT_THR2_INTR_RAW_CLR); SDL_VTM_intrCntrl(SDL_VTM_INSTANCE_VD_DOMAIN_1, ctrl);
2.5.3. Examples¶
The VTM module provide a Safety Example to show how to use VTM for some typical use-cases, and also ESM application callback usage. Details regarding the VTM Safety Example can be found here.
Test apps that are meant for verifying the functionality of the module are also provided.
Test App Name |
Description |
Location |
Build Command |
|---|---|---|---|
sdl_vtm_test_app |
|
[sdl_install_dir]/test/vtm/vtm_func |
make sdl_vtm_test_app PROFILE=release |