38 #ifndef INCLUDE_SDL_ECC_CORE_H_ 39 #define INCLUDE_SDL_ECC_CORE_H_ int32_t SDL_ECC_configECCRam(SDL_ECC_MemType eccMemType, uint32_t ramId)
uint32_t SDL_ECC_pollErrorEvent(SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType)
uint32_t SDL_ECC_MemType
This enumerator indicate ECC memory type.
Definition: sdl_ecc.h:169
void SDL_ECC_disableECCEventCheck(SDL_ECC_MemType eccMemType, SDL_ECC_InjectErrorType errorType)
Header file contains enumerations, structure definitions and function.
uint32_t SDL_ECC_MemSubType
This enumerator indicate ECC memory Sub Type.
Definition: sdl_ecc.h:680
void SDL_ECC_enableECCEventCheck(SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType)
SDL_ECC_InjectErrorType
ECC Inject error types.
Definition: sdl_ecc.h:124