MMALIB User Guide
mmalib_perfEst_cnn.h
Go to the documentation of this file.
1 /******************************************************************************
2  * *
3  * module name :MMALIB *
4  * *
5  * module descripton :Matrix Multiply Accelerator Library module for C7x+MMA *
6  * *
7  * Copyright (C) 2017-2018 Texas Instruments Incorporated - https://www.ti.com/ *
8  * ALL RIGHTS RESERVED *
9  * *
10  ******************************************************************************/
11 
23 #ifndef _MMALIB_PERFEST_CNN_H_
24 #define _MMALIB_PERFEST_CNN_H_
25 
27 
30 
31 // // #if defined(__C7120__)
32 // // #include "MMALIB_CNN_convolve_col_smallNo_legacy_ixX_ixX_oxX/MMALIB_CNN_convolve_col_smallNo_legacy_ixX_ixX_oxX.h"
33 // // #endif
34 
36 
38 
40 
42 
44 
46 
47 // #if defined(__C7100__)
48 // #include "MMALIB_CNN_pixelShuffle_row_ixX_ixX_oxX/MMALIB_CNN_pixelShuffle_row_ixX_ixX_oxX_perfEst.h"
49 // #endif
50 
51 // #if defined(__C7120__)
52 // #include "MMALIB_CNN_pixelShuffle_row_ixX_ixX_oxX/MMALIB_CNN_pixelShuffle_row_ixX_ixX_oxX_perfEst.h"
53 // #include "MMALIB_CNN_deconvolveBias_row_ixX_ixX_oxX/MMALIB_CNN_deconvolveBias_row_ixX_ixX_oxX_perfEst.h"
54 // #endif
55 
56 #endif /*_MMALIB_PERFEST_CNN_H_*/
57 
Public header file for MMALIB_CNN_convolveBias_row_ixX_ixX_oxX_perfEst function.
Public header file for MMALIB_CNN_convolve_col_smallNo_highPrecision_perfEst function.
Public header file for MMALIB_CNN_convolve_col_smallNo_highPrecision_pointwisePost_perfEst function.
Public header file for MMALIB_CNN_convolve_col_smallNo_ixX_ixX_oxX_perfEst function.
Public header file for MMALIB_CNN_convolve_row_ixX_ixX_oxX_perfEst function.
Public header file for MMALIB_CNN_deconvolve_row_ixX_ixX_oxX_perfEst function.
Public header file for MMALIB_CNN_fullyConnectedBias_ixX_ixX_oxX_perfEst function.
Public header file for MMALIB_CNN_fullyConnected_ixX_ixX_oxX_perfEst function.
Public header file for MMALIB_CNN_tensor_convert_ixX_oxX_perfEst function.