118 #define GPT_CH_GPTIMER1 (0U) 120 #define GPT_CH_GPTIMER2 (1U) 122 #define GPT_CH_GPTIMER3 (2U) 124 #define GPT_CH_GPTIMER4 (3U) 126 #define GPT_CH_GPTIMER5 (4U) 128 #define GPT_CH_GPTIMER6 (5U) 130 #define GPT_CH_GPTIMER7 (6U) 132 #define GPT_CH_GPTIMER8 (7U) 134 #define GPT_CH_GPTIMER9 (8U) 136 #define GPT_CH_GPTIMER10 (9U) 138 #define GPT_CH_GPTIMER11 (10U) 140 #define GPT_CH_GPTIMER12 (11U) 142 #define GPT_CH_GPTIMER13 (12U) 144 #define GPT_CH_GPTIMER14 (13U) 146 #define GPT_CH_GPTIMER15 (14U) 148 #define GPT_CH_GPTIMER16 (15U) 150 #define GPT_CH_GPTIMER17 (16U) 152 #define GPT_CH_GPTIMER18 (17U) 154 #define GPT_CH_GPTIMER19 (18U) 156 #define GPT_CH_GPTIMER20 (19U) 158 #define GPT_CH_GPTIMER21 (20U) 160 #define GPT_CH_GPTIMER22 (21U) 162 #define GPT_CH_GPTIMER23 (22U) 164 #define GPT_CH_GPTIMER24 (23U) 166 #define GPT_CH_GPTIMER25 (24U) 168 #define GPT_CH_GPTIMER26 (25U) 170 #define GPT_CH_GPTIMER27 (26U) 172 #define GPT_CH_GPTIMER28 (27U) 174 #define GPT_CH_GPTIMER29 (28U) 176 #define GPT_CH_GPTIMER30 (29U) 179 #define GPT_CH_GPTIMER_MAX (30U) 188 #define GPT_PRE_COMPILE_VARIANT (STD_OFF) 197 #define GPT_ISR_VOID (0x00U) 199 #define GPT_ISR_CAT1 (0x01U) 201 #define GPT_ISR_CAT2 (0x02U) 208 #define GPT_DEV_ERROR_DETECT (STD_ON) 210 #define GPT_ISR_TYPE (GPT_ISR_CAT1) 213 #define GPT_REPORT_WAKEUP_SOURCE (STD_ON) 219 #define GPT_VERSION_INFO_API (STD_ON) 224 #define GPT_DEINIT_API (STD_ON) 229 #define GPT_TIME_ELAPSED_API (STD_ON) 234 #define GPT_TIME_REMAINING_API (STD_ON) 239 #define GPT_ENABLE_DISABLE_NOTIFICATION_API (STD_ON) 244 #define GPT_WAKEUP_FUNCTIONALITY_API (STD_ON) 251 #define GPT_MAX_CHANNELS (5U) 257 #define GPT_PREDEF_TIMER_TYPE (GPT_PREDEF_TIMER_DISABLED) 261 #define GPT_PREDEF_TIMER_1US_ENABLING_GRADE (GPT_PREDEF_TIMER_1US_DISABLED) 265 #define GPT_OS_COUNTER_ID ((CounterType)OsCounter_0) 272 #define GPT_TIMEOUT_DURATION (32000U) 281 #ifndef GPT_E_HARDWARE_ERROR 283 #define GPT_E_HARDWARE_ERROR \ 285 DemConf_DemEventParameter_GPT_E_HARDWARE_ERROR \ 294 #define GPT_REGISTER_READBACK_API (STD_ON) 300 #define GptConf_GptChannelConfiguration_TIMER1 (11U) 302 #define GptConf_GptChannelConfiguration_MCU_TIMER6 (6U) 304 #define GptConf_GptChannelConfiguration_MCU_TIMER9 (9U) 306 #define GptConf_GptChannelConfiguration_TIMER5 (15U) 308 #define GptConf_GptChannelConfiguration_TIMER19 (29U) const uint32 Gpt_TimerBaseAddr[GPT_CH_GPTIMER_MAX]
Base Address of the timer peripherals.
#define GPT_CH_GPTIMER_MAX
maximum GP timer channels available
Definition: Gpt_Cfg.h:179
void Gpt_Ch12Isr(void)
GPT Channel ISR.
const struct Gpt_ConfigType_s GptChannelConfigSet
GPT Configuration.