|
FFTLIB User Guide
|
Go to the documentation of this file.
37 #ifndef C7504_FFTLIB_DEFINES_H_
38 #define C7504_FFTLIB_DEFINES_H_ 1
46 #if !defined(_HOST_BUILD)
48 #define FFTLIB_L2_AUX_BUFFER 1
58 #define FFTLIB_MMA_CONFIG_REG __HWA_CONFIG_REG_v1
59 #define FFTLIB_MMA_ARF 1
60 #define FFTLIB_MMA_NUM_ARF_ROWS 64
62 #define FFTLIB_NONZER0_PADFILL 1
64 #define MMA_INDEPENDENT_B_ROW_COUNTERS 1
65 #define MMA_PSAT_ACTIVATION_SUPPORTED 1
75 #define ENABLE_DYN_RANGE_CHECKING 1
77 #define FFTLIB_ENABLE_DYNAMIC_RANGE_TRACKING 1
79 #define FFTLIB_CONVOLVE_COL_IN_KERNEL_PADDING 1