1.2. Release Notes - 01_04_00

1.2.1. Introduction

This release notes provides important information that will assist you in using the SDL software package for the J784S4 family of devices. This document provides the product information and known issues that are specific to the SDL software package.

New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility

1.2.2. What’s New

  • Bug fixes

1.2.3. Supported Modules

SDL support for the following modules are available:

  • R5F PMU, MPU, RAT

  • ESM

  • PBIST

  • LBIST

  • VTM

  • ECC

  • RTI

  • DCC

  • MCRC

  • R5F CCM

  • TOG

  • POK

  • R5F VIM

  • ROM CHECKSUM

Not supported:

None.

1.2.4. Upgrade and Compatibility

Below ECC aggregator metadata has changed resulting in new macros:

  • SDL_COMPUTE_CLUSTER0_AW4_ECC0_AGGR

  • SDL_COMPUTE_CLUSTER0_AW5_ECC0_AGGR

  • SDL_COMPUTE_CLUSTER0_AW6_ECC0_AGGR

  • SDL_COMPUTE_CLUSTER0_AW7_ECC0_AGGR

1.2.5. Supported Devices

Supported Platform

J784S4

1.2.6. Fixed Defects

ID

Module

Summar

Comments

PROC_SDL-7823

POK

Setting trim value for non-Ping pong mode POKs accesses invalid offset

None.

PROC_SDL-8142

ECC

Incorrect base address for the SDL_WKUP_SMS0_1 aggr

None.

PROC_SDL-7650

POK

POK instance IPOK_VDD_CPU1 not included in the SDL header file

None.

PROC_SDL-7612

ESM

Remove ESM Error Pin Counter Value Register from static register read API

None.

PROC_SDL-7597

LBIST

secondaryCoreNeeded should be set to false for SDL_LBIST_INST_A72_1

None.

PROC_SDL-7487

TOG

Duplicate macro definition SDL_IP_TOG_TOP_H_ in the SDL header files (STOG and MTOG)

None.

PROC_SDL-7430

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW7_C7X_1_AGGR0

None - This issue is under investigation.

PROC_SDL-7428

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW6_C7X_1_ECC_AGGR

None - This issue is under investigation.

PROC_SDL-7426

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW5_C7X_1_ECC_AGGR

None - This issue is under investigation.

PROC_SDL-7424

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW4_C7X_ECC_AGGR

None - This issue is under investigation.

PROC_SDL-7402

BIST

Mismatch between function declaration and definition for SDL_PBIST_{start, startNeg} and SDL_LBIST_programConfig

None.

PROC_SDL-6448

PBIST

PBIST MAINR5F1 instance reset sequence disabled

None.

PROC_SDL-6356

ECC

Error Injection fails for ECC Aggregator COMPUTE_CLUSTER0_MSMC_ECC_AGGR0 for certain RAM ID’s.

None.

PROC_SDL-8316

MCRC

SDL MCRC test is failing for MAIN NAVSS instance in release mode

None.

1.2.7. Known Issues and Limitations

ID

Module

Summary

Workaround

PROC_SDL-6360

ECC

Error Injection fails for ECC Aggregator ECC_AGGR0 for certain RAM ID’s.

None - This issue is under investigation. Root cause may be incorrect metadata and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. Due to this, the ECC error inject functionality for the mentioned IPs and endpoints is not usable in this release.

PROC_SDL-6359

ECC

Error Injection fails for ECC Aggregator ECC_AGGR4 for certain RAM ID’s.

None - This issue is under investigation. Root cause may be incorrect metadata and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence. Due to this, the ECC error inject functionality for the mentioned IPs and endpoints is not usable in this release.

PROC_SDL-4141

TOG

1 STOG instances error injection test is failing and are not included in the test application. (STOG17)

None - This issue is under investigation.

PROC_SDL-7422

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_MSMC_ECC_AGGR0

None - This issue is under investigation.

PROC_SDL-7423

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW4_MSMC1_ECC_AGGR0

None - This issue is under investigation.

PROC_SDL-7425

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW5_MSMC1_ECC_AGGR0

None - This issue is under investigation.

PROC_SDL-7427

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW6_MSMC1_ECC_AGGR0

None - This issue is under investigation.

PROC_SDL-7429

ECC

ECC DED test is failing for certain RAM ID’s for SDL_COMPUTE_CLUSTER0_AW7_MSMC1_ECC_AGGR0

None - This issue is under investigation.

PROC_SDL-8248

ECC

SDL ECC error injection test for PCIE ECC aggregators failure

None - This issue is under investigation. Accessing some PCIE ECC Aggregator leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

PROC_SDL-8249

ECC

SDL ECC error injection test for CSI ECC aggregators failure

None - This issue is under investigation. Accessing some CSI ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

PROC_SDL-8258

ECC

SDL ECC error injection test for DSS ECC aggregators failure

None - This issue is under investigation. Accessing some DSS ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

PROC_SDL-8286

ECC

SDL ECC error injection test for I3C ECC aggregators failure

None - This issue is under investigation. Accessing some I3C ECC Aggregators leads to data abort. Root cause may be hardware configuration and/or pre-test sequence in the application. The IP associated with the ECC aggregator may need some additional power/init sequence.

1.2.8. Migration Information

Dependency on C7X image is removed for compute cluster instances. PBIST example, pbist_test_app and sdl_pbist_test_app can be tested as standalone images.

1.2.9. Tool Chain Information

Component

Version

TI ARM R5F Clang Compiler tools

3.2.2.LTS