4.5.9.1.7.1. Enet TSN EST Example

4.5.9.1.7.1.1. Introduction

In this example user can run the application either as talker or listener from the menu. The listen and talker should be connected to the default MAC port over which dummy AVTP packets will be sent. The EST schedule will be applied after stable synchronization to check if packets are sent and received in the expected scheduled time interval at talker and listener respectively.

This example application demonstrates how to configure the 802.1 Qbv (EST) through the TSN yang interface. The yang interface in the TSN is governed by a module called uniconf which runs as a daemon. Any application which interacts with the uniconf called a uniconf client. The uniconf client configures Qbv by opening yang database (DB), write config yang parameters to DB and trigger the uniconf for reading parameters from DB and writing to HW. The uniconf reads or writes parameters from or to HW by calling TI’s Enet LLD driver.

4.5.9.1.7.1.2. Constraints

  • This application only enables one MAC port which has the interface name tilld0. This interface is mapped to MAC port 1 for all devices except the J721E. On the J721E, that interface is mapped to MAC port 2 on QSGMII expansion board and MAC port 1 on the GESI expansion board. To change default MAC port for this example, please change the macro DEFAULT_INTERFACE_INDEX from qosapp_misc.h from 0 another value (1, 2, 3).

  • The application can be only run as talker, listener or bridge mode depending on input characters from UART terminal. (t: talker, l: listener; b: bridge mode)

  • Num of streams on talker is 2 with traffic priorities 0 and 2 mapped to HW queue 0 and 2 respectively. Num of streams and priority can be changed by modifying the gEnetEstAppTestLists from the est_init.c.

  • Both talker and listener need to apply the same EST schedule with the same baseTime to have accurate test results. Thus, there is a delayOffset added to the baseTime of the EST’s AdminList so that both schedules can be applied in the future and at the same time.

  • The EST schedule should be applied and talker starts sending test traffic after PTP synchronization is in good condition to have accurate test results.

  • The talker sends dummy data which is encapsulated in an AVTP packet. Packet sent with VLAN ID 110.

4.5.9.1.7.1.3. Configuration Parameters

  • Default MAC port can be changed by modifying the DEFAULT_INTERFACE_INDEX from the qosapp_misc.h.

  • EST Schedule (Input parameters):

Gate Control

Time Interval

oCCCCCCo

62 usecs

CCoCCCCo

62 usecs

oCCCCCCo

62 usecs

CCoCCCCo

62 usecs

  • Where o denotes open gate and C denotes close gate for a given priority.

  • The EST schedule is 248us long and it is composed of 4 intervals, each with a gate mask that enables transmission of 2 priorities. The priority 7 is for PTP traffic.

  • The gate of this priority is always opened to make sure there is no interruption of the PTP packet which keeps the PTP in good synchronization status. The remaining priorities are for test traffic (avtp packets):

Parameters

TimeValue

baseTime

((Current PTP Time + delayOffset)/delayOffset)*delayOffset

cycleTime

248us

Where:

  • baseTime: PTP time is round up to the delayOffset to have the same baseTime on talker and listener to apply the EST schedule that the same time in the future.

  • delayOffset: added time to current PTP time for baseTime to apply the schedule in the future. It should be a multiple of the cycleTime and large enough so that user can have enough time to start talker and listener by entering a character to UART terminal. The current delayOffset is 100000*cycleTime = 24800000us (24.8 seconds). The factor ‘100000’ is chosen to have delayOffset above 20secs.

4.5.9.1.7.1.4. Expected Behavior

  • With the schedule configured above, the expectation is that

    • all priority 0 & 7 packets arrive on listener inside the time windows.

    • all priority 2 & 7 packets arrive on listener inside the time windows.

../../_images/tsn_est_schedule_config.png

To check whether packets received inside a time window, the rx timestamp, called rxts (PTP time) of each received packet is captured by host port on the listener’s side.

Then the timeSlot of each packet is calculated using the following formula:

timeSlot = (rxts - BaseTime)%CycleTime

Then the timeSlot is compared with the time windows above for each packet to check whether the packet received inside or outside the expected time windows. The EST works when percentage of packets received outside of expected time windows less than or equal 1%.

4.5.9.1.7.1.5. Application Integration Guide

  • The EST application needs to run with the gPTP and yang configuration daemon. Therefore, the gPTP and uniconf must be run during initializing the application. For running the gPTP and uniconf, see Enet LLD TSN User’s Guide for detail instruction. To register the EST application to the initializer of the TSN App for running after the gPTP and uniconf, add the following line to the EnetApp_initTsnByCfg of the tsninit.c:

    #ifdef EST_APP_ENABLED
    if (res == 0)
    {
        res = EnetApp_addEstAppModCtx(gModCtxTable);
    }
    #endif //EST_APP_ENABLED
    

    Then the EST application will be started when the EnetApp_startTsn is called.

4.5.9.1.7.1.6. Yang Configuration for 802.1Qbv

  • Yang file for the 802.1Qbv is defined at standard/ieee/draft/802.1/Qcw/ieee802-dot1q-sched-bridge.yang and standard/ieee/draft/802.1/Qcw/ieee802-dot1q-sched.yang from the https://github.com/YangModels/yang.git

  • Since enet-lld only supports to configure the admin-control-list, baseTime (admin-base-time) and cycleTime (admin-cycle-time), this section only describes the parameters of the admin-control-list Here are parameters of the admin-control-list after converting parameters from yang to to xml:

    <?xml version='1.0' encoding='UTF-8'?>
    <data xmlns="urn:ietf:params:xml:ns:netconf:base:1.0">
      <interfaces xmlns="urn:ietf:params:xml:ns:yang:ietf-interfaces">
        <interface>
          <name/>
          <bridge-port xmlns="urn:ieee:std:802.1Q:yang:ieee802-dot1q-bridge">
            <traffic-class>
              <traffic-class-table>
                <number-of-traffic-classes/>
                <priority0/>
                ...
                <priority7/>
              </traffic-class-table>
              <tc-data>
                <tc/>
                <lqueue/>
                ...
              </tc-data>
              <number-of-pqueues/>
              <pqueue-map>
                <pqueue/>
                <lqueue/>
              </pqueue-map>
            </traffic-class>
            <gate-parameter-table xmlns="urn:ieee:std:802.1Q:yang:ieee802-dot1q-sched-bridge">
              <gate-enabled></gate-enabled>
              <admin-control-list>
                <gate-control-entry>
                  <index/>
                  <operation-name/>
                  <time-interval-value/>
                  <gate-states-value/>
                </gate-control-entry>
              </admin-control-list>
              <admin-cycle-time>
                <numerator/>
                <denominator/>
              </admin-cycle-time>
              <admin-base-time>
                <seconds/>
                <nanoseconds/>
              </admin-base-time>
            </gate-parameter-table>
          </bridge-port>
        </interface>
      </interfaces>
    </data>
    
  • All the supported parameters for 802.1Qbv are from yang standard except the mechanism for mapping traffic class and HW queue are augmented. To configure all parameters of 802.1Qbv above, application calls the yang_db_runtime_put_oneline to write data to DB.

  • After all required parameters written to the DB, application trigger the uniconf by writing the /ietf-interfaces/interfaces/interface|name:tilld0/bridge-port/gate-parameter-table/gate-enabled so that the uniconf writes parameters to HW. See EnetEstApp_setAdminControlList of the est_init.c for yang configuration.

  • Note:

    The network interface `tilld0` is default network interface name, name of network interface
    can be changed by changing default MAC port configured for the example.
    

4.5.9.1.7.1.7. Build Enet TSN EST Example

  • Navigate to the <pdk>/packages/ti/build directory:

    $ cd <pdk>/packages/ti/build
    
  • Build the TSN modules (tsn_unibase, tsn_combase, tsn_gptp, tsn_uniconf):

    $ make tsn_unibase tsn_combase tsn_gptp tsn_uniconf
    
  • To clean the build and remove generated files:

    $ make tsn_unibase_clean tsn_combase_clean tsn_gptp_clean tsn_uniconf_clean
    
  • You can specify the build mode as either release or debug. By default, the release mode is built. To build in debug mode, use the BUILD_PROFILE=debug option:

    $ make tsn_unibase tsn_combase tsn_gptp tsn_uniconf  BUILD_PROFILE=debug
    
  • If you want to build with C++ compiling rules, use the CPLUSPLUS_BUILD=yes option:

    $ make tsn_unibase tsn_combase tsn_gptp tsn_uniconf CPLUSPLUS_BUILD=yes
    
  • To build the TSN EST example app in the PDK, use the following command:

    $ make enet_tsn_est_example_freertos CORE=mcu2_0
    

4.5.9.1.7.1.8. Running Enet TSN EST example

  • HW devices configuration:

../../_images/est_tsn_example_config.png

Connect ethernet cable to MAC port 1.

  • Launch a CCS debug session, load and run enet_tsn_est_example_freertos_mcu2_0_release.xer5f binary file to the MAIN_Cortex_R5_0_0. Alternatively, the example application can be loaded using any other boot method such as MMC/SD.

  • The talker or listener can be run on GM or Slave, whichever devices you choose. However, we recommend running the talker on the Slave device and listener on the GM. The reason for that is the slave device needs to be adjusted PTP time to sync with the GM. Hence, there is a higher possibility that EST use case will fail due to PTP synchronization issue than running the talker on the GM. After running both devices, the PTP slave device is the one which shows the following debug log on UART:

    IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -14648ppb, GMdiff=-24nsec
    IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -14666ppb, GMdiff=-30nsec
    IFV:gptp:domainIndex=0, clock_master_sync_receive:the master clock rate to -14645ppb, GMdiff=-15nsec
    
  • When the abs(GMdiff) is below 1000ns, it is a good time to start the EST usecase.

  • Start the listener. On the GM device, press l to start a listener. It will show log on UART terminal as follows:

    TimeSlots of PacketPriority: 0:   [0, 62000]ns,  [124000, 186000]ns,
    TimeSlots of PacketPriority: 2:   [62000, 124000]ns,  [186000, 248000]ns,
    The following AdminList param will be configured for EST:
    GateMask[7..0]=oCCCCCCo (0x81), start=0 ns, end=61999 ns, dur=62000 ns
    GateMask[7..0]=oCCCCoCC (0x84), start=62000 ns, end=123999 ns, dur=62000 ns
    GateMask[7..0]=oCCCCCCo (0x81), start=124000 ns, end=185999 ns, dur=62000 ns
    GateMask[7..0]=oCCCCoCC (0x84), start=186000 ns, end=247999 ns, dur=62000 ns
    Base time=74400000000ns,Cycle time=248000ns
    INF:cbase:Successfully configure TAS
    INF:cbase:LLDEnetFilter:destmac:91:E0:F0:00:FE:00, vlanId:110, ethType:0x22f0
    
  • Start the talker right after the listener.

    On the slave device, press t to start a talker, It will show log on UART terminal as follows:

    GateMask[7..0]=oCCCCCCo (0x81), start=0 ns, end=61999 ns, dur=62000 ns
    GateMask[7..0]=oCCCCoCC (0x84), start=62000 ns, end=123999 ns, dur=62000 ns
    GateMask[7..0]=oCCCCCCo (0x81), start=124000 ns, end=185999 ns, dur=62000 ns
    GateMask[7..0]=oCCCCoCC (0x84), start=186000 ns, end=247999 ns, dur=62000 ns
    Base time=74400000000ns,Cycle time=248000ns
    INF:cbase:Successfully configure TAS
    
  • The test result will have the best accuracy if the Base time is the same for both talker and listener. To achieve that, we need to start the talker (press t) right after pressing l on the listener.

  • After starting the talker, it will start sending traffic after the EST schedule takes effect (around 20 seconds).

  • Observe test result The number of packets received inside expected time windows are called good packets and outside the expected time windows are bad packets. Press d on the UART terminal of the listener to display number of good/bad packets and the percentage of the bad packets. The expected result is as follows:

    Presss `d`
    PacketPriority: 0, nGoodPackets: 10731108, nBadPackets: 88858, percentage of bad packets: 0%
    PacketPriority: 2, nGoodPackets: 15960287, nBadPackets: 131973, percentage of bad packets: 0%
    CPU Load: 39%
    Press `d`
    PacketPriority: 0, nGoodPackets: 10733815, nBadPackets: 88880, percentage of bad packets: 0%
    PacketPriority: 2, nGoodPackets: 15964301, nBadPackets: 132010, percentage of bad packets: 0%
    Press `d`
    PacketPriority: 0, nGoodPackets: 10736486, nBadPackets: 88901, percentage of bad packets: 0%
    PacketPriority: 2, nGoodPackets: 15968259, nBadPackets: 132056, percentage of bad packets: 0%
    
    + The expected percentage of bad packets is 0-1%.
    

4.5.9.1.7.1.9. Note

  • The gPTP log will help to identify which HW device is a slave device. In case that log is not needed or noisy, please suppress them by changing the gptp:66 to gptp:55 in the enet_tsn/enet_tsn_est_example/makefile.

  • If the percentage of bad packets is greater than 1%, please check the GMdiff from the gPTP log of the slave device mentioned above, the expected GMdiff less than 1000ns. The EST use case only works when PTP synchronization is in good condition.