2.1. Release Notes - 09_02_00¶
2.1.1. Introduction¶
This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.
New features added / supported is listed below and defects fixed are highlighted in Fixed Issues. Also please check Upgrade and Compatibility for backward compatibility
2.1.2. What’s New¶
ID |
Description |
Module |
Supported Platforms |
---|---|---|---|
PDK-10712 |
IPC LLD should provide infrastructure for graceful shutdown of remote processor |
IPC |
J721E, J7200, J721S2, J784S4 |
PDK-11514 |
[SBL]: J7AHP: Test case to ensure cores are switched off if no application image |
SBL |
J784S4 |
PDK-11875 |
RTOS DDR driver shall perform DDR Init in ~10ms |
BOARD |
J784S4 |
PDK-11912 |
[McSPI]: Support for TR based submission in McSPI driver |
McSPI |
J784S4 |
PDK-11934 |
PDK: Report out with explanation benchmark numbers on DSS |
DSS |
J784S4 |
PDK-11961 |
PDK: Report out with explanation benchmark numbers on eMMC |
EMMC |
J784S4 |
PDK-13742 |
Migrate to Clang 3.2.1 version |
COMMON |
J721E, J7200, J721S2, J784S4 |
PDK-13745 |
SBL NAND boot should run with PHY tuning enabled |
SBL |
J721S2, J784S4 |
ETHFW-1221 |
Enet: TSN: gPTP + EST support |
ENET |
J721E, J7200, J721S2, J784S4 |
ETHFW-2559 |
Enet: Support for Absolute TX channel allocation for QoS |
ENET |
J721E, J7200, J721S2, J784S4 |
ETHFW-2561 |
Enet: TSN: gPTP + yang based configuration |
ENET |
J721E, J7200, J721S2, J784S4 |
2.1.3. Upgrade and Compatibility¶
2.1.3.1. TI Arm Clang (R5 Compiler)¶
Updated ti-cgt-arrmllvm(clang) compiler from version 3.2.0 to version 3.2.1
2.1.3.2. Boolean Macros Implementation¶
TRUE/FALSE macros were used both as boolean and unsigned values in last release
Defined new macros: BTRUE/BFALSE macros for boolean and UTRUE/UFALSE for unsigned values to maintain separation
TRUE/FALSE macros are deprecated from current release onwards.
2.1.3.3. SBL¶
Updated SBL to copy image from OSPI NOR with PHY enabled
None
2.1.3.4. ENET¶
ENET_RM_IOCTL_ALLOC_RX_FLOW ` ioctl inArgs changed to type `EnetRm_AllocRxFlowInArgs.
ENET_RM_IOCTL_ALLOC_TX_CH_PEERID ` ioctl inArgs changed to type `EnetRm_AllocTxChInArgs.
2.1.4. Device Support¶
J784S4 GP SR1.0, J784S4-HS-SE SR1.0, J784S4-HS-FS SR1.0 (BOARD=j784s4_evm)
Associated TIFS versions:
TIFS name
J784S4 SR revision
tifs.bin
SR1.0 GP
tifs-hs-enc.bin
SR1.0 HS-SE
tifs-hs-fs-enc.bin
SR1.0 HS-FS
2.1.5. Validation Information¶
For details on the validated examples refer to the platform specific test report available here.
2.1.6. Tool Chain Information¶
Component |
Version |
---|---|
FreeRTOS Kernel |
10.5.1 |
lwIP stack |
2.2.0 |
TI ARM CLANG |
3.2.1.LTS |
GCC ARM code generation tools |
ARCH64 9.2-2019.12 |
CGT XML Processing Scripts |
2.61.00 |
Component |
Version |
---|---|
TI C7x code generation tools |
4.1.0.LTS |
2.1.7. Change Request¶
Refer to monthly roadmap slides for changes in the planned features
2.1.8. Fixed Issues¶
ID |
Head Line |
Module |
Affected Versions |
Affected Platforms |
---|---|---|---|---|
CSI-TX takes longer time to queue and dequeue in driver than expected. |
CSITX |
08.04.00 |
J721S2, J784S4 |
|
Sciclient_rmIrqDeleteRoute API does not check return status |
SCICLIENT |
08.06.00 |
J721E, J7200, J721S2, J784S4 |
|
[SciClient] Write protection sequence is incorrect in Sciclient_serviceSecureProxy API |
SCICLIENT |
09.00.00 |
J721E, J7200, J721S2, J784S4 |
|
[CSIRX] All streams are by default enabled/disabled affecting CSITX |
CSIRX |
09.00.00 |
J721E, J721S2, J784S4 |
|
[SerDes] USXGMII single link mode is broken |
CSL |
09.01.00 |
J784S4 |
|
Sciclient: Enable support to handle TISCI_MSG_QUERY_FW_CAPS message |
SCICLIENT |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
Update security boardcfg to be compatible with TIFS |
SECURITY |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
I2C: Incorrect output frequency for 100KHz I2C operation |
I2C |
09.00.00 |
J721E, J7200, J721S2, J784S4 |
|
Boot App in lock step mode crashes while loading MCU2_0 |
SBL |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
Sciclient: osal_hwip_restore() function uses a return in a void function |
SCICLIENT |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
Sciclient Boardcfg build fails on windows |
SCICLIENT |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
OSPI Boot time values in the data sheet is incomplete |
OSPI |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
SBL is stuck in a loop upon sysfw.bin authentication failures |
SBL, SCICLIENT |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
Sciclient driver doesn’t allow multiple boot attempts for TIFS |
SCICLIENT |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
[Docs] Incorrect Platform Name in Memory Benchmarks Data Sheet |
BENCHMARKS |
09.01.00 |
J721S2, J784S4 |
|
RGMII at 10 Mbps cannot be pinged |
ENET |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
|
examples: EST: Assertion caused by invalid sizeThresEn check |
ENET |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
2.1.9. Known Issues¶
ID |
Head Line |
Module |
Reported in Release |
Affected Platforms |
Impact |
Workaround in this release |
---|---|---|---|---|---|---|
IPC Performance Test hangs after loading the binary |
IPC |
08.01.00 |
J721E, J7200, J721S2, J784S4 |
Not able to get performace numbers for IPC |
None |
|
IPC: stack corruption of taskWaiter used in RPMessage_getRemoteEndPt |
IPC |
08.00.00 |
J721E, J7200, J721S2, J784S4 |
Can not use RPMessage_getRemoteEndPt if remote endpoint is not created |
None |
|
CSL ECC Test App does not work on mcu1_0 |
CSL |
08.05.00 |
J721E, J721S2, J784S4 |
Not able to test ECC for DDR and MSMC |
None |
|
MMCSD driver has unoptimized delay values |
MMCSD |
09.00.00 |
J721E, J7200, J721S2, J784S4 |
Increase in eMMC boot time. |
None |
|
I2C: SCL line held low for longer duration on NACK |
I2C |
09.00.00 |
J721E, J7200, J721S2, J784S4 |
I2C wait time for operations could be higher than expected |
None |
|
UDMA: Driver does not clear flush bit in case of teardown for TX channels |
UDMA |
09.00.00 |
J721E, J7200, J721S2, J784S4 |
RGMII and SGMII port configuration cannot exist |
None |
|
CSIRX: Dual and 4 Pixels mode for RAW8 data is not working |
CSIRX |
09.00.00 |
J721E, J721S2, J784S4 |
Not able to use dual/quad pixel mode for raw8 |
None |
|
J784S4 / J721S2: Domain Isolation Firewalls Missing |
CSL |
09.00.00 |
J721S2, J784S4 |
Firewall cannot be setup to isolate main and mcu domains |
None |
|
BoardFlashOpen fails for Nand in DTR mode |
OSPI |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
Cannot open flash in DDR mode if already opened and closed in SDR mode |
None |
|
DSS: Dss_dctrlDrvSetLayerParamsIoctl does not support layerEnable = false |
DSS |
09.01.00 |
J721E, J721S2, J784S4 |
Not able to disable a particular pipe layer |
None |
|
GTC PLL values getting reset from SBL to Boot App |
SBL |
09.01.00 |
J7200, J721S2, J784S4 |
Incorrect GTC frequency when used with SBL or BootApp |
None |
|
DDR and MSMC Memory Benchmarking Apps are not working |
BENCHMARKS |
09.01.00 |
J721E, J7200, J721S2, J784S4 |
Not able to measure benchmarks for DDR & MSMC |
None |
|
Keywriter example application is not validated for release |
KEYWRITER |
09.02.00 |
J721E, J7200, J721S2, J784S4 |
Keywriter might flash incomplete/incorrect keys in efuse |
None, contact TI for working keywriter binary via e2e |
|
EthFW will get stuck waiting for link if link partner is not ready |
ENET |
08.x.00 |
J721E, J7200, J721S2, J784S4 |
Indefinite polling could happen in SGMII link is not up |
Link partner should be available when port is open. |
|
enet: mdio: Failure in PHY reg read in manual mode in ‘debug’ profile |
ENET |
09.00.00 |
J721E, J7200, J721S2, J784S4 |
MDIO operations will fail |
Workaround integrated in SDK 9.0 |
2.1.10. Limitations¶
2.1.10.1. PDK¶
PDK examples do not support SMP mode. Some of examples still support build in SMP mode but these binaries are not supported or validated.
TI Clang compiler does not enable O3 optimization level and Thumb2 mode which were enabled by default with TI ARM CGT compiler. This has an impact on driver throughput. E.g. Ethernet performance has reduced by ~20% on J784S4
2.1.10.2. ENET¶
Scatter-gather functionality is currently supported only for packet transmission.
gPTP stack is supported only in FreeRTOS.